PDK API Guide for J721E
|
Monolithic-mode packet descriptor.
This structure is used for monolithic-mode packet descriptors.
Data Fields | |
uint32_t | descInfo |
uint32_t | pktInfo1 |
uint32_t | pktInfo2 |
uint32_t | srcDstTag |
uint32_t CSL_UdmapCppi5MMPD::descInfo |
word 0: Monolithic Packet Descriptor Word 0
uint32_t CSL_UdmapCppi5MMPD::pktInfo1 |
word 1: Monolithic Packet Descriptor Word 1
uint32_t CSL_UdmapCppi5MMPD::pktInfo2 |
word 2: Monolithic Packet Descriptor Word 2
uint32_t CSL_UdmapCppi5MMPD::srcDstTag |
word 3: Monolithic Packet Descriptor Word 3