PDK API Guide for J721E
|
DSS Write Back Pipe DMA related Config parameters.
Data Fields | |
uint32_t | bufLowThreshold |
uint32_t | bufHighThreshold |
uint32_t | arbitration |
uint32_t | frameCaptureRate |
uint32_t | idleSize |
uint32_t | idleNumber |
uint32_t CSL_DssWbPipeDmaCfg::bufLowThreshold |
Write back DMA buffer low threshold. Number of 128 bits defining the threshold value
uint32_t CSL_DssWbPipeDmaCfg::bufHighThreshold |
Write back DMA buffer high threshold. Number of 128 bits defining the Threshold value
uint32_t CSL_DssWbPipeDmaCfg::arbitration |
Determines the priority of the write back pipeline. For valid values see CSL_DssWbPipePriorityVal
uint32_t CSL_DssWbPipeDmaCfg::frameCaptureRate |
Frame capture rate of the write back pipeline. For valid values see CSL_DssWbPipeCaptRate
uint32_t CSL_DssWbPipeDmaCfg::idleSize |
Determines if idleNumber corresponds to number of bursts or singles. Possible values are 0 or 1
uint32_t CSL_DssWbPipeDmaCfg::idleNumber |
Determines the number of idles between requests on the L3 interconnect. Used only in memory to memory mode. Range depends on idleSize parameter Range: 0-15 when idleSize is 0 0-120 when idleSize is 1