PDK API Guide for J721E
|
Stream FIFO fill level monitor. This can operate in 2 modes: 1 - Monitor peak fill level until the stream is stopped. 2 - Monitor peak fill level when the first FIFO read is made during a frame.
Data Fields | |
uint8_t | mode |
uint16_t | count |
uint8_t CSIRX_StreamFifoFillLvl::mode |
00 -> Fill level detection disabled 01 -> Mode 1 10 -> Mode 2 11 -> Reserved
uint16_t CSIRX_StreamFifoFillLvl::count |
Peak fill level of FIFO.