PDK API Guide for J721E
|
Used to observe the current data field, extracted by the protocol block from the last short packet data field and FSM state. It also indicates what data type and virtual channels were used for that short packet. This is primarily used during error condition debug. Since the data can come from asynchronous domains the data coherency cannot be relied upon.
Data Fields | |
uint8_t | protFsmState |
uint8_t | protVc |
uint8_t | protDt |
uint16_t | protWordCount |
uint8_t CSIRX_IntegrationDebug::protFsmState |
CSIRXFsmState 0x0: WAIT_FOR_PACKE 0x1: PAYLOAD_DAA 0x2: PACKET_FOOER_CHECK 0x3: Reserved
uint8_t CSIRX_IntegrationDebug::protVc |
Protocol Virtual Channel
uint8_t CSIRX_IntegrationDebug::protDt |
Protocol Datatype
uint16_t CSIRX_IntegrationDebug::protWordCount |
Protocol Word Count (Data Field)