PDK API Guide for J721E
|
TPS65941 gpio details object structure.
Data Fields | |
uint8_t | regAddr |
uint8_t | outRegAddr |
uint8_t | inRegAddr |
uint8_t | inOutRegBitPos |
uint8_t Board_Tps65941GpioRegCfg::regAddr |
uint8_t Board_Tps65941GpioRegCfg::outRegAddr |
Register Address of the gpio
uint8_t Board_Tps65941GpioRegCfg::inRegAddr |
Register Address of the output buffer of gpio
uint8_t Board_Tps65941GpioRegCfg::inOutRegBitPos |
Register Address of the input buffer of gpio