PDK API Guide for J721E
|
DMSC controls the power management, security and resource management of the device.
Data Structures | |
struct | tisci_msg_set_clock_req |
Mark a clock as required/not required. More... | |
struct | tisci_msg_set_clock_resp |
Empty response for TISCI_MSG_SET_CLOCK. More... | |
struct | tisci_msg_get_clock_req |
Get the current state of a clock. More... | |
struct | tisci_msg_get_clock_resp |
Clock state response. More... | |
struct | tisci_msg_set_clock_parent_req |
Set the clock parent. More... | |
struct | tisci_msg_set_clock_parent_resp |
Empty response for TISCI_MSG_SET_CLOCK_PARENT. More... | |
struct | tisci_msg_get_clock_parent_req |
Return the current clock parent. More... | |
struct | tisci_msg_get_clock_parent_resp |
Clock parent response. More... | |
struct | tisci_msg_get_num_clock_parents_req |
Return the number of possible parents for a clock. More... | |
struct | tisci_msg_get_num_clock_parents_resp |
Num clock parents response. More... | |
struct | tisci_msg_set_freq_req |
Set the desired frequency for a clock. More... | |
struct | tisci_msg_set_freq_resp |
Empty response for TISCI_MSG_SET_FREQ. More... | |
struct | tisci_msg_query_freq_req |
Determine the result of a hypothetical set frequency operation. More... | |
struct | tisci_msg_query_freq_resp |
Result of a query operation. More... | |
struct | tisci_msg_get_freq_req |
Get the current frequency of a device's clock. More... | |
struct | tisci_msg_get_freq_resp |
Result of get frequency request. More... | |
Functions | |
struct tisci_msg_set_clock_req | __attribute__ ((__packed__)) |
Macros | |
#define | TISCI_MSG_VALUE_CLOCK_SW_STATE_UNREQ 0 |
This file contains: More... | |
#define | TISCI_MSG_VALUE_CLOCK_SW_STATE_AUTO 1 |
#define | TISCI_MSG_VALUE_CLOCK_SW_STATE_REQ 2 |
#define | TISCI_MSG_VALUE_CLOCK_HW_STATE_NOT_READY 0 |
#define | TISCI_MSG_VALUE_CLOCK_HW_STATE_READY 1 |
#define | TISCI_MSG_FLAG_CLOCK_ALLOW_SSC TISCI_BIT(8) |
#define | TISCI_MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE TISCI_BIT(9) |
#define | TISCI_MSG_FLAG_CLOCK_INPUT_TERM TISCI_BIT(10) |
#define | TISCI_MSG_FLAG_CLOCK_SSC_ACTIVE TISCI_BIT(11) |
#define TISCI_MSG_VALUE_CLOCK_SW_STATE_UNREQ 0 |
This file contains:
WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!! System Firmware
Cortex-M3 (CM3) firmware for power management The IP does not require this clock, it can be disabled, regardless of the state of the device
#define TISCI_MSG_VALUE_CLOCK_SW_STATE_AUTO 1 |
Allow the system controller to automatically manage the state of this clock. If the device is enabled, then the clock is enabled. If the device is set to off or retention, then the clock is internally set as not being required by the device. This is the default state.
#define TISCI_MSG_VALUE_CLOCK_SW_STATE_REQ 2 |
Configure the clock to be enabled, regardless of the state of the device.
#define TISCI_MSG_VALUE_CLOCK_HW_STATE_NOT_READY 0 |
Indicate hardware state of the clock is that it is not running.
#define TISCI_MSG_VALUE_CLOCK_HW_STATE_READY 1 |
Indicate hardware state of the clock is that it is running.
#define TISCI_MSG_FLAG_CLOCK_ALLOW_SSC TISCI_BIT(8) |
Allow this clock to be modified via spread spectrum clocking.
#define TISCI_MSG_FLAG_CLOCK_ALLOW_FREQ_CHANGE TISCI_BIT(9) |
Allow this clock's frequency to be changed while it is running so long as it is within the min/max limits.
#define TISCI_MSG_FLAG_CLOCK_INPUT_TERM TISCI_BIT(10) |
Enable input termination, this is only applicable to clock inputs on the SoC pseudo-device, TISCI_BOARD0.
#define TISCI_MSG_FLAG_CLOCK_SSC_ACTIVE TISCI_BIT(11) |
Indicate that SSC is active for this clock.
struct tisci_msg_set_clock_req __attribute__ | ( | (__packed__) | ) |