This is SDE Configuration file
|
file | sde_cfg.h |
| Defines the structures / control operations that could be used to configure / control SDE of DMPAC.
|
|
|
typedef void(* | Sde_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
| Prototype for the Error Event for SDE. The callback for the SDE error events can be registered using Sde_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs. More...
|
|
#define DMPAC_SDE_NUM_SCORE_MAP (8U) |
#define SDE_MIN_IMAGE_WIDTH (128U) |
#define SDE_MIN_IMAGE_HEIGHT (64U) |
#define SDE_MAX_IMAGE_WIDTH (2048U) |
#define SDE_MAX_IMAGE_HEIGHT (1024U) |
#define VHWA_SDE_RD_ERR (0x40000U) |
Error on SDE VBUSM Read interface.
<Error on SDE SL2 VBSUM Write interface
#define VHWA_SDE_WR_ERR (0x80000U) |
Error on FOCO0 SL2 VBSUM Write interface.
#define VHWA_SDE_FOCO0_SL2_WR_ERR (0x2000000U) |
Error on FOCO0 VBUSM Read interface.
#define VHWA_SDE_FOCO0_VBUSM_RD_ERR (0x1000000U) |
typedef void(* Sde_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
Prototype for the Error Event for SDE. The callback for the SDE error events can be registered using Sde_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs.
- Parameters
-
handle | FVID2 driver handle, for which error has occurred. |
errEvents | Error Events occured, Refer to Sde_ErrorEvents for valid values. |
- Returns
- None.
This function should be used to initialize SDE configuration.
- Parameters
-
- Returns
- None