This is NF Configuration file
|
file | nf_cfg.h |
| Defines the structures / control operations that could be used to configure / control NF of VPAC.
|
|
|
typedef void(* | Nf_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
| Prototype for the Error Event for NF. The callback for the NF error events can be registered using Nf_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs. More...
|
|
|
Macro's to define NF Error events, for which NF callback could be registered.
Caution: These macro values are directly used by driver
for enabling events. |
#define | VHWA_NF_RD_ERR (0x400U) |
| Error on NF VBUSM Read interface. More...
|
|
#define | VHWA_NF_WR_ERR (0x200U) |
|
#define NF_BL_LUT_SIZE (5U*256U) |
NF Lut Size in bytes for in Bi-lateral filter mode.
NF Lut Size in Words for in Bi-lateral filter mode.
#define NF_GEN_LUT_SIZE (24U) |
NF Lut Size in bytes for in Generic filter mode.
NF Lut Size in Words for in Generic filter mode.
#define VHWA_NF_RD_ERR (0x400U) |
Error on NF VBUSM Read interface.
<Error on NF SL2 VBSUM Write interface
#define VHWA_NF_WR_ERR (0x200U) |
#define NF_FILTER_MODE_BILATERAL (0x0u) |
Use Bilateral filtering.
<Use Generic 2D filtering
#define NF_FILTER_MODE_GENERIC_2D_FILTER (0x1u) |
typedef void(* Nf_ErrEventCbFxn) (Fvid2_Handle handle, uint32_t errEvents, void *appData) |
Prototype for the Error Event for NF. The callback for the NF error events can be registered using Nf_ErrEventParams. One of the parameter in this is call back. Driver calls this callback when error occurs.
- Parameters
-
handle | FVID2 driver handle, for which error has occurred. |
errEvents | Error Events occured, Refer to Nf_ErrorEvents for valid values. |
- Returns
- None.
static void Nf_ConfigInit |
( |
Nf_Config * |
nfCfg | ) |
|
|
inlinestatic |
This function should be used to initialize variable of type Nf_Config.
- Parameters
-
- Returns
- None