This is documentation for MultiProc configuration used by IPC
|
file | ipc_mp.h |
| IPC - Multiproc interface.
|
|
#define IPC_MP_INVALID_ID (0xFFFFFFFFU) |
int32_t Ipc_mpSetConfig |
( |
uint32_t |
selfId, |
|
|
uint16_t |
numProc, |
|
|
uint32_t |
procArry[IPC_MAX_PROCS] |
|
) |
| |
Sets the multiproc configuration.
sets the current current processor, number of processor, and array of processors participating
- Parameters
-
selfId | [IN] Self ProcId |
numProc | [IN] Number of core in application |
procArry | [IN] Array of processorId in application |
- Returns
- IPC_SOK for success IPC_MP_INVALID_ID for invalid parameter
uint32_t Ipc_mpGetId |
( |
const char * |
name | ) |
|
Gets the MultiProc id.
Retrieves the MultiProc id for the processor with corresponding MultiProc name. IPC_MP_INVALID_ID is returned if the name was not found.
- Parameters
-
name | [IN] Name of the processor. |
- Returns
- ProcId if valid core name, else returns -1
const char* Ipc_mpGetName |
( |
uint32_t |
id | ) |
|
Gets the name of a processor.
- Parameters
-
- Returns
- Name of the processor The returned string should never be modified.
uint16_t Ipc_mpGetNumProcessors |
( |
void |
| ) |
|
Gets the number of processors.
- Returns
- Number of processors configured with MultiProc
uint32_t Ipc_mpGetSelfId |
( |
void |
| ) |
|
Gets executing processor's MultiProc id.
- Returns
- Executing processor's id
const char* Ipc_mpGetSelfName |
( |
void |
| ) |
|
Get the processor name for current processor.
uint32_t Ipc_mpGetRemoteProcId |
( |
uint32_t |
coreIndex | ) |
|
Returns procId of the given index.