This is VISS H3A Configuration file
|
file | h3a_cfg.h |
| Interface file for H3A module, Defines the structures / control operations that could be used to configure / control H3A module in VISS H3A is independent module, which takes input from RAWFE. This is why a separate interface file is used for controlling H3A.
|
|
|
struct | H3a_AfIirFiltConfig |
| IIR Filter Configuration structure. More...
|
|
struct | H3a_AfFirFilrConfig |
| FIR Filter Configuration structure. More...
|
|
struct | H3a_PaxelConfig |
| Paxel/Window configuration structure Used to define paxel for AEWB and window for AF. More...
|
|
struct | H3a_AfConfig |
| Structure for ISP H3A AF engine parameters. More...
|
|
struct | H3a_AewbConfig |
| Structure for ISP H3A AEWB engine parameters. More...
|
|
struct | H3a_Config |
| Structure for H3A configuration VPAC can output only one of AF or AEWB output. This structure is used for selecting H3A output module AF/AEWB and also used for for setting module configuration. When AF is enabled as an output module, only AF will be configured. Also when AEWB module is enabled/selected as an output module, only AEWB mdule will be configured. More...
|
|
|
Control commands for H3A module in VISS Mainly used to set H3A AF/AEWB configuration
|
#define | IOCTL_H3A_SET_CONFIG (VHWA_IOCTL_H3A_IOCTL_BASE) |
| Ioctl for setting H3A parameters. Only one of AF or AEWB module can be configured at a time. Only one of AF and AEWB can be enabled in the H3A module at a time for a frame. So this ioctl enables/supports only one of these modules. Refer to structure H3a_Config. More...
|
|
#define | IOCTL_H3A_GET_AEWB_SIZE (IOCTL_H3A_SET_CONFIG + 1U) |
| Ioctl for Getting H3a output size for AF/AEWB module. Depending on the H3A AF/AEWB module enabled, it returns the output frame size. Refer to structure H3a_Config. More...
|
|
|
Defines vertical focus mode Refer to specs for more details
Caution: This macro values are directly used in
configuring register |
#define | H3A_AF_VF_HORZ_ONLY (0x0U) |
|
#define | H3A_AF_VF_VERT_HORZ (0x1U) |
|
Ioctl for setting H3A parameters. Only one of AF or AEWB module can be configured at a time. Only one of AF and AEWB can be enabled in the H3A module at a time for a frame. So this ioctl enables/supports only one of these modules. Refer to structure H3a_Config.
- Returns
- FVID2_SOK on success, else error code.
Ioctl for Getting H3a output size for AF/AEWB module. Depending on the H3A AF/AEWB module enabled, it returns the output frame size. Refer to structure H3a_Config.
- Returns
- FVID2_SOK on success, else error code.
#define H3A_AF_IIR_COEFF_MAX (11U) |
Maximum IIR coefficients.
#define H3A_AF_FIR_COEFF_MAX (5U) |
Maximum FIR coefficients.
#define H3A_MODULE_MIN (0x0U) |
< AutoFocus module AutoFocus module
#define H3A_MODULE_AF (0x1U) |
Auto Exposure and Auto White Balance Module
#define H3A_MODULE_AEWB (0x2U) |
Max value, used internally for error checking
#define H3A_MODULE_MAX (0x3U) |
#define H3A_AF_RGBPOS_GR_GB (0x0U) |
< The input Bayer format is GRGB The input Bayer format is RGGB
#define H3A_AF_RGBPOS_RG_GB (0x1U) |
The input Bayer format is GRBG
#define H3A_AF_RGBPOS_GR_BG (0x2U) |
The input Bayer format is RGBG
#define H3A_AF_RGBPOS_RG_BG (0x3U) |
The input Bayer format is GGRB
#define H3A_AF_RGBPOS_GG_RB (0x4U) |
The input Bayer format is RBGG
#define H3A_AF_RGBPOS_RB_GG (0x5U) |
Max Value, used for error checking
#define H3A_AF_RGBPOS_MAX (0x6U) |
#define H3A_AF_FV_MODE_SUM (0x0U) |
< FV Accumulation mode is sum mode FV Accumulation mode is Peak mode
#define H3A_AF_FV_MODE_PEAK (0x1U) |
Max Value, used for error checking
#define H3A_AF_FV_MODE_MAX (0x2U) |
#define H3A_AF_VF_HORZ_ONLY (0x0U) |
< Vertical Focus mode is 4 color horizontal FV Only Vertical Focus mode is 1 color horizontal and 1 color vertical
#define H3A_AF_VF_VERT_HORZ (0x1U) |
#define H3A_AEWB_OUTPUT_MODE_SUM_SQR (0x0U) |
< Output format is sum of square Output format is Min and Max Value
#define H3A_AEWB_OUTPUT_MODE_MIN_MAX (0x1U) |
Output format is sum only
#define H3A_AEWB_OUTPUT_MODE_SUM_ONLY (0x2U) |