PDK API Guide for J721E
|
This is DSS documentation specific to J7 SoC
Sub Modules | |
Display Controller IOCTLs | |
Files | |
file | dss_soc.h |
DSS Driver J7 SOC specific file. | |
Data Structures | |
struct | Dss_IrqParams |
Structure containing DSS interrupt information. Events should be enabled only for available Video Ports and Video Pipes. More... | |
struct | Dss_RmInfo |
Structure containing resources manager information. This enables display sharing between two different softwares. More... | |
struct | Dss_DpInitParams |
Structure containing Display Port init parameters. More... | |
struct | Dss_DsiInitParams |
Structure containing DSI init parameters. More... | |
struct | Dss_SocParams |
DSS SOC parameters. More... | |
struct | Dss_DctrlDpHpdCbParams |
DSS DP HPD Callback parameters. More... | |
Functions | |
static uint32_t | Dss_dispIsVidInst (uint32_t instId) |
Check if the display driver instance is of type Video pipeline. More... | |
static uint32_t | Dss_dispIsVidLInst (uint32_t instId) |
Check if the display driver instance is of type Video lite pipeline. More... | |
static void | Dss_irqParamsInit (Dss_IrqParams *irqParams) |
Dss_IrqParams structure init function. More... | |
static void | Dss_rmInfoInit (Dss_RmInfo *rmInfo) |
Dss_RmInfo structure init function. More... | |
static void | Dss_dpInitParamsInit (Dss_DpInitParams *dpInitParams) |
Dss_DpInitParams structure init function. More... | |
static void | Dss_socParamsInit (Dss_SocParams *socParams) |
Dss_SocParams structure init function. More... | |
static void | Dss_dctrlDpHpdCbParamsInit (Dss_DctrlDpHpdCbParams *cbParams) |
Dss_DctrlDpHpdCbParams structure init function. More... | |
static void | Dss_dsiInitParamsInit (Dss_DsiInitParams *dsiInitParams) |
Typedefs | |
typedef void(* | Dss_DctrlDpHpdCbFxn) (uint32_t hpdState, void *appData) |
DP HPD callback function prototype. More... | |
Macros | |
#define | DSS_DCTRL_MAX_NODES (22U) |
Defines maximum number of nodes for allocation including invalid node. More... | |
#define | DSS_DCTRL_MAX_EDGES (32U) |
Defines maximum number of edges for allocation. This is derived by looking at all possible DSS connections in the SoC. More... | |
#define | DSS_FUNC_IRQ_DEFAULT_NUM (52U) |
DSS Safety Interrupt Number for R5. More... | |
#define | DSS_SAFE_IRQ_DEFAULT_NUM (54U) |
DSS Functional Interrupt Number for R5. More... | |
#define | DSS_SECURE_IRQ_DEFAULT_NUM (56U) |
DSS DCTRL Instance IDs | |
#define | DSS_DCTRL_INST_0 (0U) |
Display controller instance 0. More... | |
#define | DSS_DCTRL_INST_MAX (1U) |
Maximum number of display driver instances. More... | |
DSS Display Instance IDs | |
#define | DSS_DISP_INST_VID1 (CSL_DSS_VID_PIPE_ID_VID1) |
Video 1 Pipeline display driver instance number. More... | |
#define | DSS_DISP_INST_VIDL1 (CSL_DSS_VID_PIPE_ID_VIDL1) |
Video Lite 1 Pipeline display driver instance number. More... | |
#define | DSS_DISP_INST_VID2 (CSL_DSS_VID_PIPE_ID_VID2) |
Video 2 Pipeline display driver instance number. More... | |
#define | DSS_DISP_INST_VIDL2 (CSL_DSS_VID_PIPE_ID_VIDL2) |
Video Lite 2 Pipeline display driver instance number. More... | |
#define | DSS_DISP_INST_MAX (CSL_DSS_VID_PIPE_ID_MAX) |
Maximum number of display driver instances. More... | |
DSS DCTRL Node type | |
Node types that are used by the set path to connect different modules and create a graph | |
#define | DSS_DCTRL_NODE_TYPE_INVALID ((uint32_t) 0x0U) |
#define | DSS_DCTRL_NODE_TYPE_PIPE ((uint32_t) 0x1U) |
#define | DSS_DCTRL_NODE_TYPE_OVERLAY ((uint32_t) 0x2U) |
#define | DSS_DCTRL_NODE_TYPE_VP ((uint32_t) 0x3U) |
#define | DSS_DCTRL_NODE_TYPE_OUTPUT ((uint32_t) 0x4U) |
DSS DCTRL Node Id | |
Node ids that are used by the set path to connect different modules and create a graph | |
#define | DSS_DCTRL_NODE_INVALID (0x0U) |
#define | DSS_DCTRL_NODE_VID1 (0x1U) |
#define | DSS_DCTRL_NODE_VIDL1 (0x2U) |
#define | DSS_DCTRL_NODE_VID2 (0x3U) |
#define | DSS_DCTRL_NODE_VIDL2 (0x4U) |
#define | DSS_DCTRL_NODE_OVERLAY1 (0x5U) |
#define | DSS_DCTRL_NODE_OVERLAY2 (0x6U) |
#define | DSS_DCTRL_NODE_OVERLAY3 (0x7U) |
#define | DSS_DCTRL_NODE_OVERLAY4 (0x8U) |
#define | DSS_DCTRL_NODE_VP1 (0x9U) |
#define | DSS_DCTRL_NODE_VP2 (0xAU) |
#define | DSS_DCTRL_NODE_VP3 (0xBU) |
#define | DSS_DCTRL_NODE_VP4 (0xCU) |
#define | DSS_DCTRL_NODE_DPI_DPI0 (0xDU) |
#define | DSS_DCTRL_NODE_DPI_DPI1 (0xEU) |
#define | DSS_DCTRL_NODE_EDP_DPI0 (0xFU) |
#define | DSS_DCTRL_NODE_EDP_DPI1 (0x10U) |
#define | DSS_DCTRL_NODE_EDP_DPI2 (0x11U) |
#define | DSS_DCTRL_NODE_EDP_DPI3 (0x12U) |
#define | DSS_DCTRL_NODE_DSI_DPI2 (0x13U) |
#define | DSS_DCTRL_NODE_DISCSYNC0 (0x14U) |
#define | DSS_DCTRL_NODE_DISCSYNC1 (0x15U) |
Instance Ids for DSS Event Manager. | |
#define | DSS_EVT_MGR_INST_ID_FUNC ((uint32_t) 0x00U) |
Instance Id for functional interrupts. More... | |
#define | DSS_EVT_MGR_INST_ID_SAFETY ((uint32_t) 0x01U) |
Instance Id for security interrupts. More... | |
#define | DSS_EVT_MGR_INST_ID_SECURITY ((uint32_t) 0x02U) |
Max Instance Id. More... | |
#define | DSS_EVT_MGR_INST_ID_MAX ((uint32_t) 0x03U) |
Invalid Instance Id. More... | |
#define | DSS_EVT_MGR_INST_ID_INVALID ((uint32_t) 0xFFU) |
#define DSS_DCTRL_INST_0 (0U) |
Display controller instance 0.
#define DSS_DCTRL_INST_MAX (1U) |
Maximum number of display driver instances.
#define DSS_DISP_INST_VID1 (CSL_DSS_VID_PIPE_ID_VID1) |
Video 1 Pipeline display driver instance number.
#define DSS_DISP_INST_VIDL1 (CSL_DSS_VID_PIPE_ID_VIDL1) |
Video Lite 1 Pipeline display driver instance number.
#define DSS_DISP_INST_VID2 (CSL_DSS_VID_PIPE_ID_VID2) |
Video 2 Pipeline display driver instance number.
#define DSS_DISP_INST_VIDL2 (CSL_DSS_VID_PIPE_ID_VIDL2) |
Video Lite 2 Pipeline display driver instance number.
#define DSS_DISP_INST_MAX (CSL_DSS_VID_PIPE_ID_MAX) |
Maximum number of display driver instances.
#define DSS_DCTRL_NODE_TYPE_INVALID ((uint32_t) 0x0U) |
#define DSS_DCTRL_NODE_TYPE_PIPE ((uint32_t) 0x1U) |
#define DSS_DCTRL_NODE_TYPE_OVERLAY ((uint32_t) 0x2U) |
#define DSS_DCTRL_NODE_TYPE_VP ((uint32_t) 0x3U) |
#define DSS_DCTRL_NODE_TYPE_OUTPUT ((uint32_t) 0x4U) |
#define DSS_DCTRL_NODE_INVALID (0x0U) |
#define DSS_DCTRL_NODE_VID1 (0x1U) |
#define DSS_DCTRL_NODE_VIDL1 (0x2U) |
#define DSS_DCTRL_NODE_VID2 (0x3U) |
#define DSS_DCTRL_NODE_VIDL2 (0x4U) |
#define DSS_DCTRL_NODE_OVERLAY1 (0x5U) |
#define DSS_DCTRL_NODE_OVERLAY2 (0x6U) |
#define DSS_DCTRL_NODE_OVERLAY3 (0x7U) |
#define DSS_DCTRL_NODE_OVERLAY4 (0x8U) |
#define DSS_DCTRL_NODE_VP1 (0x9U) |
#define DSS_DCTRL_NODE_VP2 (0xAU) |
#define DSS_DCTRL_NODE_VP3 (0xBU) |
#define DSS_DCTRL_NODE_VP4 (0xCU) |
#define DSS_DCTRL_NODE_DPI_DPI0 (0xDU) |
#define DSS_DCTRL_NODE_DPI_DPI1 (0xEU) |
#define DSS_DCTRL_NODE_EDP_DPI0 (0xFU) |
#define DSS_DCTRL_NODE_EDP_DPI1 (0x10U) |
#define DSS_DCTRL_NODE_EDP_DPI2 (0x11U) |
#define DSS_DCTRL_NODE_EDP_DPI3 (0x12U) |
#define DSS_DCTRL_NODE_DSI_DPI2 (0x13U) |
#define DSS_DCTRL_NODE_DISCSYNC0 (0x14U) |
#define DSS_DCTRL_NODE_DISCSYNC1 (0x15U) |
#define DSS_DCTRL_MAX_NODES (22U) |
Defines maximum number of nodes for allocation including invalid node.
#define DSS_DCTRL_MAX_EDGES (32U) |
Defines maximum number of edges for allocation. This is derived by looking at all possible DSS connections in the SoC.
DSS Functional Interrupt Number for R5
#define DSS_FUNC_IRQ_DEFAULT_NUM (52U) |
DSS Safety Interrupt Number for R5.
#define DSS_SAFE_IRQ_DEFAULT_NUM (54U) |
DSS Functional Interrupt Number for R5.
#define DSS_SECURE_IRQ_DEFAULT_NUM (56U) |
#define DSS_EVT_MGR_INST_ID_FUNC ((uint32_t) 0x00U) |
Instance Id for functional interrupts.
<Instance Id for safety interrupts
#define DSS_EVT_MGR_INST_ID_SAFETY ((uint32_t) 0x01U) |
Instance Id for security interrupts.
#define DSS_EVT_MGR_INST_ID_SECURITY ((uint32_t) 0x02U) |
Max Instance Id.
#define DSS_EVT_MGR_INST_ID_MAX ((uint32_t) 0x03U) |
Invalid Instance Id.
#define DSS_EVT_MGR_INST_ID_INVALID ((uint32_t) 0xFFU) |
typedef void(* Dss_DctrlDpHpdCbFxn) (uint32_t hpdState, void *appData) |
DP HPD callback function prototype.
hpdState | [OUT] HPD state TRUE / FALSE. |
appData | [OUT] Application's private data. |
|
inlinestatic |
Check if the display driver instance is of type Video pipeline.
instId | [IN]Driver Instance Id. |
|
inlinestatic |
Check if the display driver instance is of type Video lite pipeline.
instId | [IN]Driver Instance Id. |
|
inlinestatic |
Dss_IrqParams structure init function.
irqParams | Pointer to Dss_IrqParams structure. |
|
inlinestatic |
|
inlinestatic |
Dss_DpInitParams structure init function.
dpInitParams | Pointer to Dss_DpInitParams structure. |
|
inlinestatic |
Dss_SocParams structure init function.
socParams | Pointer to Dss_SocParams structure. |
|
inlinestatic |
Dss_DctrlDpHpdCbParams structure init function.
cbParams | Pointer to Dss_DctrlDpHpdCbParams structure. |
|
inlinestatic |