PDK API Guide for J721E
CSITX SoC Config

Introduction

This is CSITX documentation specific to J7ES SoC

Files

file  csitx_soc.h
 CSITX Low Level Driver SOC specific file.
 

Data Structures

struct  Csitx_DPhyCfg
 D-PHY configuration structure. More...
 

Functions

void Csitx_initDPhyCfgParams (Csitx_DPhyCfg *dphyCfg)
 Csitx_DPhyCfg structure init function. More...
 

Macros

#define CSITX_NUM_STREAM   (1U)
 CSITX DRV Numbers: Number of stream per CSI TX module. More...
 

CSITX Module Instance ID

Different instances of CSI Tx Module instances.

#define CSITX_INSTANCE_ID_0   ((uint32_t) 0x0U)
 CSITX Module Instance ID: CSI2TX Module 0. More...
 
#define CSITX_INSTANCE_ID_MAX   ((uint32_t)CSITX_INSTANCE_ID_0 + 1U)
 Maximum value of CSITX Module Instance. More...
 

CSITX SoC integration details

Different instances of CSI Tx transmit module supported in the Instance and their configuration/integration supported in the Instance.

#define CSITX_NUM_STRMS_TX   ((uint32_t) 1U)
 Total number of transmit processing streams available in the Instance. More...
 
#define CSITX_NUM_STRMS_COLORBAR   ((uint32_t) 1U)
 Total number of COLORBAR streams available in the Instance. Note: COLORBAR stream is only supported on 'CSITX_INSTANCE_ID_0' only. More...
 
#define CSITX_NUM_STRMS_LPBK   ((uint32_t) 2U)
 Total number of Loop-back streams available in the Instance. More...
 
#define CSITX_NUM_CH_TX   ((uint32_t) 32U)
 Number of transmit channels per CSITX instance. More...
 
#define CSITX_NUM_CH_LPBK   ((uint32_t) 1U)
 Number of transmit channels per CSITX instance. More...
 
#define CSITX_NUM_CH_TX_MAX
 Number of transmit channels that can run in parallel in the Instance. More...
 
#define CSITX_NUM_CH_COLORBAR_MAX   ((uint32_t) 1U)
 Number of COLORBAR channels that can run in parallel in the Instance. More...
 
#define CSITX_NUM_CH_LPBK_MAX
 Number of Loop-back channels that can run in parallel in the Instance. Note: Though each CSI instance have one loop-back stream, only one can be used in the Instance which can be configured on any instance. More...
 
#define CSITX_NUM_CH_MAX
 Maximum number of channels that can be processed per CSITX module These many valid channel configurations can exists per CSITX DRV instance. More...
 
#define CSITX_TX_DATA_LANES_MAX   ((uint32_t)4U)
 Defines total number of physical data lanes that can be used per CSITX instance. More...
 
#define CSITX_TX_CLK_LANES_MAX   ((uint32_t)1U)
 Defines total number of physical clock lanes that can be used per CSITX instance. More...
 
#define CSITX_TX_VC_CFG_MAX   ((uint32_t)16U)
 Defines total number of VC configurations available CSITX instance. More...
 
#define CSITX_TX_DT_CFG_MAX   ((uint32_t)16U)
 Defines total number of DT configurations available CSITX instance. More...
 
#define CSITX_TX_STRM_NUM_MAX   ((uint32_t)4U)
 Defines total number of streams available CSITX instance. More...
 
#define CSITX_TX_STRM_FIFO_FILL_LVL   ((uint32_t)960U)
 Defines total number of words for stream FIFO fill level 1920 RAW12 format, 1920 * 12 / 32 = 720. More...
 
#define CSITX_NUM_STRMS_TX_ID   ((uint32_t) 0U)
 Tx Stream ID. More...
 
#define CSITX_NUM_STRMS_TX_COLORBAR   ((uint32_t) 1U)
 Color-bar Stream ID. More...
 
#define CSITX_NUM_STRMS_TX_RETRANS_0   ((uint32_t) 2U)
 Re-transmit Stream 0 ID. More...
 
#define CSITX_NUM_STRMS_TX_RETRANS_1   ((uint32_t) 3U)
 Re-transmit Stream 1 ID. More...
 

CSITX D-PHY lane band speed

Lane band speed options for CSITX D-PHY.

#define CSITX_LANE_BAND_SPEED_80_TO_100_MBPS   ((uint32_t) 0x00U)
 Lane Band Speed: 80 Mbps to 100 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_100_TO_120_MBPS   ((uint32_t) 0x01U)
 Lane Band Speed: 100 Mbps to 120 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_120_TO_160_MBPS   ((uint32_t) 0x02U)
 Lane Band Speed: 120 Mbps to 160 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_160_TO_200_MBPS   ((uint32_t) 0x03U)
 Lane Band Speed: 160 Mbps to 200 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_200_TO_240_MBPS   ((uint32_t) 0x04U)
 Lane Band Speed: 200 Mbps to 240 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_240_TO_320_MBPS   ((uint32_t) 0x05U)
 Lane Band Speed: 240 Mbps to 320 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_320_TO_390_MBPS   ((uint32_t) 0x06U)
 Lane Band Speed: 320 Mbps to 390 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_390_TO_450_MBPS   ((uint32_t) 0x07U)
 Lane Band Speed: 390 Mbps to 450 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_450_TO_510_MBPS   ((uint32_t) 0x08U)
 Lane Band Speed: 450 Mbps to 520 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_510_TO_560_MBPS   ((uint32_t) 0x09U)
 Lane Band Speed: 510 Mbps to 560 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_560_TO_640_MBPS   ((uint32_t) 0x0AU)
 Lane Band Speed: 560 Mbps to 640 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_640_TO_690_MBPS   ((uint32_t) 0x0BU)
 Lane Band Speed: 640 Mbps to 690 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_690_TO_770_MBPS   ((uint32_t) 0x0CU)
 Lane Band Speed: 690 Mbps to 770 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_770_TO_870_MBPS   ((uint32_t) 0x0DU)
 Lane Band Speed: 770 Mbps to 870 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_870_TO_950_MBPS   ((uint32_t) 0x0EU)
 Lane Band Speed: 870 Mbps to 950 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_950_TO_1000_MBPS   ((uint32_t) 0x0FU)
 Lane Band Speed: 950 Mbps to 1000 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_1000_TO_1200_MBPS   ((uint32_t) 0x10U)
 Lane Band Speed: 1000 Mbps to 1200 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_1200_TO_1400_MBPS   ((uint32_t) 0x11U)
 Lane Band Speed: 1200 Mbps to 1400 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_1400_TO_1600_MBPS   ((uint32_t) 0x12U)
 Lane Band Speed: 1400 Mbps to 1600 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_1600_TO_1800_MBPS   ((uint32_t) 0x13U)
 Lane Band Speed: 1600 Mbps to 1800 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_1800_TO_2000_MBPS   ((uint32_t) 0x14U)
 Lane Band Speed: 1800 Mbps to 2000 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_2000_TO_2200_MBPS   ((uint32_t) 0x15U)
 Lane Band Speed: 2000 Mbps to 2200 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_2200_TO_2500_MBPS   ((uint32_t) 0x16U)
 Lane Band Speed: 2200 Mbps to 2500 Mbps. More...
 
#define CSITX_LANE_BAND_SPEED_RESERVED   ((uint32_t) 0x17U)
 Lane Band Speed: Reserved. More...
 

CSITX D-PHY clock mode

clock mode for CSITX D-PHY.

#define CSITX_CLK_MODE_CONTINUOUS   ((uint32_t) 0x0U)
 DPHY Clock Mode: Continuous. More...
 
#define CSITX_CLK_MODE_NON_CONTINUOUS   ((uint32_t) 0x1U)
 DPHY Clock Mode: Non-continuous. More...
 

CSITX D-PHY mode

Operational mode for CSITX D-PHY lanes.

#define CSITX_DPHY_MODE_ULP   ((uint32_t) 0x0U)
 DPHY Clock Mode: ultra low power. More...
 
#define CSITX_DPHY_MODE_HIGH_SPEED   ((uint32_t) 0x1U)
 DPHY Clock Mode: high speed. More...
 
#define CSITX_DPHY_MODE_LOW_POWER   ((uint32_t) 0x2U)
 DPHY Clock Mode: low power stop state. More...
 

CSITX Stream ID

CSI2 TX streams are hw entities that processes incoming frames and sends it to particular destination like DDR, VISS/VP and CSI2 TX. Mapping of streams to destination is fixed in the design and can not be changes runtime.

#define CSITX_STREAM_ID_INST_0_STRM_0   ((uint32_t) 0x0U)
 CSITX Instance ID: transmit stream0 0 on CSI2TX Module 0. More...
 
#define CSITX_STREAM_ID_INST_0_STRM_1   ((uint32_t) 0x1U)
 CSITX Instance ID: Color-bar stream on CSI2TX Module 0. More...
 
#define CSITX_STREAM_ID_INST_0_STRM_2   ((uint32_t) 0x2U)
 CSITX Instance ID: CSI2RX loop-back 0 on CSI2TX Module 0. More...
 
#define CSITX_STREAM_ID_INST_0_STRM_3   ((uint32_t) 0x3U)
 CSITX Instance ID: CSI2RX loop-back 1 on CSI2TX Module 0. More...
 

Macro Definition Documentation

#define CSITX_INSTANCE_ID_0   ((uint32_t) 0x0U)

CSITX Module Instance ID: CSI2TX Module 0.

#define CSITX_INSTANCE_ID_MAX   ((uint32_t)CSITX_INSTANCE_ID_0 + 1U)

Maximum value of CSITX Module Instance.

#define CSITX_NUM_STRMS_TX   ((uint32_t) 1U)

Total number of transmit processing streams available in the Instance.

#define CSITX_NUM_STRMS_COLORBAR   ((uint32_t) 1U)

Total number of COLORBAR streams available in the Instance. Note: COLORBAR stream is only supported on 'CSITX_INSTANCE_ID_0' only.

#define CSITX_NUM_STRMS_LPBK   ((uint32_t) 2U)

Total number of Loop-back streams available in the Instance.

#define CSITX_NUM_CH_TX   ((uint32_t) 32U)

Number of transmit channels per CSITX instance.

#define CSITX_NUM_CH_LPBK   ((uint32_t) 1U)

Number of transmit channels per CSITX instance.

#define CSITX_NUM_CH_TX_MAX
Value:
((uint32_t) (CSITX_NUM_CH_TX *\
#define CSITX_INSTANCE_ID_MAX
Maximum value of CSITX Module Instance.
Definition: csitx_soc.h:74
#define CSITX_NUM_CH_TX
Number of transmit channels per CSITX instance.
Definition: csitx_soc.h:93

Number of transmit channels that can run in parallel in the Instance.

#define CSITX_NUM_CH_COLORBAR_MAX   ((uint32_t) 1U)

Number of COLORBAR channels that can run in parallel in the Instance.

#define CSITX_NUM_CH_LPBK_MAX
Value:
((uint32_t) (CSITX_NUM_CH_LPBK * \
#define CSITX_NUM_STRMS_LPBK
Total number of Loop-back streams available in the Instance.
Definition: csitx_soc.h:91
#define CSITX_NUM_CH_LPBK
Number of transmit channels per CSITX instance.
Definition: csitx_soc.h:95

Number of Loop-back channels that can run in parallel in the Instance. Note: Though each CSI instance have one loop-back stream, only one can be used in the Instance which can be configured on any instance.

#define CSITX_NUM_CH_MAX
Value:
((uint32_t) (CSITX_NUM_CH_TX +\
#define CSITX_NUM_CH_COLORBAR_MAX
Number of COLORBAR channels that can run in parallel in the Instance.
Definition: csitx_soc.h:100
#define CSITX_NUM_CH_TX
Number of transmit channels per CSITX instance.
Definition: csitx_soc.h:93
#define CSITX_NUM_CH_LPBK_MAX
Number of Loop-back channels that can run in parallel in the Instance. Note: Though each CSI instance...
Definition: csitx_soc.h:105

Maximum number of channels that can be processed per CSITX module These many valid channel configurations can exists per CSITX DRV instance.

#define CSITX_TX_DATA_LANES_MAX   ((uint32_t)4U)

Defines total number of physical data lanes that can be used per CSITX instance.

#define CSITX_TX_CLK_LANES_MAX   ((uint32_t)1U)

Defines total number of physical clock lanes that can be used per CSITX instance.

#define CSITX_TX_VC_CFG_MAX   ((uint32_t)16U)

Defines total number of VC configurations available CSITX instance.

#define CSITX_TX_DT_CFG_MAX   ((uint32_t)16U)

Defines total number of DT configurations available CSITX instance.

#define CSITX_TX_STRM_NUM_MAX   ((uint32_t)4U)

Defines total number of streams available CSITX instance.

#define CSITX_TX_STRM_FIFO_FILL_LVL   ((uint32_t)960U)

Defines total number of words for stream FIFO fill level 1920 RAW12 format, 1920 * 12 / 32 = 720.

#define CSITX_NUM_STRMS_TX_ID   ((uint32_t) 0U)

Tx Stream ID.

#define CSITX_NUM_STRMS_TX_COLORBAR   ((uint32_t) 1U)

Color-bar Stream ID.

#define CSITX_NUM_STRMS_TX_RETRANS_0   ((uint32_t) 2U)

Re-transmit Stream 0 ID.

#define CSITX_NUM_STRMS_TX_RETRANS_1   ((uint32_t) 3U)

Re-transmit Stream 1 ID.

#define CSITX_LANE_BAND_SPEED_80_TO_100_MBPS   ((uint32_t) 0x00U)

Lane Band Speed: 80 Mbps to 100 Mbps.

#define CSITX_LANE_BAND_SPEED_100_TO_120_MBPS   ((uint32_t) 0x01U)

Lane Band Speed: 100 Mbps to 120 Mbps.

#define CSITX_LANE_BAND_SPEED_120_TO_160_MBPS   ((uint32_t) 0x02U)

Lane Band Speed: 120 Mbps to 160 Mbps.

#define CSITX_LANE_BAND_SPEED_160_TO_200_MBPS   ((uint32_t) 0x03U)

Lane Band Speed: 160 Mbps to 200 Mbps.

#define CSITX_LANE_BAND_SPEED_200_TO_240_MBPS   ((uint32_t) 0x04U)

Lane Band Speed: 200 Mbps to 240 Mbps.

#define CSITX_LANE_BAND_SPEED_240_TO_320_MBPS   ((uint32_t) 0x05U)

Lane Band Speed: 240 Mbps to 320 Mbps.

#define CSITX_LANE_BAND_SPEED_320_TO_390_MBPS   ((uint32_t) 0x06U)

Lane Band Speed: 320 Mbps to 390 Mbps.

#define CSITX_LANE_BAND_SPEED_390_TO_450_MBPS   ((uint32_t) 0x07U)

Lane Band Speed: 390 Mbps to 450 Mbps.

#define CSITX_LANE_BAND_SPEED_450_TO_510_MBPS   ((uint32_t) 0x08U)

Lane Band Speed: 450 Mbps to 520 Mbps.

#define CSITX_LANE_BAND_SPEED_510_TO_560_MBPS   ((uint32_t) 0x09U)

Lane Band Speed: 510 Mbps to 560 Mbps.

#define CSITX_LANE_BAND_SPEED_560_TO_640_MBPS   ((uint32_t) 0x0AU)

Lane Band Speed: 560 Mbps to 640 Mbps.

#define CSITX_LANE_BAND_SPEED_640_TO_690_MBPS   ((uint32_t) 0x0BU)

Lane Band Speed: 640 Mbps to 690 Mbps.

#define CSITX_LANE_BAND_SPEED_690_TO_770_MBPS   ((uint32_t) 0x0CU)

Lane Band Speed: 690 Mbps to 770 Mbps.

#define CSITX_LANE_BAND_SPEED_770_TO_870_MBPS   ((uint32_t) 0x0DU)

Lane Band Speed: 770 Mbps to 870 Mbps.

#define CSITX_LANE_BAND_SPEED_870_TO_950_MBPS   ((uint32_t) 0x0EU)

Lane Band Speed: 870 Mbps to 950 Mbps.

#define CSITX_LANE_BAND_SPEED_950_TO_1000_MBPS   ((uint32_t) 0x0FU)

Lane Band Speed: 950 Mbps to 1000 Mbps.

#define CSITX_LANE_BAND_SPEED_1000_TO_1200_MBPS   ((uint32_t) 0x10U)

Lane Band Speed: 1000 Mbps to 1200 Mbps.

#define CSITX_LANE_BAND_SPEED_1200_TO_1400_MBPS   ((uint32_t) 0x11U)

Lane Band Speed: 1200 Mbps to 1400 Mbps.

#define CSITX_LANE_BAND_SPEED_1400_TO_1600_MBPS   ((uint32_t) 0x12U)

Lane Band Speed: 1400 Mbps to 1600 Mbps.

#define CSITX_LANE_BAND_SPEED_1600_TO_1800_MBPS   ((uint32_t) 0x13U)

Lane Band Speed: 1600 Mbps to 1800 Mbps.

#define CSITX_LANE_BAND_SPEED_1800_TO_2000_MBPS   ((uint32_t) 0x14U)

Lane Band Speed: 1800 Mbps to 2000 Mbps.

#define CSITX_LANE_BAND_SPEED_2000_TO_2200_MBPS   ((uint32_t) 0x15U)

Lane Band Speed: 2000 Mbps to 2200 Mbps.

#define CSITX_LANE_BAND_SPEED_2200_TO_2500_MBPS   ((uint32_t) 0x16U)

Lane Band Speed: 2200 Mbps to 2500 Mbps.

#define CSITX_LANE_BAND_SPEED_RESERVED   ((uint32_t) 0x17U)

Lane Band Speed: Reserved.

#define CSITX_CLK_MODE_CONTINUOUS   ((uint32_t) 0x0U)

DPHY Clock Mode: Continuous.

#define CSITX_CLK_MODE_NON_CONTINUOUS   ((uint32_t) 0x1U)

DPHY Clock Mode: Non-continuous.

#define CSITX_DPHY_MODE_ULP   ((uint32_t) 0x0U)

DPHY Clock Mode: ultra low power.

#define CSITX_DPHY_MODE_HIGH_SPEED   ((uint32_t) 0x1U)

DPHY Clock Mode: high speed.

#define CSITX_DPHY_MODE_LOW_POWER   ((uint32_t) 0x2U)

DPHY Clock Mode: low power stop state.

#define CSITX_NUM_STREAM   (1U)

CSITX DRV Numbers: Number of stream per CSI TX module.

#define CSITX_STREAM_ID_INST_0_STRM_0   ((uint32_t) 0x0U)

CSITX Instance ID: transmit stream0 0 on CSI2TX Module 0.

#define CSITX_STREAM_ID_INST_0_STRM_1   ((uint32_t) 0x1U)

CSITX Instance ID: Color-bar stream on CSI2TX Module 0.

#define CSITX_STREAM_ID_INST_0_STRM_2   ((uint32_t) 0x2U)

CSITX Instance ID: CSI2RX loop-back 0 on CSI2TX Module 0.

#define CSITX_STREAM_ID_INST_0_STRM_3   ((uint32_t) 0x3U)

CSITX Instance ID: CSI2RX loop-back 1 on CSI2TX Module 0.

Function Documentation

void Csitx_initDPhyCfgParams ( Csitx_DPhyCfg dphyCfg)

Csitx_DPhyCfg structure init function.

Parameters
dphyCfg[IN] Pointer to Csitx_DPhyCfg structure.

Note: If given 'dphyCfg.laneBandSpeed' does no match with pre-defined configurations, this API will default the DPHY parameters for 800 Mbps. Application should change the DPHY parameters (if needed) prior to calling 'Fvid2_create()'. Pre-defined configurations are supported for following lane-speeds:

  1. CSITX_LANE_BAND_SPEED_770_TO_870_MBPS
  2. CSITX_LANE_BAND_SPEED_1000_TO_1200_MBPS
  3. CSITX_LANE_BAND_SPEED_1400_TO_1600_MBPS
  4. CSITX_LANE_BAND_SPEED_2200_TO_2500_MBPS