PDK API Guide for J721E
|
This is documentation for CSIRX driver configuration.
Files | |
file | csirx_cfg.h |
CSIRX Driver configuration file. | |
Macros | |
#define | CsirxTrace |
Log enable for CSIRX module. More... | |
#define | CSIRX_DRV_ENABLE_DEBUG (0U) |
Enable logging for debug purpose. Set to '1' to enable debug logging. More... | |
#define | CSIRX_DRV_LOG_CNT (2000U) |
Number of entries to log for debug. More... | |
CSIRX Create Default configurations. | |
Default values for create time parameters. See Csirx_CreateParams for details | |
#define | CSIRX_NUM_CH (CSIRX_NUM_CH_MAX) |
Number of Channels: Maximum number of channels for configuration. More... | |
#define | CSIRX_CH_ID_DEFAULT ((uint32_t) 0x00U) |
Channel ID: Default channel ID used for initialization. More... | |
#define | CSIRX_VC_NUM_DEFAULT ((uint32_t) 0x00U) |
Virtual Channel ID: Default virtual channel ID used for initialization. More... | |
#define | CSIRX_IN_DT_DEFAULT (FVID2_CSI2_DF_RGB888) |
Frame Width: Default frame width used for initialization. More... | |
#define | CSIRX_CAPT_QUEUE_DEPTH_PER_CH ((uint32_t)10U) |
Default max number of frames that can be queued per capture driver instance. More... | |
#define | CSIRX_TIMEOUT_VAL_MS ((uint32_t)10U) |
Time out value: Time-out value in ms. More... | |
#define CSIRX_NUM_CH (CSIRX_NUM_CH_MAX) |
Number of Channels: Maximum number of channels for configuration.
#define CSIRX_CH_ID_DEFAULT ((uint32_t) 0x00U) |
Channel ID: Default channel ID used for initialization.
#define CSIRX_VC_NUM_DEFAULT ((uint32_t) 0x00U) |
Virtual Channel ID: Default virtual channel ID used for initialization.
#define CSIRX_IN_DT_DEFAULT (FVID2_CSI2_DF_RGB888) |
Frame Width: Default frame width used for initialization.
#define CSIRX_CAPT_QUEUE_DEPTH_PER_CH ((uint32_t)10U) |
Default max number of frames that can be queued per capture driver instance.
#define CSIRX_TIMEOUT_VAL_MS ((uint32_t)10U) |
Time out value: Time-out value in ms.
#define CsirxTrace |
Log enable for CSIRX module.
#define CSIRX_DRV_ENABLE_DEBUG (0U) |
Enable logging for debug purpose. Set to '1' to enable debug logging.
#define CSIRX_DRV_LOG_CNT (2000U) |
Number of entries to log for debug.