PDK API Guide for J721E
CSIRX Configuration and Hardware Operation Information

Introduction

The following definitions specify the driver operation environment that is defined by hardware configuration or client code. These defines are located in the header file of the core driver.

Macros

#define CSIRX_MAX_NUM_OF_STREAMS   (0x4U)
 
#define CSIRX_MAGIC_NUMBER   0x50220200U
 

Macro Definition Documentation

#define CSIRX_MAX_NUM_OF_STREAMS   (0x4U)
#define CSIRX_MAGIC_NUMBER   0x50220200U

Magic number value