PDK API Guide for J721E
DSS Common CSL FL

Introduction

Files

file  csl_dssCommon.h
 DSS Common CSL FL interface file.
 

Data Structures

struct  CSL_DssGlobalMFlagCfg
 DSS Global MFLAG Config parameters. More...
 
struct  CSL_DssCbaCfg
 DSS CBA Config parameters. More...
 

Functions

void CSL_dssModuleReset (CSL_dss_commRegs *commRegs)
 Reset the DSS Module. Application should make sure Video Ports are disabled before calling this API. More...
 
void CSL_dssEnableDispcIntr (CSL_dss_commRegs *commRegs, uint32_t intrMask, uint32_t intrEnable)
 Enable/disable the interrupts at DSS top level. More...
 
void CSL_dssEnablePipeIntr (CSL_dss_commRegs *commRegs, uint32_t vidPipeId, uint32_t intrMask, uint32_t intrEnable)
 Enable/disable the interrupts for Video Pipe. More...
 
void CSL_dssEnableVpIntr (CSL_dss_commRegs *commRegs, uint32_t portId, uint32_t intrMask, uint32_t intrEnable)
 Enable/disable the interrupts for Video Port. More...
 
void CSL_dssEnableWbIntr (CSL_dss_commRegs *commRegs, uint32_t wbPipeId, uint32_t intrMask, uint32_t intrEnable)
 Enable/disable the interrupts for Write Back Pipe. More...
 
void CSL_dssClearDispcIntr (CSL_dss_commRegs *commRegs, uint32_t intrMask)
 Clear the interrupts at DSS top level. More...
 
void CSL_dssClearPipeIntr (CSL_dss_commRegs *commRegs, uint32_t vidPipeId, uint32_t intrMask)
 Clear the interrupts for Video Pipe. More...
 
void CSL_dssClearVpIntr (CSL_dss_commRegs *commRegs, uint32_t portId, uint32_t intrMask)
 Clear the interrupts for Video Port. More...
 
void CSL_dssClearWbIntr (CSL_dss_commRegs *commRegs, uint32_t wbPipeId, uint32_t intrMask)
 Clear the interrupts for Write Back Pipe. More...
 
uint32_t CSL_dssGetDispcIntrStatus (const CSL_dss_commRegs *commRegs)
 Get the top level interrupt status of DSS. More...
 
uint32_t CSL_dssGetPipeIntrStatus (const CSL_dss_commRegs *commRegs, uint32_t vidPipeId)
 Get the interrupt status of Video Pipe. More...
 
uint32_t CSL_dssGetVpIntrStatus (const CSL_dss_commRegs *commRegs, uint32_t portId)
 Get the interrupt status of Video Port. More...
 
uint32_t CSL_dssGetWbIntrStatus (const CSL_dss_commRegs *commRegs, uint32_t wbPipeId)
 Get the interrupt status of Write Back Pipe. More...
 
void CSL_dssSetGlobalMflagConfig (CSL_dss_commRegs *commRegs, const CSL_DssGlobalMFlagCfg *mflagCfg)
 Set the global MFLAG configuration. More...
 
void CSL_dssGlobalVpEnable (CSL_dss_commRegs *commRegs, uint32_t portIdMask, uint32_t enable)
 Enable the global VP enable bit. This allows setting multiple outputs synchronously. The 'OR' result of different masks can be used as input parameter. More...
 
void CSL_dssGlobalVpGoBitEnable (CSL_dss_commRegs *commRegs, uint32_t portIdMask)
 Enable the global VP go bit. This allows setting multiple outputs synchronously. The 'OR' result of different masks can be used as input parameter. More...
 
void CSL_dssSetCbaConfig (CSL_dss_commRegs *commRegs, const CSL_DssCbaCfg *cbaCfg)
 Set the CBA configuration. More...
 
int32_t CSL_dssConnectVpToDpi (CSL_dss_commRegs *commRegs, uint32_t portId, uint32_t dpiId)
 This API can be used to select the VP connection to DPI. More...
 
void CSL_dssSetWbInputCh (CSL_dss_commRegs *commRegs, uint32_t inputCh)
 This API is used to set the write back input channel. More...
 
static void CSL_dssGlobalMFlagCfgInit (CSL_DssGlobalMFlagCfg *mflagCfg)
 CSL_DssGlobalMFlagCfg structure init function. More...
 
static void CSL_dssCbaCfgInit (CSL_DssCbaCfg *cbaCfg)
 CSL_DssCbaCfg structure init function. More...
 

Typedefs

typedef CSL_dss_common_mRegs CSL_dss_commRegs
 DSS Common Registers. More...
 

DISPC Interrupt Mask

#define CSL_DSS_DISPC_INTR_WB_MASK   ((uint32_t) 0x4000U)
 Write Back Pipeline Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VIDL2_MASK   ((uint32_t) 0x80U)
 Video Lite Pipeline 2 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VID2_MASK   ((uint32_t) 0x40U)
 Video PipeLine 2 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VIDL1_MASK   ((uint32_t) 0x20U)
 Video Lite Pipeline 1 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VID1_MASK   ((uint32_t) 0x10U)
 Video PipeLine 1 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VP4_MASK   ((uint32_t) 0x08U)
 Video Port 4 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VP3_MASK   ((uint32_t) 0x04U)
 Video Port 3 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VP2_MASK   ((uint32_t) 0x02U)
 Video Port 2 Interrupt. More...
 
#define CSL_DSS_DISPC_INTR_VP1_MASK   ((uint32_t) 0x01U)
 Video Port 1 Interrupt. More...
 

Video Pipeline Interrupt Mask

#define CSL_DSS_VID_PIPE_INTR_FBDC_ILLEGALTILE_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_FBDC_ILLEGALTILEREQ_EN_MASK)
 Interrupt due to FBDC illegal tile request. More...
 
#define CSL_DSS_VID_PIPE_INTR_FBDC_CORRUPTTILE_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_FBDC_CORRUPTTILE_EN_MASK)
 Interrupt due to FBDC corrupted tile detection. More...
 
#define CSL_DSS_VID_PIPE_INTR_SAFETYVIOLATION_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_SAFETYREGION_EN_MASK)
 Interrupt due to safety violation. More...
 
#define CSL_DSS_VID_PIPE_INTR_WINDOWEND_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_VIDENDWINDOW_EN_MASK)
 Interrupt due to video window end. More...
 
#define CSL_DSS_VID_PIPE_INTR_BUFUNDERFLOW_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_VIDBUFFERUNDERFLOW_EN_MASK)
 Interrupt due to buffer underflow. More...
 
#define CSL_DSS_VID_PIPE_INTR_ALL_MASK
 All Video Pipe interrupts. More...
 

Video Port Interrupt Mask

#define CSL_DSS_VP_INTR_FRAMEDONE_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPFRAMEDONE_EN_MASK)
 Frame Done for Video Port. More...
 
#define CSL_DSS_VP_INTR_VSYNC_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPVSYNC_EN_MASK)
 Vertical Synchronization for Video Port. More...
 
#define CSL_DSS_VP_INTR_ODDVSYNC_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPVSYNC_ODD_EN_MASK)
 VSYNC for odd field from interlace mode only. More...
 
#define CSL_DSS_VP_INTR_PROGLINENUM_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPPROGRAMMEDLINENUMBER_EN_MASK)
 Display scan has reached the programmed user line number. More...
 
#define CSL_DSS_VP_INTR_SYNCLOST_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPSYNCLOST_EN_MASK)
 Synchronization Lost for Video Port. More...
 
#define CSL_DSS_VP_INTR_ACBIASCOUNT_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_ACBIASCOUNTSTATUS_EN_MASK)
 AC Bias transition counter has decremented to zero. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION0_MASK   ((uint32_t) 0x40U)
 Interrupt due to region 0 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION1_MASK   ((uint32_t) 0x80U)
 Interrupt due to region 1 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION2_MASK   ((uint32_t) 0x100U)
 Interrupt due to region 2 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION3_MASK   ((uint32_t) 0x200U)
 Interrupt due to region 3 safety violation. More...
 
#define CSL_DSS_VP_INTR_SECURITYVIOLATION_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_SECURITYVIOLATION_EN_MASK)
 Interrupt due to security violation. More...
 
#define CSL_DSS_VP_INTR_GOBITCLEAR_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPSYNC_EN_MASK)
 Go bit clear interrupt for VP. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION4_MASK   ((uint32_t) 0x2000U)
 Interrupt due to region 4 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION5_MASK   ((uint32_t) 0x4000U)
 Interrupt due to region 5 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION6_MASK   ((uint32_t) 0x8000U)
 Interrupt due to region 6 safety violation. More...
 
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION7_MASK   ((uint32_t) 0x10000U)
 Interrupt due to region 7 safety violation. More...
 
#define CSL_DSS_VP_INTR_ALL_MASK
 All Video Port interrupts. More...
 

Write back Pipeline Interrupt Mask

#define CSL_DSS_WB_PIPE_INTR_WBSYNC_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_WBSYNC_EN_MASK)
 Interrupt due to completion of write back sync. More...
 
#define CSL_DSS_WB_PIPE_INTR_SECURITYVIOLATION_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_SECURITYVIOLATION_EN_MASK)
 Interrupt due to security violation. More...
 
#define CSL_DSS_WB_PIPE_INTR_FRAMEDONE_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_WBFRAMEDONE_EN_MASK)
 Interrupt due to write back frame completion. More...
 
#define CSL_DSS_WB_PIPE_INTR_INCOMPLETE_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_WBUNCOMPLETEERROR_EN_MASK)
 Interrupt due to buffer flush before full drain (Only Capture WB) More...
 
#define CSL_DSS_WB_PIPE_INTR_OVERFLOW_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_WBBUFFEROVERFLOW_EN_MASK)
 Interrupt due to buffer overflow. More...
 
#define CSL_DSS_WB_PIPE_INTR_ALL_MASK
 All Write Back Pipe interrupts. More...
 

Mflag Start Mode

#define CSL_DSS_MFLAG_START_NORMAL   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_START_VAL_MFLAGNORMALSTARTMODE)
 Mflag of each pipe is kept at 0 until preload is reached. More...
 
#define CSL_DSS_MFLAG_START_FORCED   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_START_VAL_MFLAGFORCESTARTMODE)
 Mflag is driven as per Mflag Ctrl. More...
 

Mflag Control

#define CSL_DSS_MFLAG_CTRL_DISABLED   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGDIS)
 Mflag is disabled. More...
 
#define CSL_DSS_MFLAG_CTRL_FORCE_ENABLE   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGFORCE)
 Mflag is force enabled. More...
 
#define CSL_DSS_MFLAG_CTRL_DYNAMIC   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGEN)
 Mflag signal is set dynamically as per rules. More...
 

Write back input channel.

#define CSL_DSS_WB_INPUT_DISABLED   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_NULL)
 Write back input is disabled. More...
 
#define CSL_DSS_WB_INPUT_VIDL2   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_VIDL2)
 Write back input is VIDL2. More...
 
#define CSL_DSS_WB_INPUT_OVERLAY1   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_OVR1)
 Write back input is overlay 1. More...
 
#define CSL_DSS_WB_INPUT_OVERLAY2   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_OVR2)
 Write back input is overlay 2. More...
 
#define CSL_DSS_WB_INPUT_OVERLAY3   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_OVR3)
 Write back input is overlay 3. More...
 
#define CSL_DSS_WB_INPUT_OVERLAY4   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_OVR4)
 Write back input is overlay 4. More...
 

Macro Definition Documentation

#define CSL_DSS_DISPC_INTR_WB_MASK   ((uint32_t) 0x4000U)

Write Back Pipeline Interrupt.

#define CSL_DSS_DISPC_INTR_VIDL2_MASK   ((uint32_t) 0x80U)

Video Lite Pipeline 2 Interrupt.

#define CSL_DSS_DISPC_INTR_VID2_MASK   ((uint32_t) 0x40U)

Video PipeLine 2 Interrupt.

#define CSL_DSS_DISPC_INTR_VIDL1_MASK   ((uint32_t) 0x20U)

Video Lite Pipeline 1 Interrupt.

#define CSL_DSS_DISPC_INTR_VID1_MASK   ((uint32_t) 0x10U)

Video PipeLine 1 Interrupt.

#define CSL_DSS_DISPC_INTR_VP4_MASK   ((uint32_t) 0x08U)

Video Port 4 Interrupt.

#define CSL_DSS_DISPC_INTR_VP3_MASK   ((uint32_t) 0x04U)

Video Port 3 Interrupt.

#define CSL_DSS_DISPC_INTR_VP2_MASK   ((uint32_t) 0x02U)

Video Port 2 Interrupt.

#define CSL_DSS_DISPC_INTR_VP1_MASK   ((uint32_t) 0x01U)

Video Port 1 Interrupt.

#define CSL_DSS_VID_PIPE_INTR_FBDC_ILLEGALTILE_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_FBDC_ILLEGALTILEREQ_EN_MASK)

Interrupt due to FBDC illegal tile request.

#define CSL_DSS_VID_PIPE_INTR_FBDC_CORRUPTTILE_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_FBDC_CORRUPTTILE_EN_MASK)

Interrupt due to FBDC corrupted tile detection.

#define CSL_DSS_VID_PIPE_INTR_SAFETYVIOLATION_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_SAFETYREGION_EN_MASK)

Interrupt due to safety violation.

#define CSL_DSS_VID_PIPE_INTR_WINDOWEND_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_VIDENDWINDOW_EN_MASK)

Interrupt due to video window end.

#define CSL_DSS_VID_PIPE_INTR_BUFUNDERFLOW_MASK   ((uint32_t) CSL_DSS_COMMON_M_VID_IRQENABLE_0_VIDBUFFERUNDERFLOW_EN_MASK)

Interrupt due to buffer underflow.

#define CSL_DSS_VID_PIPE_INTR_ALL_MASK
Value:
#define CSL_DSS_VID_PIPE_INTR_BUFUNDERFLOW_MASK
Interrupt due to buffer underflow.
Definition: csl_dssCommon.h:116
#define CSL_DSS_VID_PIPE_INTR_FBDC_CORRUPTTILE_MASK
Interrupt due to FBDC corrupted tile detection.
Definition: csl_dssCommon.h:107
#define CSL_DSS_VID_PIPE_INTR_SAFETYVIOLATION_MASK
Interrupt due to safety violation.
Definition: csl_dssCommon.h:110
#define CSL_DSS_VID_PIPE_INTR_FBDC_ILLEGALTILE_MASK
Interrupt due to FBDC illegal tile request.
Definition: csl_dssCommon.h:104
#define CSL_DSS_VID_PIPE_INTR_WINDOWEND_MASK
Interrupt due to video window end.
Definition: csl_dssCommon.h:113

All Video Pipe interrupts.

#define CSL_DSS_VP_INTR_FRAMEDONE_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPFRAMEDONE_EN_MASK)

Frame Done for Video Port.

#define CSL_DSS_VP_INTR_VSYNC_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPVSYNC_EN_MASK)

Vertical Synchronization for Video Port.

#define CSL_DSS_VP_INTR_ODDVSYNC_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPVSYNC_ODD_EN_MASK)

VSYNC for odd field from interlace mode only.

#define CSL_DSS_VP_INTR_PROGLINENUM_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPPROGRAMMEDLINENUMBER_EN_MASK)

Display scan has reached the programmed user line number.

#define CSL_DSS_VP_INTR_SYNCLOST_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPSYNCLOST_EN_MASK)

Synchronization Lost for Video Port.

#define CSL_DSS_VP_INTR_ACBIASCOUNT_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_ACBIASCOUNTSTATUS_EN_MASK)

AC Bias transition counter has decremented to zero.

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION0_MASK   ((uint32_t) 0x40U)

Interrupt due to region 0 safety violation.

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION1_MASK   ((uint32_t) 0x80U)

Interrupt due to region 1 safety violation.

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION2_MASK   ((uint32_t) 0x100U)

Interrupt due to region 2 safety violation.

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION3_MASK   ((uint32_t) 0x200U)

Interrupt due to region 3 safety violation.

#define CSL_DSS_VP_INTR_SECURITYVIOLATION_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_SECURITYVIOLATION_EN_MASK)

Interrupt due to security violation.

#define CSL_DSS_VP_INTR_GOBITCLEAR_MASK   ((uint32_t) CSL_DSS_COMMON_M_VP_IRQENABLE_0_VPSYNC_EN_MASK)

Go bit clear interrupt for VP.

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION4_MASK   ((uint32_t) 0x2000U)

Interrupt due to region 4 safety violation.

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION5_MASK   ((uint32_t) 0x4000U)

Interrupt due to region 5 safety violation.

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION6_MASK   ((uint32_t) 0x8000U)

Interrupt due to region 6 safety violation.

#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION7_MASK   ((uint32_t) 0x10000U)

Interrupt due to region 7 safety violation.

#define CSL_DSS_VP_INTR_ALL_MASK
Value:
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION1_MASK
Interrupt due to region 1 safety violation.
Definition: csl_dssCommon.h:155
#define CSL_DSS_VP_INTR_FRAMEDONE_MASK
Frame Done for Video Port.
Definition: csl_dssCommon.h:134
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION0_MASK
Interrupt due to region 0 safety violation.
Definition: csl_dssCommon.h:152
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION6_MASK
Interrupt due to region 6 safety violation.
Definition: csl_dssCommon.h:176
#define CSL_DSS_VP_INTR_SYNCLOST_MASK
Synchronization Lost for Video Port.
Definition: csl_dssCommon.h:146
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION3_MASK
Interrupt due to region 3 safety violation.
Definition: csl_dssCommon.h:161
#define CSL_DSS_VP_INTR_GOBITCLEAR_MASK
Go bit clear interrupt for VP.
Definition: csl_dssCommon.h:167
#define CSL_DSS_VP_INTR_ACBIASCOUNT_MASK
AC Bias transition counter has decremented to zero.
Definition: csl_dssCommon.h:149
#define CSL_DSS_VP_INTR_PROGLINENUM_MASK
Display scan has reached the programmed user line number.
Definition: csl_dssCommon.h:143
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION5_MASK
Interrupt due to region 5 safety violation.
Definition: csl_dssCommon.h:173
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION4_MASK
Interrupt due to region 4 safety violation.
Definition: csl_dssCommon.h:170
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION7_MASK
Interrupt due to region 7 safety violation.
Definition: csl_dssCommon.h:179
#define CSL_DSS_VP_INTR_ODDVSYNC_MASK
VSYNC for odd field from interlace mode only.
Definition: csl_dssCommon.h:140
#define CSL_DSS_VP_INTR_SECURITYVIOLATION_MASK
Interrupt due to security violation.
Definition: csl_dssCommon.h:164
#define CSL_DSS_VP_INTR_VSYNC_MASK
Vertical Synchronization for Video Port.
Definition: csl_dssCommon.h:137
#define CSL_DSS_VP_INTR_SAFETYVIOLATION_REGION2_MASK
Interrupt due to region 2 safety violation.
Definition: csl_dssCommon.h:158

All Video Port interrupts.

#define CSL_DSS_WB_PIPE_INTR_WBSYNC_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_WBSYNC_EN_MASK)

Interrupt due to completion of write back sync.

#define CSL_DSS_WB_PIPE_INTR_SECURITYVIOLATION_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_SECURITYVIOLATION_EN_MASK)

Interrupt due to security violation.

#define CSL_DSS_WB_PIPE_INTR_FRAMEDONE_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_WBFRAMEDONE_EN_MASK)

Interrupt due to write back frame completion.

#define CSL_DSS_WB_PIPE_INTR_INCOMPLETE_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_WBUNCOMPLETEERROR_EN_MASK)

Interrupt due to buffer flush before full drain (Only Capture WB)

#define CSL_DSS_WB_PIPE_INTR_OVERFLOW_MASK   ((uint32_t) CSL_DSS_COMMON_M_WB_IRQENABLE_WBBUFFEROVERFLOW_EN_MASK)

Interrupt due to buffer overflow.

#define CSL_DSS_WB_PIPE_INTR_ALL_MASK
Value:
CSL_DSS_WB_PIPE_INTR_UNCOMPLETE_MASK | \
#define CSL_DSS_WB_PIPE_INTR_SECURITYVIOLATION_MASK
Interrupt due to security violation.
Definition: csl_dssCommon.h:211
#define CSL_DSS_WB_PIPE_INTR_OVERFLOW_MASK
Interrupt due to buffer overflow.
Definition: csl_dssCommon.h:220
#define CSL_DSS_WB_PIPE_INTR_FRAMEDONE_MASK
Interrupt due to write back frame completion.
Definition: csl_dssCommon.h:214
#define CSL_DSS_WB_PIPE_INTR_WBSYNC_MASK
Interrupt due to completion of write back sync.
Definition: csl_dssCommon.h:208

All Write Back Pipe interrupts.

#define CSL_DSS_MFLAG_START_NORMAL   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_START_VAL_MFLAGNORMALSTARTMODE)

Mflag of each pipe is kept at 0 until preload is reached.

#define CSL_DSS_MFLAG_START_FORCED   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_START_VAL_MFLAGFORCESTARTMODE)

Mflag is driven as per Mflag Ctrl.

#define CSL_DSS_MFLAG_CTRL_DISABLED   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGDIS)

Mflag is disabled.

#define CSL_DSS_MFLAG_CTRL_FORCE_ENABLE   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGFORCE)

Mflag is force enabled.

#define CSL_DSS_MFLAG_CTRL_DYNAMIC   ((uint32_t) CSL_DSS_COMMON_M_DISPC_GLOBAL_MFLAG_ATTRIBUTE_MFLAG_CTRL_VAL_MFLAGEN)

Mflag signal is set dynamically as per rules.

#define CSL_DSS_WB_INPUT_DISABLED   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_NULL)

Write back input is disabled.

#define CSL_DSS_WB_INPUT_VIDL2   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_VIDL2)

Write back input is VIDL2.

#define CSL_DSS_WB_INPUT_OVERLAY1   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_OVR1)

Write back input is overlay 1.

#define CSL_DSS_WB_INPUT_OVERLAY2   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_OVR2)

Write back input is overlay 2.

#define CSL_DSS_WB_INPUT_OVERLAY3   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_OVR3)

Write back input is overlay 3.

#define CSL_DSS_WB_INPUT_OVERLAY4   ((uint32_t) CSL_DSS_COMMON_M_DISPC_CONNECTIONS_WB_CONN_VAL_OVR4)

Write back input is overlay 4.

Typedef Documentation

typedef CSL_dss_common_mRegs CSL_dss_commRegs

DSS Common Registers.

DSS7 has four common blocks, hence define a generic structure to have common APIs

Function Documentation

void CSL_dssModuleReset ( CSL_dss_commRegs commRegs)

Reset the DSS Module. Application should make sure Video Ports are disabled before calling this API.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
Returns
None
void CSL_dssEnableDispcIntr ( CSL_dss_commRegs commRegs,
uint32_t  intrMask,
uint32_t  intrEnable 
)

Enable/disable the interrupts at DSS top level.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
intrMaskInterrupt Mask. Refer CSL_DssDispcIntrMask for values
intrEnableEnable/Disable the interrupt TRUE: Enable interrupt FALSE: Disable interrupt
Returns
None
void CSL_dssEnablePipeIntr ( CSL_dss_commRegs commRegs,
uint32_t  vidPipeId,
uint32_t  intrMask,
uint32_t  intrEnable 
)

Enable/disable the interrupts for Video Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
vidPipeIdVideo Pipe for which interrupt should be configured. Valid Values: CSL_DSS_VID_PIPE_ID_VID1 CSL_DSS_VID_PIPE_ID_VIDL1 CSL_DSS_VID_PIPE_ID_VID2 CSL_DSS_VID_PIPE_ID_VIDL2
intrMaskInterrupt Mask. Refer CSL_DssVidPipeIntrMask for values
intrEnableEnable/Disable the interrupt TRUE: Enable interrupt FALSE: Disable interrupt
Returns
None
void CSL_dssEnableVpIntr ( CSL_dss_commRegs commRegs,
uint32_t  portId,
uint32_t  intrMask,
uint32_t  intrEnable 
)

Enable/disable the interrupts for Video Port.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdVideo Port for which interrupt should be configured. Valid Values: CSL_DSS_VP_ID_1 CSL_DSS_VP_ID_2 CSL_DSS_VP_ID_3 CSL_DSS_VP_ID_4
intrMaskInterrupt Mask. Refer CSL_DssVpIntrMask for values
intrEnableEnable/Disable the interrupt TRUE: Enable interrupt FALSE: Disable interrupt
Returns
None
void CSL_dssEnableWbIntr ( CSL_dss_commRegs commRegs,
uint32_t  wbPipeId,
uint32_t  intrMask,
uint32_t  intrEnable 
)

Enable/disable the interrupts for Write Back Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
wbPipeIdWrite back Pipe for which interrupt should be configured. Valid Values: CSL_DSS_WB_PIPE_ID_1
intrMaskInterrupt Mask. Refer CSL_DssWbPipeIntrMask for values
intrEnableEnable/Disable the interrupt TRUE: Enable interrupt FALSE: Disable interrupt
Returns
None
void CSL_dssClearDispcIntr ( CSL_dss_commRegs commRegs,
uint32_t  intrMask 
)

Clear the interrupts at DSS top level.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
intrMaskInterrupt Mask. Refer CSL_DssDispcIntrMask for values
Returns
None
void CSL_dssClearPipeIntr ( CSL_dss_commRegs commRegs,
uint32_t  vidPipeId,
uint32_t  intrMask 
)

Clear the interrupts for Video Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
vidPipeIdVideo Pipe for which interrupt should be cleared. Valid Values: CSL_DSS_VID_PIPE_ID_VID1 CSL_DSS_VID_PIPE_ID_VIDL1 CSL_DSS_VID_PIPE_ID_VID2 CSL_DSS_VID_PIPE_ID_VIDL2
intrMaskInterrupt Mask. Refer CSL_DssVidPipeIntrMask for values
Returns
None
void CSL_dssClearVpIntr ( CSL_dss_commRegs commRegs,
uint32_t  portId,
uint32_t  intrMask 
)

Clear the interrupts for Video Port.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdVideo Port for which interrupt should be cleared. Valid Values: CSL_DSS_VP_ID_1 CSL_DSS_VP_ID_2 CSL_DSS_VP_ID_3 CSL_DSS_VP_ID_4
intrMaskInterrupt Mask. Refer CSL_DssVpIntrMask for values
Returns
None
void CSL_dssClearWbIntr ( CSL_dss_commRegs commRegs,
uint32_t  wbPipeId,
uint32_t  intrMask 
)

Clear the interrupts for Write Back Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
wbPipeIdWrite back Pipe for which interrupt should be cleared. Valid Values: CSL_DSS_WB_PIPE_ID_1
intrMaskInterrupt Mask. Refer CSL_DssWbPipeIntrMask for values
Returns
None
uint32_t CSL_dssGetDispcIntrStatus ( const CSL_dss_commRegs commRegs)

Get the top level interrupt status of DSS.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
Returns
Interrupt status
uint32_t CSL_dssGetPipeIntrStatus ( const CSL_dss_commRegs commRegs,
uint32_t  vidPipeId 
)

Get the interrupt status of Video Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
vidPipeIdVideo Pipe for which interrupt status should be read. Valid Values: CSL_DSS_VID_PIPE_ID_VID1 CSL_DSS_VID_PIPE_ID_VIDL1 CSL_DSS_VID_PIPE_ID_VID2 CSL_DSS_VID_PIPE_ID_VIDL2
Returns
Interrupt status
uint32_t CSL_dssGetVpIntrStatus ( const CSL_dss_commRegs commRegs,
uint32_t  portId 
)

Get the interrupt status of Video Port.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdVideo Port for which interrupt status should be read. Valid Values: CSL_DSS_VP_ID_1 CSL_DSS_VP_ID_2 CSL_DSS_VP_ID_3 CSL_DSS_VP_ID_4
Returns
Interrupt status
uint32_t CSL_dssGetWbIntrStatus ( const CSL_dss_commRegs commRegs,
uint32_t  wbPipeId 
)

Get the interrupt status of Write Back Pipe.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
wbPipeIdWrite Back Pipe for which interrupt status should be read. Valid Values: CSL_DSS_WB_PIPE_ID_1
Returns
Interrupt status
void CSL_dssSetGlobalMflagConfig ( CSL_dss_commRegs commRegs,
const CSL_DssGlobalMFlagCfg mflagCfg 
)

Set the global MFLAG configuration.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
mflagCfgPointer to CSL_DssGlobalMFlagCfg structure. This parameter should not be NULL
Returns
None
void CSL_dssGlobalVpEnable ( CSL_dss_commRegs commRegs,
uint32_t  portIdMask,
uint32_t  enable 
)

Enable the global VP enable bit. This allows setting multiple outputs synchronously. The 'OR' result of different masks can be used as input parameter.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdMaskVideo Port for which enable bit should be set. Refer CSL_DssVpIdMask for details.
enableEnable/Disable the ports TRUE: Enable ports synchronously FALSE: Disable ports synchronously
Returns
None
void CSL_dssGlobalVpGoBitEnable ( CSL_dss_commRegs commRegs,
uint32_t  portIdMask 
)

Enable the global VP go bit. This allows setting multiple outputs synchronously. The 'OR' result of different masks can be used as input parameter.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdMaskVideo Port for which go bit should be set. Refer CSL_DssVpIdMask for details.
Returns
None
void CSL_dssSetCbaConfig ( CSL_dss_commRegs commRegs,
const CSL_DssCbaCfg cbaCfg 
)

Set the CBA configuration.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
cbaCfgPointer to CSL_DssCbaCfg structure. This parameter should not be NULL
Returns
None
int32_t CSL_dssConnectVpToDpi ( CSL_dss_commRegs commRegs,
uint32_t  portId,
uint32_t  dpiId 
)

This API can be used to select the VP connection to DPI.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
portIdVideo Port Id. Possible values are: CSL_DSS_VP_ID_2 or CSL_DSS_VP_ID_4
dpiIdDPI Id. Possible values are: CSL_DSS_DPI_ID_DPI_0 or CSL_DSS_DPI_ID_DPI_1
Returns
CSL_ErrType_t
void CSL_dssSetWbInputCh ( CSL_dss_commRegs commRegs,
uint32_t  inputCh 
)

This API is used to set the write back input channel.

Parameters
commRegsPointer to a CSL_dss_commRegs structure containing the common configuration
inputChWrite back input channel. Refer CSL_DssWbInputCh for details.
Returns
None
static void CSL_dssGlobalMFlagCfgInit ( CSL_DssGlobalMFlagCfg mflagCfg)
inlinestatic

CSL_DssGlobalMFlagCfg structure init function.

Parameters
mflagCfgPointer to CSL_DssGlobalMFlagCfg structure
Returns
None
static void CSL_dssCbaCfgInit ( CSL_DssCbaCfg cbaCfg)
inlinestatic

CSL_DssCbaCfg structure init function.

Parameters
cbaCfgPointer to CSL_DssCbaCfg structure
Returns
None