PDK API Guide for J721E
DRU Enumerated Data Types

Introduction

Macros

#define CSL_DRU_MAX_CH   (512U)
 Maximum number of channels supported by DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_CH macro. More...
 
#define CSL_DRU_NUM_CH   (64U)
 Number of channels supported by the DRU. More...
 
#define CSL_DRU_MAX_QUEUE   (8U)
 Maximum number of queues supported by DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_QUEUE macro. More...
 
#define CSL_DRU_NUM_QUEUE   (5U)
 Number of queues supported by the DRU. More...
 
#define CSL_DRU_MAX_CORE   (4U)
 Maximum number of core submission set supported by the DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_CORE macro. More...
 
#define CSL_DRU_NUM_CORE   (3U)
 Number of core submission set supported by the DRU. More...
 

DRU Owner - Direct TR submission or UDMA-C TR submission

DRU owner.

#define CSL_DRU_OWNER_DIRECT_TR   ((uint64_t) 0x0000U)
 Direct TR - SUBMISSION registers must be written to submit TR. More...
 
#define CSL_DRU_OWNER_UDMAC_TR   ((uint64_t) 0x0001U)
 UDMA-C TR - TR will be received through PSIL. More...
 

DRU Queue ID

DRU queue ID. 0th queue is a priority queue. All others are round robin queues.

#define CSL_DRU_QUEUE_ID_0   ((uint32_t) 0x0000U)
 
#define CSL_DRU_QUEUE_ID_1   ((uint32_t) 0x0001U)
 
#define CSL_DRU_QUEUE_ID_2   ((uint32_t) 0x0002U)
 
#define CSL_DRU_QUEUE_ID_3   ((uint32_t) 0x0003U)
 
#define CSL_DRU_QUEUE_ID_4   ((uint32_t) 0x0004U)
 
#define CSL_DRU_QUEUE_ID_5   ((uint32_t) 0x0005U)
 
#define CSL_DRU_QUEUE_ID_6   ((uint32_t) 0x0006U)
 
#define CSL_DRU_QUEUE_ID_7   ((uint32_t) 0x0007U)
 

DRU Core ID

DRU core ID used to submit non-atomic TR submission. Note: There are only three core ID set present in the AM65xx and J721E SOC.

#define CSL_DRU_CORE_ID_0   ((uint32_t) 0x0000U)
 
#define CSL_DRU_CORE_ID_1   ((uint32_t) 0x0001U)
 
#define CSL_DRU_CORE_ID_2   ((uint32_t) 0x0002U)
 
#define CSL_DRU_CORE_ID_3   ((uint32_t) 0x0003U)
 

Macro Definition Documentation

#define CSL_DRU_MAX_CH   (512U)

Maximum number of channels supported by DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_CH macro.

#define CSL_DRU_NUM_CH   (64U)

Number of channels supported by the DRU.

#define CSL_DRU_MAX_QUEUE   (8U)

Maximum number of queues supported by DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_QUEUE macro.

#define CSL_DRU_NUM_QUEUE   (5U)

Number of queues supported by the DRU.

#define CSL_DRU_MAX_CORE   (4U)

Maximum number of core submission set supported by the DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_CORE macro.

#define CSL_DRU_NUM_CORE   (3U)

Number of core submission set supported by the DRU.

#define CSL_DRU_OWNER_DIRECT_TR   ((uint64_t) 0x0000U)

Direct TR - SUBMISSION registers must be written to submit TR.

#define CSL_DRU_OWNER_UDMAC_TR   ((uint64_t) 0x0001U)

UDMA-C TR - TR will be received through PSIL.

#define CSL_DRU_QUEUE_ID_0   ((uint32_t) 0x0000U)
#define CSL_DRU_QUEUE_ID_1   ((uint32_t) 0x0001U)
#define CSL_DRU_QUEUE_ID_2   ((uint32_t) 0x0002U)
#define CSL_DRU_QUEUE_ID_3   ((uint32_t) 0x0003U)
#define CSL_DRU_QUEUE_ID_4   ((uint32_t) 0x0004U)
#define CSL_DRU_QUEUE_ID_5   ((uint32_t) 0x0005U)
#define CSL_DRU_QUEUE_ID_6   ((uint32_t) 0x0006U)
#define CSL_DRU_QUEUE_ID_7   ((uint32_t) 0x0007U)
#define CSL_DRU_CORE_ID_0   ((uint32_t) 0x0000U)
#define CSL_DRU_CORE_ID_1   ((uint32_t) 0x0001U)
#define CSL_DRU_CORE_ID_2   ((uint32_t) 0x0002U)
#define CSL_DRU_CORE_ID_3   ((uint32_t) 0x0003U)