PDK API Guide for J721E
|
Data Structures | |
struct | Board_FlashInfo |
This structure contains information about the flash device on the board. More... | |
Typedefs | |
typedef uintptr_t | Board_flashHandle |
This type defines the opaque handle returned to a flash device that is opened. The handle must be used in all subsequent operations. More... | |
typedef int32_t | Board_flash_STATUS |
Enumerations | |
enum | Board_flashNorPeriType { BOARD_FLASH_NOR_SPI = 0, BOARD_FLASH_NOR_QSPI, BOARD_FLASH_NOR_GPMC, BOARD_FLASH_NOR_OSPI, BOARD_FLASH_NOR_HPF, BOARD_FLASH_NOR_INTF_MAX } |
Board specific Flash Device Identifiers. More... | |
enum | Board_flashNandPeriType { BOARD_FLASH_NAND_GPMC = 0, BOARD_FLASH_NAND_EMIF16, BOARD_FLASH_NAND_INTF_MAX } |
Indicates the type of NAND flash peripheral. More... | |
enum | Board_flashType { BOARD_FLASH_NAND, BOARD_FLASH_NOR, BOARD_FLASH_EEPROM, BOARD_FLASH_SD, BOARD_FLASH_EMMC, BOARD_FLASH_QSPI_FLASH, BOARD_FLASH_MAX } |
Indicates the type of device. More... | |
enum | Board_flashQspiIoMode { BOARD_FLASH_QSPI_IO_MODE_SINGLE, BOARD_FLASH_QSPI_IO_MODE_DUAL, BOARD_FLASH_QSPI_IO_MODE_QUAD } |
Options to set qspi flash read/write access mode. More... | |
#define BOARD_FLASH_EINVALID -3 |
Board Flash API return type Error code for invalid parameters
#define BOARD_FLASH_EUNSUPPORTED -2 |
Error code for unsupported feature
#define BOARD_FLASH_EFAIL -1 |
General failure code
#define BOARD_FLASH_EOK 0 |
General success code
#define BOARD_FLASH_ID_MT29F1G08ABCHC 0x2CA1 |
Device Identifiers. These are used in the Open call to allow access to a specific memory device.
128MB NAND Flash
#define BOARD_FLASH_ID_NAND512R3A2D 0x2036 |
64MB NAND Flash
#define BOARD_FLASH_ID_MT29F4G08ABADA 0x2CDC |
512MB NAND Flash
#define BOARD_FLASH_ID_MT29F16G08ADBCAH4C 0x2CA5 |
16Gb,1.8v,x8
#define BOARD_FLASH_ID_MT29F2G16ABAFA 0x2CCA |
2Gb, x16, 3.3V
#define BOARD_FLASH_ID_NORN25Q128 0xBB18 |
16MB NOR Flash
#define BOARD_FLASH_ID_NORN25Q128A13ESF40F 0xBA18 |
16MB, 3.3v NOR Flash
#define BOARD_FLASH_ID_W25X32VSFIG 0x4016 |
w25x32 SPI Flash Device ID
#define BOARD_FLASH_ID_NORN25Q032A 0xBB16 |
4MB NOR Flash
#define BOARD_FLASH_ID_EEPROM50 0x50 |
EEPROM @ slave address 0x50
#define BOARD_FLASH_ID_EEPROM51 0x51 |
EEPROM @ slave address 0x51
#define BOARD_FLASH_ID_EMMC 0xFF00 |
eMMC device Id
#define BOARD_FLASH_ID_SD 0xFF01 |
Micro SD device Id
#define BOARD_FLASH_ID_QSPIFLASH_S25FL512S 0x0220 |
QSPI flash device Id - S25FL512S
#define BOARD_FLASH_ID_QSPIFLASH_S25FL256S 0x0219 |
QSPI flash device Id - S25FL256S
#define BOARD_FLASH_ID_S25FL512S (0x0220U) |
Spansion 64MB NOR flash
#define BOARD_FLASH_ID_S25FL256S (0x0219U) |
Spansion 32MB NOR flash
#define BOARD_FLASH_ID_MT29W160EB (0x2249U) |
Micron 2MB NOR flash
#define BOARD_FLASH_ID_MT29F4G08ABAEAWP (0xDC90U) |
Micron 512MB NAND flash
#define BOARD_FLASH_ID_MT35XU512ABA1G12 (0x5B1AU) |
Micro 512Mb NOR flash device Id
#define BOARD_FLASH_ID_MT35XU256ABA1G12 (0x5B19U) |
Micro 256Mb NOR flash device Id
#define BOARD_FLASH_ID_MT25QU512ABB (0xBB20) |
64MB NOR Flash
#define BOARD_FLASH_ID_S71KS512S (0x007EU) |
512 Mb cypress Hyperflash device Id
#define MAX_BOARD_FLASH_INSTANCE_NUM 8 |
Maximum Board flash instance number that can be opened.
typedef uintptr_t Board_flashHandle |
This type defines the opaque handle returned to a flash device that is opened. The handle must be used in all subsequent operations.
typedef int32_t Board_flash_STATUS |
Error codes used by Board flash functions. Negative values are errors, while positive values indicate success.
Board specific Flash Device Identifiers.
Indicates the type of NOR flash peripheral
enum Board_flashType |