PDK API Guide for J721E
|
Application Interfaces provided by IMX390 sensor device library
Functions | |
Board_STATUS | Board_imx390CamCfg (void *handle, Board_FpdRmtDevObj *rmtSlvParams) |
Initializes the imx390 camera sensor device. More... | |
Board_STATUS Board_imx390CamCfg | ( | void * | handle, |
Board_FpdRmtDevObj * | rmtSlvParams | ||
) |
Initializes the imx390 camera sensor device.
This function is used to initialize the imx390 camera sensor module
handle | [IN] Low level driver handle |
rmtSlvParams | [IN] Remote slave params |