PDK API Guide for J721E
|
CSIRX Driver API/interface file.
Requirement: NA
Go to the source code of this file.
Data Structures | |
struct | Csirx_ChCfg |
Structure containing Channels configurations. More... | |
struct | Csirx_InstCfg |
Structure containing csirx module initialization arguments. More... | |
struct | Csirx_CreateParams |
Capture driver create arguments, used when calling Fvid2_create(). Structure containing Streams configurations. More... | |
struct | Csirx_InitParams |
Capture driver create arguments, used when calling Fvid2_create(). Structure containing Streams configurations. More... | |
struct | Csirx_CreateStatus |
Capture driver create status. Returned after calling Fvid2_create(). More... | |
struct | Csirx_InstStatus |
Capture status structure used to get the current status. More... | |
Macros | |
#define | CSIRX_CAPT_DRV_ID (FVID2_CSIRX_DRV_BASE + 0x00000000U) |
CSIRX capture driver ID used at the time of FVID2 create. More... | |
#define | IOCTL_CSIRX_GET_INST_STATUS (FVID2_CSIRX_DRV_IOCTL_BASE + 0x0000U) |
Get capture status IOCTL. More... | |
#define | IOCTL_CSIRX_PRINT_DEBUG_LOGS (FVID2_CSIRX_DRV_IOCTL_BASE + 0x0100U) |
Print capture debug logs. More... | |
#define | IOCTL_CSIRX_SET_DPHY_CONFIG (FVID2_CSIRX_DRV_IOCTL_BASE + 0x0200U) |
Set CSIRX D-PHY Configuration Parameters. More... | |
#define | IOCTL_CSIRX_REGISTER_EVENT (FVID2_CSIRX_DRV_IOCTL_BASE + 0x0300U) |
Register CSIRX events. More... | |
#define | IOCTL_CSIRX_UNREGISTER_EVENT (FVID2_CSIRX_DRV_IOCTL_BASE + 0x0400U) |
Un-register CSIRX events. More... | |
#define | CSIRX_BUF_ALIGNMENT (UDMA_CACHELINE_ALIGNMENT) |
Buffer memory alignment with cache line size. More... | |
CSIRX Channel Type | |
#define | CSIRX_CH_TYPE_CAPT ((uint32_t) 0x0U) |
Stream type: capture mode, frames will captured to internal memory or DDR. More... | |
#define | CSIRX_CH_TYPE_OTF ((uint32_t) 0x1U) |
Stream type: OTF mode, frames will be forwarded to Video Port/VISS. More... | |
#define | CSIRX_CH_TYPE_LPBK ((uint32_t) 0x2U) |
Stream type: Loopback mode, frames will be forwarded to CSI Tx trans PADs. More... | |
Functions | |
int32_t | Csirx_init (const Csirx_InitParams *initParams) |
CSIRX Driver Init function. More... | |
int32_t | Csirx_deInit (void) |
CSIRX Driver de-Init function. More... | |
static void | Csirx_initParamsInit (Csirx_InitParams *initPrms) |
Csirx_InitParams structure init function. More... | |
static void | Csirx_createParamsInit (Csirx_CreateParams *createPrms) |
Csirx_CreateParams structure init function. More... | |
static void | Csirx_chCfgInit (Csirx_ChCfg *chCfg) |
Csirx_ChCfg structure init function. More... | |
static void | Csirx_instCfgInit (Csirx_InstCfg *instCfg) |
Csirx_InstCfg structure init function. More... | |
static void | Csirx_instStatusInit (Csirx_InstStatus *status) |
Csirx_InstStatus structure init function. More... | |
#define CSIRX_CH_TYPE_CAPT ((uint32_t) 0x0U) |
Stream type: capture mode, frames will captured to internal memory or DDR.
#define CSIRX_CH_TYPE_OTF ((uint32_t) 0x1U) |
Stream type: OTF mode, frames will be forwarded to Video Port/VISS.
#define CSIRX_CH_TYPE_LPBK ((uint32_t) 0x2U) |
Stream type: Loopback mode, frames will be forwarded to CSI Tx trans PADs.
#define CSIRX_BUF_ALIGNMENT (UDMA_CACHELINE_ALIGNMENT) |
Buffer memory alignment with cache line size.
int32_t Csirx_init | ( | const Csirx_InitParams * | initParams | ) |
CSIRX Driver Init function.
initParams | [IN] Pointer to Csirx_InitParams structure. |
int32_t Csirx_deInit | ( | void | ) |
CSIRX Driver de-Init function.
|
inlinestatic |
Csirx_InitParams structure init function.
initPrms | [IN] Pointer to Csirx_InitParams structure. |
|
inlinestatic |
Csirx_CreateParams structure init function.
createPrms | [IN] Pointer to Csirx_CreateParams structure. |
|
inlinestatic |
Csirx_ChCfg structure init function.
chCfg | [IN] Pointer to Csirx_ChCfg structure. |
|
inlinestatic |
Csirx_InstCfg structure init function.
instCfg | [IN] Pointer to Csirx_InstCfg structure. |
|
inlinestatic |
Csirx_InstStatus structure init function.
status | [IN] Pointer to Csirx_InstStatus structure. |