![]() |
PDK API Guide for J721E
|
Event module for the RTOS Porting Interface.
============================================================================
Go to the source code of this file.
Data Structures | |
struct | EventP_Params |
Basic EventP Parameters. More... | |
Macros | |
#define | EventP_ID_NONE Event_Id_NONE |
Event ID 0. More... | |
#define | EventP_ID_00 Event_Id_00 |
Event ID 0. More... | |
#define | EventP_ID_01 Event_Id_01 |
Event ID 1. More... | |
#define | EventP_ID_02 Event_Id_02 |
Event ID 2. More... | |
#define | EventP_ID_03 Event_Id_03 |
Event ID 3. More... | |
#define | EventP_ID_04 Event_Id_04 |
Event ID 4. More... | |
#define | EventP_ID_05 Event_Id_05 |
Event ID 5. More... | |
#define | EventP_ID_06 Event_Id_06 |
Event ID 6. More... | |
#define | EventP_ID_07 Event_Id_07 |
Event ID 7. More... | |
#define | EventP_ID_08 Event_Id_08 |
Event ID 8. More... | |
#define | EventP_ID_09 Event_Id_09 |
Event ID 9. More... | |
#define | EventP_ID_10 Event_Id_10 |
Event ID 10. More... | |
#define | EventP_WAIT_FOREVER (~((uint32_t)0U)) |
Wait forever define. More... | |
#define | EventP_NO_WAIT ((uint32_t)0U) |
No wait define. More... | |
Typedefs | |
typedef void * | EventP_Handle |
Opaque client reference to an instance of a EventP. More... | |
Enumerations | |
enum | EventP_Status { EventP_OK = 0, EventP_FAILURE = (-(int32_t)1) } |
Status codes for EventP APIs. More... | |
Functions | |
EventP_Handle | EventP_create (EventP_Params *params) |
Function to create an event. More... | |
void | EventP_delete (EventP_Handle *handle) |
Function to delete an event. More... | |
void | EventP_Params_init (EventP_Params *params) |
Initialize params structure to default values. More... | |
uint32_t | EventP_pend (EventP_Handle handle, uint32_t andMask, uint32_t orMask, uint32_t timeout) |
Function for Event Pend. More... | |
void | EventP_post (EventP_Handle handle, uint32_t eventMask) |
Function for Event Post. More... | |
uint32_t | EventP_getPostedEvents (EventP_Handle handle) |
Function for Event Post. More... | |