![]() |
TI Deep Learning Library User Guide
|
This structure defines the parameters for custom layer in TIDL.
Data Fields | |
int32_t | customLayerType |
int32_t | padW |
int32_t | padH |
int32_t | memOverlapType |
int32_t | customLayerParamsOffset |
int32_t sTIDL_CustomParams_t::customLayerType |
Type of the custom layer
int32_t sTIDL_CustomParams_t::padW |
Horizontal Padding requirement in number of elements
int32_t sTIDL_CustomParams_t::padH |
Vertical Padding requirement in number of elements
int32_t sTIDL_CustomParams_t::memOverlapType |
Parameter specifying whether input and output memory can overlap 0: Input cannot be overwritten by output 1: Input can be overwritten by input
int32_t sTIDL_CustomParams_t::customLayerParamsOffset |
Custom parameters that should be defined in tidl_custom.h/ This variable provides offset to the parameters in the net file