TI Deep Learning Library User Guide
|
This structure define the parameters Crop layer in TIDL.
Data Fields | |
int32_t | numChannels |
int32_t | inDataQ |
int32_t | outDataQ |
int32_t | offsetW |
int32_t | offsetH |
int32_t sTIDL_CropParams_t::numChannels |
Number of channels channels to be processed
int32_t sTIDL_CropParams_t::inDataQ |
Q value of the in data
int32_t sTIDL_CropParams_t::outDataQ |
Q value expected for out data
int32_t sTIDL_CropParams_t::offsetW |
Horizontal offset
int32_t sTIDL_CropParams_t::offsetH |
Vertical offset