#include <stdio.h>
#include <stdlib.h>
#include <stdint.h>
#include <string.h>
#include <stdbool.h>
Go to the source code of this file.
◆ Cache_EMIFA_CFG
| #define Cache_EMIFA_CFG 0x1e00000 |
◆ Cache_EMIFA_BASE
| #define Cache_EMIFA_BASE 0x2000000 |
◆ Cache_EMIFA_LENGTH
| #define Cache_EMIFA_LENGTH 0x8000000 |
◆ Cache_EMIFB_CFG
| #define Cache_EMIFB_CFG 0x20000000 |
◆ Cache_EMIFB_BASE
| #define Cache_EMIFB_BASE 0x80000000 |
◆ Cache_EMIFB_LENGTH
| #define Cache_EMIFB_LENGTH 0x10000000 |
◆ Cache_EMIFC_CFG
| #define Cache_EMIFC_CFG 0x1e00000 |
◆ Cache_EMIFC_BASE
| #define Cache_EMIFC_BASE 0x42000000 |
◆ Cache_EMIFC_LENGTH
| #define Cache_EMIFC_LENGTH 0x8000000 |
◆ L2CFG
| #define L2CFG (volatile unsigned int *)0x01840000 |
◆ L1PCFG
| #define L1PCFG (volatile unsigned int *)0x01840020 |
◆ L1PCC
| #define L1PCC (volatile unsigned int *)0x01840024 |
◆ L1DCFG
| #define L1DCFG (volatile unsigned int *)0x01840040 |
◆ L1DCC
| #define L1DCC (volatile unsigned int *)0x01840044 |
◆ L2WBAR
| #define L2WBAR (volatile unsigned int *)0x01844000 |
◆ L2WWC
| #define L2WWC (volatile unsigned int *)0x01844004 |
◆ L2WIBAR
| #define L2WIBAR (volatile unsigned int *)0x01844010 |
◆ L2IBAR
| #define L2IBAR (volatile unsigned int *)0x01844018 |
◆ L2WBINV
| #define L2WBINV (volatile unsigned int *)0x01845004 |
◆ L1DWBINV
| #define L1DWBINV (volatile unsigned int *)0x01845044 |
◆ L1DINV
| #define L1DINV (volatile unsigned int *)0x01845048 |
◆ L2INV
| #define L2INV (volatile unsigned int *)0x01845008 |
◆ L1DWb
| #define L1DWb (volatile unsigned int *)0x01845040 |
◆ L2Wb
| #define L2Wb (volatile unsigned int *)0x01845000 |
◆ L1DWWC
| #define L1DWWC (volatile unsigned int *)0x0184404C |
◆ MAXWC
| #define MAXWC 0xFF00 /* Max word count per cache operations */ |
◆ Cache_inv()
| void Cache_inv |
( |
uint8_t * |
blockPtr, |
|
|
unsigned int |
byteCnt, |
|
|
bool |
wait |
|
) |
| |
◆ Cache_wb()
| void Cache_wb |
( |
uint8_t * |
blockPtr, |
|
|
unsigned int |
byteCnt, |
|
|
bool |
wait |
|
) |
| |
◆ Cache_wbInv()
| void Cache_wbInv |
( |
uint8_t * |
blockPtr, |
|
|
unsigned int |
byteCnt, |
|
|
bool |
wait |
|
) |
| |
◆ Cache_WbInvAll()
◆ Cache_InvAll()
◆ Cache_WbAll()