PDK Documentation
|
Go to the source code of this file.
Data Structures | |
struct | tisci_msg_rm_udmap_gcfg_cfg_req |
Configures a Navigator Subsystem UDMAP global configuration region. Configures the non-real-time registers of a Navigator Subsystem UDMAP global configuration region. The GCFG region being programmed must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment array. Individual fields for registers specified as valid are not checked for correctness. It is the application's responsibility to verify if the register fields are being set according to the device specification. More... | |
struct | tisci_msg_rm_udmap_gcfg_cfg_resp |
Response to configuring UDMAP global configuration. More... | |
struct | tisci_msg_rm_udmap_gcfg_get_cfg_req |
Get Navigator Subsystem UDMAP global configuration's non-real-time register configuration. Gets the configuration of the non-real-time register fields of a UDMAP global configuration. The host, or a supervisor of the host, who owns the gcfg region must be the requesting host. The values of the non-real-time registers are returned in tisci_msg_rm_udmap_gcfg_get_cfg_resp. The reset_cfg parameter is used to request either the existing non-real-time register values or the hardware reset values for the UDMAP global configuration register fields. More... | |
struct | tisci_msg_rm_udmap_gcfg_get_cfg_resp |
UDMAP global configuration get configuration response message. Response received by host processor after RM has handled tisci_msg_rm_udmap_gcfg_get_cfg_req. The response contains the global configuration's non-real-time register values. More... | |
struct | tisci_msg_rm_udmap_tx_ch_cfg_req |
Configures a Navigator Subsystem UDMAP transmit channel. More... | |
struct | tisci_msg_rm_udmap_tx_ch_cfg_resp |
Response to configuring a UDMAP transmit channel. More... | |
struct | tisci_msg_rm_udmap_tx_ch_get_cfg_req |
Get Navigator Subsystem UDMAP transmit channel's non-real-time register configuration. More... | |
struct | tisci_msg_rm_udmap_tx_ch_get_cfg_resp |
UDMAP transmit channel get configuration response message. More... | |
struct | tisci_msg_rm_udmap_rx_ch_cfg_req |
Configures a Navigator Subsystem UDMAP receive channel. More... | |
struct | tisci_msg_rm_udmap_rx_ch_cfg_resp |
Response to configuring a UDMAP receive channel. More... | |
struct | tisci_msg_rm_udmap_rx_ch_get_cfg_req |
Get Navigator Subsystem UDMAP receive channel's non-real-time register configuration. More... | |
struct | tisci_msg_rm_udmap_rx_ch_get_cfg_resp |
UDMAP receive channel get configuration response message. More... | |
struct | tisci_msg_rm_udmap_flow_cfg_req |
Configures a Navigator Subsystem UDMAP receive flow. More... | |
struct | tisci_msg_rm_udmap_flow_cfg_resp |
Response to configuring a Navigator Subsystem UDMAP receive flow. More... | |
struct | tisci_msg_rm_udmap_flow_get_cfg_req |
Get Navigator Subsystem UDMAP receive flow's non-real-time register configuration. More... | |
struct | tisci_msg_rm_udmap_flow_get_cfg_resp |
UDMAP receive flow get configuration response message. More... | |
struct | tisci_msg_rm_udmap_flow_size_thresh_cfg_req |
Configures a Navigator Subsystem UDMAP receive flow's size threshold fields. More... | |
struct | tisci_msg_rm_udmap_flow_size_thresh_cfg_resp |
Response to configuring a Navigator Subsystem UDMAP receive flow's size threshold fields. More... | |
struct | tisci_msg_rm_udmap_flow_size_thresh_get_cfg_req |
Get Navigator Subsystem UDMAP receive flow's non-real-time size threshold based queue routing register configuration. More... | |
struct | tisci_msg_rm_udmap_flow_size_thresh_get_cfg_resp |
UDMAP receive flow get size threshold configuration response message. More... | |
Functions | |
struct tisci_msg_rm_udmap_gcfg_cfg_req | __attribute__ ((__packed__)) |
struct tisci_header hdr |
uint32_t valid_params |
uint16_t nav_id |
uint32_t perf_ctrl |
uint32_t emu_ctrl |
uint32_t psil_to |
uint32_t rflowfwstat |
uint8_t get_reset_cfg |
uint32_t revision |
uint32_t utc_ctrl |
uint32_t cap0 |
uint32_t cap1 |
uint32_t cap2 |
uint32_t cap3 |
uint16_t index |
uint8_t tx_pause_on_err |
uint8_t tx_filt_einfo |
uint8_t tx_filt_pswords |
uint8_t tx_atype |
uint8_t tx_chan_type |
uint8_t tx_supr_tdpkt |
uint16_t tx_fetch_size |
uint8_t tx_credit_count |
uint16_t txcq_qnum |
uint8_t tx_priority |
uint8_t tx_qos |
uint8_t tx_orderid |
uint16_t fdepth |
uint8_t tx_sched_priority |
uint8_t tx_burst_size |
uint8_t tx_tdtype |
uint16_t rx_fetch_size |
uint16_t rxcq_qnum |
uint8_t rx_priority |
uint8_t rx_qos |
uint8_t rx_orderid |
uint8_t rx_sched_priority |
uint16_t flowid_start |
uint16_t flowid_cnt |
uint8_t rx_pause_on_err |
uint8_t rx_atype |
uint8_t rx_chan_type |
uint8_t rx_ignore_short |
uint8_t rx_ignore_long |
uint8_t rx_burst_size |
uint16_t flow_index |
uint8_t rx_einfo_present |
uint8_t rx_psinfo_present |
uint8_t rx_error_handling |
uint8_t rx_desc_type |
uint16_t rx_sop_offset |
uint16_t rx_dest_qnum |
uint8_t rx_src_tag_hi |
uint8_t rx_src_tag_lo |
uint8_t rx_dest_tag_hi |
uint8_t rx_dest_tag_lo |
uint8_t rx_src_tag_hi_sel |
uint8_t rx_src_tag_lo_sel |
uint8_t rx_dest_tag_hi_sel |
uint8_t rx_dest_tag_lo_sel |
uint16_t rx_fdq0_sz0_qnum |
uint16_t rx_fdq1_qnum |
uint16_t rx_fdq2_qnum |
uint16_t rx_fdq3_qnum |
uint8_t rx_ps_location |
uint16_t rx_size_thresh0 |
uint16_t rx_size_thresh1 |
uint16_t rx_size_thresh2 |
uint16_t rx_fdq0_sz1_qnum |
uint16_t rx_fdq0_sz2_qnum |
uint16_t rx_fdq0_sz3_qnum |
uint8_t rx_size_thresh_en |