![]() |
PDK Documentation
|
OS Abstraction Layer header.
============================================================================
Go to the source code of this file.
Data Structures | |
| struct | Osal_StaticMemStatus |
| This structure holds static memory status parameters of OSAL library. More... | |
| struct | Osal_memRange |
| Osal memory address range. More... | |
| struct | Osal_HwAttrs |
| Osal hw attributes structure. More... | |
Macros | |
| #define | osal_OK (0) |
| #define | osal_FAILURE (-(int32_t)(1)) |
| #define | osal_UNSUPPORTED (-(int32_t)(2)) |
| #define | osal_NOMEM (-(int32_t)(3)) |
| #define | OSAL_NONOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 48U) |
| #define | OSAL_NONOS_HWIP_SIZE_BYTES ((uint32_t) 48U) |
| #define | OSAL_TIRTOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 96U) |
| #define | OSAL_TIRTOS_HWIP_SIZE_BYTES (96U) |
| #define | OSAL_Assert(expression) |
| Assert checking function. More... | |
| #define | OSAL_HWATTR_SET_EXT_CLK (0x00000001U) |
| #define | OSAL_HWATTR_SET_ECM_INT (0x00000002U) |
| #define | OSAL_HWATTR_SET_HWACCESS_TYPE (0x00000004U) |
| #define | OSAL_HWATTR_SET_OSALDELAY_TIMER_BASE (0x00000008U) |
| #define | OSAL_HWATTR_SET_SEMP_EXT_BASE (0x00000010U) |
| #define | OSAL_HWATTR_SET_HWIP_EXT_BASE (0x00000020U) |
| #define | OSAL_HWATTR_SET_CPU_FREQ (0x00000040U) |
| #define | OSAL_HWATTR_SET_TARG_PROC_LIST (0x00000080) |
| #define | OSAL_COMPILE_TIME_SIZE_CHECK(x, y) |
Enumerations | |
| enum | Osal_ThreadType { Osal_ThreadType_Hwi, Osal_ThreadType_Swi, Osal_ThreadType_Task, Osal_ThreadType_Main } |
| This enum defines the multiple thread types used under OSAL library. More... | |
| enum | Osal_HwAccessType { OSAL_HWACCESS_UNRESTRICTED, OSAL_HWACCESS_RESTRICTED } |
| Osal hw access type. More... | |
Functions | |
| void | Osal_DebugP_assert (int32_t expression, const char *file, int32_t line) |
| Osal_ThreadType | Osal_getThreadType (void) |
| Function to get the current thread type. More... | |
| int32_t | Osal_delay (uint32_t nTicks) |
| Function to get the delay/sleep. More... | |
| int32_t | Osal_setHwAttrs (uint32_t ctrlBitMap, const Osal_HwAttrs *hwAttrs) |
| Function to set the Hw Attributes. More... | |
| int32_t | Osal_getHwAttrs (Osal_HwAttrs *hwAttrs) |
| Function to get the Hw Attributes. More... | |
| int32_t | Osal_getStaticMemStatus (Osal_StaticMemStatus *pMemStat) |
| Function to get the static memory usage of OSAL library. More... | |
| int32_t | Osal_getCoreId (void) |
| Function to get the core ID of the running Core. More... | |
Variables | |
| Osal_HwAttrs | gOsal_HwAttrs |
| external references for Osal Hw Attribute structure More... | |