This is DMA Utils related configuration parameters and API
|
| file | dmautils_autoincrement_3d.h |
| | This file contains the data types and util function prototype for configuring DMA Utility autoincrement 3D usecase.
|
| |
|
| int32_t | DmaUtilsAutoInc3d_getContextSize (int32_t numChannels) |
| | Returns the size of dmautils context. More...
|
| |
| int32_t | DmaUtilsAutoInc3d_init (void *autoIncrementContext, DmaUtilsAutoInc3d_InitParam *initParams, DmaUtilsAutoInc3d_ChannelInitParam chInitParams[]) |
| | This function initializes the DMA UTILS context for autoincrement usecase. More...
|
| |
| int32_t | DmaUtilsAutoInc3d_getTrMemReq (int32_t numTRs) |
| | This function returns the size of the TR descriptor required for the transfer configuration given by the user. More...
|
| |
| int32_t | DmaUtilsAutoInc3d_prepareTr (DmaUtilsAutoInc3d_TrPrepareParam *trPrepParam, DmaUtilsAutoInc3d_TransferProp transferProp[]) |
| | This function will prepare a TR/ TR descriptor depending on the number of Tr's to be submitted on a particular channel. More...
|
| |
| int32_t | DmaUtilsAutoInc3d_configure (void *autoIncrementContext, int32_t channelId, uint8_t *trMem, int32_t numTr) |
| | This function configures autoincrement for a particular channel. More...
|
| |
| int32_t | DmaUtilsAutoInc3d_trigger (void *autoIncrementContext, int32_t channelId) |
| | This function triggers transfer on a particular channel. More...
|
| |
| void | DmaUtilsAutoInc3d_wait (void *autoIncrementContext, int32_t channelId) |
| | This function waits for completion transfer on a particular channel. More...
|
| |
| int32_t | DmaUtilsAutoInc3d_deconfigure (void *autoIncrementContext, int32_t channelId, uint8_t *trMem, int32_t numTr) |
| | This function deconfigures autoincrement for a particular channel. More...
|
| |
| int32_t | DmaUtilsAutoInc3d_deinit (void *autoIncrementContext) |
| | This function deinit autoincrement by releasing all the resorces allocated. More...
|
| |
◆ DMAUTILS_MAX_NUM_TR_DIRECT_TR_MODE
| #define DMAUTILS_MAX_NUM_TR_DIRECT_TR_MODE (1U) |
Number of TR's that can be submitted back to back channel.
◆ DmaUtilsAutoInc3d_SyncType
Describes the boundary at which the DMA is suppose to get synced.
| Enumerator |
|---|
| DMAUTILSAUTOINC3D_SYNC_1D | DMA is synced at each 1D transfer i.e. it is synced whenever icnt1 is decremented by 1
|
| DMAUTILSAUTOINC3D_SYNC_2D | DMA is synced at each 2D transfer i.e. it is synced whenever icnt2 is decremented by 1
|
| DMAUTILSAUTOINC3D_SYNC_3D | DMA is synced at each 3D transfer i.e. it is synced whenever icnt3 is decremented by 1
|
| DMAUTILSAUTOINC3D_SYNC_4D | DMA is synced at each 4D transfer i.e. it is synced whenever one TR is completed
|
◆ DmaUtilsAutoInc3d_AddrType
Describes the boundary at which the DMA is suppose to get synced.
| Enumerator |
|---|
| DMAUTILSAUTOINC3D_ADDR_LINEAR | Linear addressing, addresses will be updated linearly as per the dim's and icnt's
|
| DMAUTILSAUTOINC3D_ADDR_CIRC1 | Circular addressing, address will hold the upper bits of the addresses to be constant. This enum is to use circSize1 for circularity
|
| DMAUTILSAUTOINC3D_ADDR_CIRC2 | Circular addressing, address will hold the upper bits of the addresses to be constant. This enum is to use circSize2 for circularity
|
◆ DmaUtilsAutoInc3d_CircDirType
Describes the direction in which circular addressing is applied.
| Enumerator |
|---|
| DMAUTILSAUTOINC3D_CIRCDIR_SRC | Circular addressing if enabled is applied on source side
|
| DMAUTILSAUTOINC3D_CIRCDIR_DST | Circular addressing if enabled is applied on desination side
|
◆ DmaUtilsAutoInc3d_druOwner
| Enumerator |
|---|
| DMAUTILSAUTOINC3D_DRUOWNER_DIRECT_TR | DRU channel is used in Direct TR mode
|
| DMAUTILSAUTOINC3D_DRUOWNER_UDMA | Dru channel is used via ring based mechanism
|
◆ DmaUtilsAutoInc3d_getContextSize()
| int32_t DmaUtilsAutoInc3d_getContextSize |
( |
int32_t |
numChannels | ) |
|
Returns the size of dmautils context.
This function returns the size of the DMA UTILS autoincrement 3D handle. User is then expected to allocate this memory and provide it to DMA UTILS autoincrement 3D function as an input.
- Parameters
-
| numChannels | [IN] Number of channels required for a usecase |
- Returns
- Size of the DMA UTILS context in bytes
◆ DmaUtilsAutoInc3d_init()
This function initializes the DMA UTILS context for autoincrement usecase.
This function initializes the DMA UTILS context for autoincrement usecase. Internally it allocates numChannels DRU channels for the use case
- Parameters
-
| autoIncrementContext | [IN] Memory allocated by the user as per DmaUtilsAutoInc3d_getContextSize API. Try to allocate this memory in the fastest available memory for optimal performance |
| initParams | [IN] Init params for the dmautils |
| chInitParams | [IN] Init parameter for each channel. This is an array and number of enteries should be same as numChannels |
- Returns
- Udma_ErrorCodes
◆ DmaUtilsAutoInc3d_getTrMemReq()
| int32_t DmaUtilsAutoInc3d_getTrMemReq |
( |
int32_t |
numTRs | ) |
|
This function returns the size of the TR descriptor required for the transfer configuration given by the user.
- Parameters
-
| numTRs | [IN] Number of Transfer Records (TR's) that will be submitted to a particular channel |
- Returns
- Size of the TR descriptor in bytes.
◆ DmaUtilsAutoInc3d_prepareTr()
This function will prepare a TR/ TR descriptor depending on the number of Tr's to be submitted on a particular channel.
- Parameters
-
| trPrepParam | [IN] Parameters required for preparing TR |
| transferProp | [IN] Transfer properties of all the TR'sr which needs to be submitted to a single channel |
- Returns
- Udma_ErrorCodes
◆ DmaUtilsAutoInc3d_configure()
| int32_t DmaUtilsAutoInc3d_configure |
( |
void * |
autoIncrementContext, |
|
|
int32_t |
channelId, |
|
|
uint8_t * |
trMem, |
|
|
int32_t |
numTr |
|
) |
| |
This function configures autoincrement for a particular channel.
- Parameters
-
| autoIncrementContext | [IN] Context allocated for dmautils usecase |
| channelId | [IN] Channel Id which needs to be configured. It is important to note that this id is a virtual id for channel and is not related to the actual channel used internally to do the transfer |
| trMem | [IN] Populated TrMem after calling DmaUtilsAutoInc3d_prepareTr function |
| numTr | [IN] Number of Transfer Records (TR's) that will be submitted to a particular channel |
- Returns
- Udma_ErrorCodes
◆ DmaUtilsAutoInc3d_trigger()
| int32_t DmaUtilsAutoInc3d_trigger |
( |
void * |
autoIncrementContext, |
|
|
int32_t |
channelId |
|
) |
| |
This function triggers transfer on a particular channel.
- Parameters
-
| autoIncrementContext | [IN] Context allocated for dmautils usecase |
| channelId | [IN] Channel Id which needs to be triggered. It is important to note that this id is a virtual id for channel and is not related to the actual channel used internally to do the transfer |
- Returns
- Number of triggered required to complete the full transfer
◆ DmaUtilsAutoInc3d_wait()
| void DmaUtilsAutoInc3d_wait |
( |
void * |
autoIncrementContext, |
|
|
int32_t |
channelId |
|
) |
| |
This function waits for completion transfer on a particular channel.
- Parameters
-
| autoIncrementContext | [IN] Context allocated for dmautils usecase |
| channelId | [IN] Channel Id for which we need to wait for transfer completion. It is important to note that this id is a virtual id for channel and is not related to the actual channel used internally to do the transfer |
- Returns
- Number of triggered required to complete the full transfer
◆ DmaUtilsAutoInc3d_deconfigure()
| int32_t DmaUtilsAutoInc3d_deconfigure |
( |
void * |
autoIncrementContext, |
|
|
int32_t |
channelId, |
|
|
uint8_t * |
trMem, |
|
|
int32_t |
numTr |
|
) |
| |
This function deconfigures autoincrement for a particular channel.
- Parameters
-
| autoIncrementContext | [IN] Context allocated for dmautils usecase |
| channelId | [IN] Channel Id which needs to be de-configured. It is important to note that this id is a virtual id for channel and is not related to the actual channel used internally to do the transfer |
| trMem | [IN] Populated TrMem after calling DmaUtilsAutoInc3d_prepareTr function |
| numTr | [IN] Number of Transfer Records (TR's) that will be submitted to a particular channel |
- Returns
- Udma_ErrorCodes
◆ DmaUtilsAutoInc3d_deinit()
| int32_t DmaUtilsAutoInc3d_deinit |
( |
void * |
autoIncrementContext | ) |
|
This function deinit autoincrement by releasing all the resorces allocated.
- Parameters
-
| autoIncrementContext | [IN] Context allocated for dmautils usecase |
- Returns
- Udma_ErrorCodes