![]() |
PDK Documentation
|
Functions | |
void | CSL_SGMII_getVersionInfo (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum, CSL_SGMII_VERSION *sgmiiVersionInfo) |
void | CSL_SGMII_doSoftReset (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
Uint32 | CSL_SGMII_getSoftResetStatus (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_startRxTxSoftReset (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_endRxTxSoftReset (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
Uint32 | CSL_SGMII_getRxTxSoftResetStatus (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
Uint32 | CSL_SGMII_getSerdesPLLLockStatus (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_enableTestPattern (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_DisableTestPattern (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_enableMasterMode (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_disableMasterMode (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
Uint32 | CSL_SGMII_isMasterModeEnabled (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_enableLoopback (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_disableLoopback (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
Uint32 | CSL_SGMII_isLoopbackModeEnabled (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_restartAutoNegotiation (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_enableAutoNegotiation (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_disableAutoNegotiation (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
Uint32 | CSL_SGMII_isAutoNegotiationEnabled (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum) |
void | CSL_SGMII_getStatus (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum, CSL_SGMII_STATUS *pSgmiiStatus) |
void | CSL_SGMII_setAdvAbility (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum, CSL_SGMII_ADVABILITY *pSgmiiAdvAbility) |
void | CSL_SGMII_getAdvAbility (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum, CSL_SGMII_ADVABILITY *pSgmiiAdvAbility) |
void | CSL_SGMII_getLinkPartnerAdvAbility (CSL_CpsgmiiRegs *hCpSgmiiRegs, Uint32 portNum, CSL_SGMII_ADVABILITY *pSgmiiAdvAbility) |
void CSL_SGMII_getVersionInfo | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum, | ||
CSL_SGMII_VERSION * | sgmiiVersionInfo | ||
) |
============================================================================
CSL_SGMII_getVersionInfo
Description
This function retrieves the SGMII version information for the SGMII port specified.
Arguments
portNum SGMII port number for which settings must be retrieved. sgmiiVersionInfo CSL_SGMII_VERSION structure that needs to be populated with the version info read from the SGMII_IDVER register. *
Return Value
None
Pre Condition
None
Post Condition
None
Reads
CPSGMII_IDVER_REG_MINOR_VER, CPSGMII_IDVER_REG_MAJOR_VER, CPSGMII_IDVER_REG_RTL_VER, CPSGMII_IDVER_REG_TX_IDENT
Example
CSL_SGMII_VERSION sgmiiVersionInfo; Uint32 portNum = 1; CSL_SGMII_getVersion (portNum, &sgmiiVersionInfo);
void CSL_SGMII_doSoftReset | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_doSoftReset
Description
This function initiates a CPSGMII logic software reset for the SGMII port specified by setting the 'SOFT_RESET' bit of the CPSGMII Software Reset register to 1.
Arguments
portNum SGMII port number for which reset must be performed. *
Return Value
None
Pre Condition
None
Post Condition
Software reset on CPSGMII port is initiated. The Soft reset bit is set back to 0 once the reset operation is completed.
Writes
CPSGMII_SOFT_RESET_REG_SOFT_RESET=1
Affects
CPSGMII_SOFT_RESET_REG_SOFT_RESET=0
Example
Uint32 portNum = 1; CSL_SGMII_doSoftReset (portNum);
Uint32 CSL_SGMII_getSoftResetStatus | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_getSoftResetStatus
Description
This function reads the 'SOFT_RESET' bit of the CPSGMII Software Reset register and returns its contents for the port specified.
Arguments
portNum SGMII port number for which reset status must be retrieved. *
Return Value Uint32
Pre Condition
None
Post Condition
None
Reads
CPSGMII_SOFT_RESET_REG_SOFT_RESET
Example
Uint32 portNum = 1; if (!CSL_SGMII_getSoftResetStatus (portNum)) { // Software reset is completed. }
void CSL_SGMII_startRxTxSoftReset | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_startRxTxSoftReset
Description
This function initiates a SGMII Receive and Transmit logic software reset by setting the 'RT_SOFT_RESET' bit of the CPSGMII Software Reset register to 1. This reset is to be started when switching between normal and loopback modes of operation.
Arguments
portNum SGMII port number for which reset must started. *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII Rx/Tx Software logic reset initiated.
Writes
CPSGMII_SOFT_RESET_REG_RT_SOFT_RESET=1
Example
Uint32 portNum = 1; CSL_SGMII_startRxTxSoftReset (portNum);
void CSL_SGMII_endRxTxSoftReset | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_endRxTxSoftReset
Description
This function terminates a SGMII Receive and Transmit logic software reset initiated earlier by calling CSL_SGMII_startRxTxSoftReset () API. This API sets the 'RT_SOFT_RESET' bit of the CPSGMII Software Reset register to 0 to do so. This API is to be called once the loopback/normal switch is done.
Arguments
portNum SGMII port number for which reset must be ended. *
Return Value
None
Pre Condition
CSL_SGMII_startRxTxSoftReset () API must have been called earlier to initiate the Rx/Tx Soft reset before calling this API.
Post Condition
CPSGMII Rx/Tx Software logic reset cleared.
Writes
CPSGMII_SOFT_RESET_REG_RT_SOFT_RESET=0
Example
Uint32 portNum = 1; CSL_SGMII_endRxTxSoftReset (portNum);
Uint32 CSL_SGMII_getRxTxSoftResetStatus | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_getRxTxSoftResetStatus
Description
This function reads the 'RT_SOFT_RESET' bit of the CPSGMII Software Reset register and returns its contents.
Arguments
portNum SGMII port number for which reset status must be retrieved. *
Return Value Uint32
Pre Condition
None
Post Condition
None
Reads
CPSGMII_SOFT_RESET_REG_RT_SOFT_RESET
Example
Uint32 portNum = 1; if (!CSL_SGMII_getRxTxSoftResetStatus (portNum)) { // Software reset is completed. }
Uint32 CSL_SGMII_getSerdesPLLLockStatus | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_getSerdesPLLLockStatus
Description
This function reads the 'PLL_LOCK' bit of the CPSGMII status register and returns its contents.
Arguments
portNum SGMII port number for which loopback must be enabled. *
Return Value
None
Pre Condition
None
Post Condition
None
Reads
CPSGMII_STATUS_REG_LOCK
Example
Uint32 portNum = 1; CSL_SGMII_getSerdesPLLLockStatus (portNum);
void CSL_SGMII_enableTestPattern | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_enableTestPattern
Description
This function enables test pattern (Force the output of K28.5 on TX_ENC for test purposes) for the port specified.
Arguments
portNum SGMII port number for which the operation must be performed. *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII test-pattern enabled.
Writes
CPSGMII_CONTROL_REG_TEST_PATTERN=1
Example
Uint32 portNum = 1; CSL_SGMII_enableTestPattern (portNum);
void CSL_SGMII_DisableTestPattern | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_DisableTestPattern
Description
This function clears test pattern enable bit for the port specified.
Arguments
portNum SGMII port number for which the operation must be performed. *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII test-pattern disabled.
Writes
CPSGMII_CONTROL_REG_TEST_PATTERN=0
Example
Uint32 portNum = 1; CSL_SGMII_DisableTestPattern (portNum);
void CSL_SGMII_enableMasterMode | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_enableMasterMode
Description
This function configures the CPSGMII in 'Master' mode. Master mode allows a CPSGMII direct connection with auto-negotiation or with forced link.
Arguments
portNum SGMII port number for which settings must be configured *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII Master mode enabled.
Writes
CPSGMII_CONTROL_REG_MASTER=1
Example
Uint32 portNum = 1; CSL_SGMII_enableMasterMode (portNum);
void CSL_SGMII_disableMasterMode | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_disableMasterMode
Description
This function configures the CPSGMII in 'Slave' mode or in other words disables the master mode for the port specified.
Arguments
portNum SGMII port number for which settings must be configured. *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII Master mode disabled, slave mode enabled.
Writes
CPSGMII_CONTROL_REG_MASTER=0
Example
Uint32 portNum = 1; CSL_SGMII_disableMasterMode (portNum);
Uint32 CSL_SGMII_isMasterModeEnabled | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_isMasterModeEnabled
Description
This function reads the 'MASTER' bit of the CPSGMII Control register and returns 1 to indicate that the CPSGMII is configured in 'Master' mode and 0 otherwise to indicate 'Slave' mode.
Arguments
portNum SGMII port number for which settings must be retrieved. *
Return Value Uint32
Pre Condition
None
Post Condition
None
Reads
CPSGMII_CONTROL_REG_MASTER
Example
Uint32 portNum = 1; if (!CSL_SGMII_isMasterModeEnabled (portNum)) { // Slave Mode } else { // Master mode }
void CSL_SGMII_enableLoopback | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_enableLoopback
Description
This function configures the CPSGMII in internal loopback mode for the port number specified.
Arguments
portNum SGMII port number for which loopback must be enabled. *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII internal loopback mode enabled.
Writes
CPSGMII_CONTROL_REG_LOOPBACK=1
Example
Uint32 portNum = 1; CSL_SGMII_enableLoopback (portNum);
void CSL_SGMII_disableLoopback | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_disableLoopback
Description
This function disables CPSGMII internal loopback for the port specified.
Arguments
portNum SGMII port number for which loopback must be disabled *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII loopback mode disabled.
Writes
CPSGMII_CONTROL_REG_LOOPBACK=0
Example
Uint32 portNum = 1; CSL_SGMII_disableLoopback (portNum);
Uint32 CSL_SGMII_isLoopbackModeEnabled | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_isLoopbackModeEnabled
Description
This function reads the 'LOOPBACK' bit of the CPSGMII Control register and returns 1 to indicate that the CPSGMII is configured in 'Loopback' mode and 0 otherwise.
Arguments
portNum SGMII port number for which loopback mode must be read. *
Return Value Uint32
Pre Condition
None
Post Condition
None
Reads
CPSGMII_CONTROL_REG_LOOPBACK
Example
Uint32 portNum = 1; if (CSL_SGMII_isLoopbackModeEnabled (portNum)) { // Loopback mode enabled. }
void CSL_SGMII_restartAutoNegotiation | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_restartAutoNegotiation
Description
This function restarts link auto-negotiation process for the port specified.
Arguments
portNum SGMII port number for which the operation must be performed *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII auto-negotiation restarted.
Writes
CPSGMII_CONTROL_REG_MR_AN_RESTART=1, CPSGMII_CONTROL_REG_MR_AN_RESTART=0
Example
Uint32 portNum = 1; CSL_SGMII_restartAutoNegotiation (portNum);
void CSL_SGMII_enableAutoNegotiation | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_enableAutoNegotiation
Description
This function enables auto-negotiation process for the port specified.
Arguments
portNum SGMII port number for which the operation must be performed. *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII auto-negotiation enabled.
Writes
CPSGMII_CONTROL_REG_MR_AN_ENABLE=1
Example
Uint32 portNum = 1; CSL_SGMII_enableAutoNegotiation (portNum);
void CSL_SGMII_disableAutoNegotiation | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_disableAutoNegotiation
Description
This function disables auto-negotiation process for the port number specified.
Arguments
portNum SGMII port number for which the operation must be performed *
Return Value
None
Pre Condition
None
Post Condition
CPSGMII auto-negotiation disabled.
Writes
CPSGMII_CONTROL_REG_MR_AN_ENABLE=0
Example
Uint32 portNum = 1; CSL_SGMII_disableAutoNegotiation (portNum);
Uint32 CSL_SGMII_isAutoNegotiationEnabled | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum | ||
) |
============================================================================
CSL_SGMII_isAutoNegotiationEnabled
Description
This function reads the 'MR_AN_ENABLE' bit of the CPSGMII Control register and returns 1 to indicate that the CPSGMII is configured in 'auto-negotiate' mode and 0 otherwise.
Arguments
portNum SGMII port number for which autonegotiation must be enabled. *
Return Value Uint32
Pre Condition
None
Post Condition
None
Reads
CPSGMII_CONTROL_REG_MR_AN_ENABLE
Example
Uint32 portNum = 1; if (CSL_SGMII_isAutoNegotiationEnabled (portNum)) { // auto-negotiation enabled. }
void CSL_SGMII_getStatus | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum, | ||
CSL_SGMII_STATUS * | pSgmiiStatus | ||
) |
============================================================================
CSL_SGMII_getStatus
Description
This function retrieves the SGMII status information from the hardware. The status info returned by this function are valid only if the 'bIsLocked' bit of status info is set to 1 and must be disregarded otherwise.
Arguments
portNum SGMII port number for which status must be retrieved. * pSgmiiStatus CSL_SGMII_STATUS structure pointer that needs to be * populated with link status information. *
Return Value None
Pre Condition
None
Post Condition
None
Reads
CPSGMII_STATUS_REG_LINK, CPSGMII_STATUS_REG_AN_ERROR, CPSGMII_STATUS_REG_MR_AN_COMPLETE, CPSGMII_STATUS_REG_LOCK
Example
Uint32 portNum = 1; CSL_SGMII_STATUS sgmiiStatus; // Get link status info CSL_SGMII_getStatus (portNum, &sgmiiStatus);
void CSL_SGMII_setAdvAbility | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum, | ||
CSL_SGMII_ADVABILITY * | pSgmiiAdvAbility | ||
) |
============================================================================
CSL_SGMII_setAdvAbility
Description
This function sets up the 'MR_ADV_ABILITY' register as per the input specified to this function in 'pSgmiiAdvAbility' param.
Arguments
portNum SGMII port number for which configuration must be done. * pSgmiiAdvAbility CSL_SGMII_ADVABILITY input params structure that contains * the advertised ability configuration that needs to be * populated to the hardware registers. *
Return Value None
Pre Condition
None
Post Condition
MR_ADV_ABILITY register setup accordingly.
Writes
CPSGMII_MR_ADV_ABILITY_REG
Example
Uint32 portNum = 1; CSL_SGMII_STATUS sgmiiAdvAbility; sgmiiAdvAbility.bLinkUp = 1; sgmiiAdvAbility.duplexMode = CSL_SGMII_FULL_DUPLEX; sgmiiAdvAbility.linkSpeed = CSL_SGMII_1000_MBPS; sgmiiAdvAbility.sgmiimode = CSL_SGMII_MODE_SGMII; // Configure SGMII Advertised ability info CSL_SGMII_setAdvAbility (portNum, &sgmiiAdvAbility);
void CSL_SGMII_getAdvAbility | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum, | ||
CSL_SGMII_ADVABILITY * | pSgmiiAdvAbility | ||
) |
============================================================================
CSL_SGMII_getAdvAbility
Description
This function rerturns the contents of 'MR_ADV_ABILITY' register in the output parameter 'pSgmiiAdvAbility'.
Arguments
portNum SGMII port number for which the read operation must be done. * pSgmiiAdvAbility CSL_SGMII_ADVABILITY output param structure pointer * that needs to be populated with advertised ability * register contents. *
Return Value None
Pre Condition
None
Post Condition
None
Reads
CPSGMII_MR_ADV_ABILITY_REG
Example
* CSL_SGMII_STATUS sgmiiAdvAbility; Uint32 portNum = 1; // Get SGMII Advertised ability info CSL_SGMII_getAdvAbility (portNum, &sgmiiAdvAbility);
void CSL_SGMII_getLinkPartnerAdvAbility | ( | CSL_CpsgmiiRegs * | hCpSgmiiRegs, |
Uint32 | portNum, | ||
CSL_SGMII_ADVABILITY * | pSgmiiAdvAbility | ||
) |
============================================================================
CSL_SGMII_getLinkPartnerAdvAbility
Description
This function rerturns the contents of 'MR_LP_ADV_ABILITY' register in the output parameter 'pSgmiiAdvAbility'.
Arguments
portNum SGMII port number for which read operation must be done * pSgmiiAdvAbility CSL_SGMII_ADVABILITY output param structure pointer * that needs to be populated with link partnet advertised * ability register contents. *
Return Value None
Pre Condition
None
Post Condition
None
Reads
CPSGMII_MR_LP_ADV_ABILITY_REG
Example
* CSL_SGMII_STATUS sgmiiAdvAbility; Uint32 portNum = 1; // Get SGMII Advertised ability info CSL_SGMII_getLinkPartnerAdvAbility (portNum, &sgmiiAdvAbility);