![]() |
PDK Documentation
|
Files | |
| file | csl_dssVideoPort.h |
| DSS Video Port CSL FL interface file. | |
Data Structures | |
| struct | CSL_DssVpGammaCfg |
| Gamma Correction configuration for DSS Video Port Output. More... | |
| struct | CSL_DssVpLcdTdmCfg |
| LCD Configuration for Time Division Multiplexing. More... | |
| struct | CSL_DssVpLcdSignalPolarityCfg |
| Polarity of Active Video, Pixel Clock, HSync and VSync signals for the LCD. More... | |
| struct | CSL_DssVpLcdAdvSignalCfg |
| Advance Signal Configuration for the LCD. More... | |
| struct | CSL_DssVpLcdOpTimingCfg |
| Timing configuration for the LCD output. More... | |
| struct | CSL_DssVpLcdBlankTimingCfg |
| Blanking Timing parameters for the LCD. More... | |
Functions | |
| void | CSL_dssVpEnable (CSL_dss_vpRegs *vpRegs, uint32_t enable) |
| Enable the DSS Video Port. More... | |
| void | CSL_dssVpSetGoBit (CSL_dss_vpRegs *vpRegs) |
| GO Command for the VP output. It is used to synchronize the pipelines associated with the VP output. More... | |
| void | CSL_dssVpSetLcdTdmConfig (CSL_dss_vpRegs *vpRegs, const CSL_DssVpLcdTdmCfg *lcdTdmCfg) |
| Configure the LCD TDM(Time division multiplexing) parameters. More... | |
| void | CSL_dssVpSetLcdLineNum (CSL_dss_vpRegs *vpRegs, uint32_t lineNum) |
| Set the Line Number at which the interrupt should be generated. More... | |
| int32_t | CSL_dssVpSetLcdOpTimingConfig (CSL_dss_vpRegs *vpRegs, const CSL_DssVpLcdOpTimingCfg *lcdCfg) |
| Configure the LCD Timing parameters. More... | |
| int32_t | CSL_dssVpSetLcdBlankTiming (CSL_dss_vpRegs *vpRegs, const CSL_DssVpLcdBlankTimingCfg *blankCfg, uint32_t dvoFormat, uint32_t scanFormat, uint32_t isCustomTiming) |
| Configure the LCD Blank Timing parameters. More... | |
| void | CSL_dssVpSetLcdAdvSignalConfig (CSL_dss_vpRegs *vpRegs, const CSL_DssVpLcdAdvSignalCfg *advSignalCfg) |
| Configure the advance LCD Signal parameters. More... | |
| void | CSL_dssVpSetLcdSignalPolarityConfig (CSL_dss_vpRegs *vpRegs, const CSL_DssVpLcdSignalPolarityCfg *polarityCfg) |
| Configure the Polarity of LCD signals(HSYNC, VSYNC, PCLK, Data) More... | |
| void | CSL_dssVpEnableTvGamma (CSL_dss_vpRegs *vpRegs, const CSL_DssVpGammaCfg *gammaCfg) |
| Enable/Bypass TV Gamma Table. More... | |
| void | CSL_dssVpSetCSCCoeff (CSL_dss_vpRegs *vpRegs, const CSL_DssCscCoeff *cscCoeff, uint32_t cscPos, uint32_t cscEnable) |
| Configure the coefficients for Color Space Conversion. More... | |
| void | CSL_dssVpSetSafetySignSeedVal (CSL_dss_vpRegs *vpRegs, uint32_t signSeedVal) |
| Set the seed value for the signature calculation. More... | |
| void | CSL_dssVpSetSafetyReferenceSign (CSL_dss_vpRegs *vpRegs, uint32_t referenceSign, uint32_t regionId) |
| Set the reference safety signature for data correctness check. More... | |
| void | CSL_dssVpSetSafetyChkConfig (CSL_dss_vpRegs *vpRegs, const CSL_DssSafetyChkCfg *safetyCfg, uint32_t regionId) |
| Configure the Safety Check parameters. More... | |
| uint32_t | CSL_dssVpGetSafetySign (const CSL_dss_vpRegs *vpRegs, uint32_t regionId) |
| Get the Safety Signature of the sub region. More... | |
| void | CSL_dssVpStallModeEnable (CSL_dss_vpRegs *vpRegs, uint32_t enable, uint32_t stallModeType) |
| Enable/disable the Video Port stall mode. More... | |
| static void | CSL_dssVpGammaCfgInit (CSL_DssVpGammaCfg *gammaCfg) |
| CSL_DssVpGammaCfg structure init function. More... | |
| static void | CSL_dssVpLcdTdmCfgInit (CSL_DssVpLcdTdmCfg *tdmCfg) |
| CSL_DssVpLcdTdmCfg structure init function. More... | |
| static void | CSL_dssVpLcdSignalPolarityCfgInit (CSL_DssVpLcdSignalPolarityCfg *polarityCfg) |
| CSL_DssVpLcdSignalPolarityCfg structure init function. More... | |
| static void | CSL_dssVpLcdAdvSignalCfgInit (CSL_DssVpLcdAdvSignalCfg *advSignalCfg) |
| CSL_DssVpLcdAdvSignalCfg structure init function. More... | |
| static void | CSL_dssVpLcdOpTimingCfgInit (CSL_DssVpLcdOpTimingCfg *lcdCfg) |
| CSL_DssVpLcdOpTimingCfg structure init function. More... | |
| static void | CSL_dssVpLcdBlankTimingCfgInit (CSL_DssVpLcdBlankTimingCfg *blankCfg) |
| CSL_DssVpLcdBlankTimingCfg structure init function. More... | |
Typedefs | |
| typedef CSL_dss_vp1Regs | CSL_dss_vpRegs |
| DSS Video Port Registers. More... | |
Video Port CSC Position | |
DSS Video Port Color Space Conversion block position wrt Gamma block | |
| #define | CSL_DSS_VP_CSC_POS_AFTER_GAMMA ((uint32_t) CSL_DSS_VP1_CONFIG_COLORCONVPOS_VAL_AFTERGAMMA) |
| CSC block is after GAMMA correction. More... | |
| #define | CSL_DSS_VP_CSC_POS_BEFORE_GAMMA ((uint32_t) CSL_DSS_VP1_CONFIG_COLORCONVPOS_VAL_BEFOREGAMMA) |
| CSC block is before GAMMA correction. More... | |
TDM Mode Unused Bits Level | |
| #define | CSL_DSS_VP_TDM_UNUSED_BITS_LEVEL_LOW ((uint32_t) CSL_DSS_VP1_CONTROL_TDMUNUSEDBITS_VAL_LOWLEVEL) |
| Low level. More... | |
| #define | CSL_DSS_VP_TDM_UNUSED_BITS_LEVEL_HIGH ((uint32_t) CSL_DSS_VP1_CONTROL_TDMUNUSEDBITS_VAL_HIGHLEVEL) |
| High level. More... | |
| #define | CSL_DSS_VP_TDM_UNUSED_BITS_LEVEL_UNCHANGED ((uint32_t) CSL_DSS_VP1_CONTROL_TDMUNUSEDBITS_VAL_UNCHANGED) |
| Unchanged level. More... | |
TDM Cycle format | |
| #define | CSL_DSS_VP_TDM_CYCLE_1PERPIXEL ((uint32_t) CSL_DSS_VP1_CONTROL_TDMCYCLEFORMAT_VAL_1CYCPERPIX) |
| 1 cycle per pixel More... | |
| #define | CSL_DSS_VP_TDM_CYCLE_2PERPIXEL ((uint32_t) CSL_DSS_VP1_CONTROL_TDMCYCLEFORMAT_VAL_2CYCPERPIX) |
| 2 cycles per pixel More... | |
| #define | CSL_DSS_VP_TDM_CYCLE_3PERPIXEL ((uint32_t) CSL_DSS_VP1_CONTROL_TDMCYCLEFORMAT_VAL_3CYCPERPIX) |
| 3 cycles per pixel More... | |
| #define | CSL_DSS_VP_TDM_CYCLE_3PER2PIXEL ((uint32_t) CSL_DSS_VP1_CONTROL_TDMCYCLEFORMAT_VAL_3CYCPER2PIX) |
| 3 cycles per 2 pixels More... | |
Output interface width in TDM mode | |
| #define | CSL_DSS_VP_TDM_PARALLEL_OUTPUT_8BIT ((uint32_t) CSL_DSS_VP1_CONTROL_TDMPARALLELMODE_VAL_8BPARAINT) |
| 8-bit parallel output interface selected More... | |
| #define | CSL_DSS_VP_TDM_PARALLEL_OUTPUT_9BIT ((uint32_t) CSL_DSS_VP1_CONTROL_TDMPARALLELMODE_VAL_9BPARAINT) |
| 9-bit parallel output interface selected More... | |
| #define | CSL_DSS_VP_TDM_PARALLEL_OUTPUT_12BIT ((uint32_t) CSL_DSS_VP1_CONTROL_TDMPARALLELMODE_VAL_12BPARAINT) |
| 12-bit parallel output interface selected More... | |
| #define | CSL_DSS_VP_TDM_PARALLEL_OUTPUT_16BIT ((uint32_t) CSL_DSS_VP1_CONTROL_TDMPARALLELMODE_VAL_16BPARAINT) |
| 16-bit parallel output interface selected More... | |
LCD HSync VSync Alignment | |
| #define | CSL_DSS_VP_HVSYNC_NOT_ALIGNED ((uint32_t) CSL_DSS_VP1_POL_FREQ_ALIGN_VAL_NOTALIGNED) |
| HSYNC and VSYNC are not aligned. More... | |
| #define | CSL_DSS_VP_HVSYNC_ALIGNED ((uint32_t) CSL_DSS_VP1_POL_FREQ_ALIGN_VAL_ALIGNED) |
| HSYNC and VSYNC assertions are aligned. More... | |
LCD HSYNC/VSYNC pixel clock control | |
| #define | CSL_DSS_VP_HVCLK_CONTROL_OFF ((uint32_t) CSL_DSS_VP1_POL_FREQ_ONOFF_VAL_DOPEDPCK) |
| HSYNC and VSYNC are driven on opposite edges of the pixel clock than pixel data. More... | |
| #define | CSL_DSS_VP_HVCLK_CONTROL_ON ((uint32_t) CSL_DSS_VP1_POL_FREQ_ONOFF_VAL_DBIT16) |
| HSYNC and VSYNC are driven according to hVClkRiseFall value. More... | |
Delta Lines Per Panel | |
Delta size value of the odd field compared to the even field | |
| #define | CSL_DSS_VP_LPP_DELTA_ZERO ((uint32_t) CSL_DSS_VP1_SIZE_SCREEN_DELTA_LPP_VAL_SAME) |
| Odd field has same size as even. More... | |
| #define | CSL_DSS_VP_LPP_DELTA_PLUSONE ((uint32_t) CSL_DSS_VP1_SIZE_SCREEN_DELTA_LPP_VAL_PLUSONE) |
| Odd field is equal to even field + 1. More... | |
| #define | CSL_DSS_VP_LPP_DELTA_MINUSONE ((uint32_t) CSL_DSS_VP1_SIZE_SCREEN_DELTA_LPP_VAL_MINUSONE) |
| Odd field is equal to even field - 1. More... | |
Video Port First Field | |
| #define | CSL_DSS_VP_FID_FIRST_EVEN ((uint32_t) CSL_DSS_VP1_CONFIG_FIDFIRST_VAL_EVEN) |
| First field is even. More... | |
| #define | CSL_DSS_VP_FID_FIRST_ODD ((uint32_t) CSL_DSS_VP1_CONFIG_FIDFIRST_VAL_ODD) |
| First field is odd. More... | |
Video Port Stall Mode | |
| #define | CSL_DSS_VP_STALL_MODE_COMMAND ((uint32_t) CSL_DSS_VP1_CONTROL_STALLMODETYPE_VAL_COMMANDMODE) |
| Stall mode is command. More... | |
| #define | CSL_DSS_VP_STALL_MODE_VIDEO ((uint32_t) CSL_DSS_VP1_CONTROL_STALLMODETYPE_VAL_VIDEOMODE) |
| Stall mode is video. More... | |
DSS Video Port Safety Region Id | |
| #define | CSL_DSS_VP_SAFETY_REGION_0 ((uint32_t) 0x0U) |
| Safety Region 0. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_1 ((uint32_t) 0x1U) |
| Safety Region 1. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_2 ((uint32_t) 0x2U) |
| Safety Region 2. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_3 ((uint32_t) 0x3U) |
| Safety Region 3. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_4 ((uint32_t) 0x4U) |
| Safety Region 4. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_5 ((uint32_t) 0x5U) |
| Safety Region 5. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_6 ((uint32_t) 0x6U) |
| Safety Region 6. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_7 ((uint32_t) 0x7U) |
| Safety Region 7. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_MAX ((uint32_t) 0x8U) |
| Safety Region Max. More... | |
| #define | CSL_DSS_VP_SAFETY_REGION_INVALID ((uint32_t) 0xFFU) |
| Invalid Safety Region. More... | |
| #define CSL_DSS_VP_CSC_POS_AFTER_GAMMA ((uint32_t) CSL_DSS_VP1_CONFIG_COLORCONVPOS_VAL_AFTERGAMMA) |
CSC block is after GAMMA correction.
| #define CSL_DSS_VP_CSC_POS_BEFORE_GAMMA ((uint32_t) CSL_DSS_VP1_CONFIG_COLORCONVPOS_VAL_BEFOREGAMMA) |
CSC block is before GAMMA correction.
| #define CSL_DSS_VP_TDM_UNUSED_BITS_LEVEL_LOW ((uint32_t) CSL_DSS_VP1_CONTROL_TDMUNUSEDBITS_VAL_LOWLEVEL) |
Low level.
| #define CSL_DSS_VP_TDM_UNUSED_BITS_LEVEL_HIGH ((uint32_t) CSL_DSS_VP1_CONTROL_TDMUNUSEDBITS_VAL_HIGHLEVEL) |
High level.
| #define CSL_DSS_VP_TDM_UNUSED_BITS_LEVEL_UNCHANGED ((uint32_t) CSL_DSS_VP1_CONTROL_TDMUNUSEDBITS_VAL_UNCHANGED) |
Unchanged level.
| #define CSL_DSS_VP_TDM_CYCLE_1PERPIXEL ((uint32_t) CSL_DSS_VP1_CONTROL_TDMCYCLEFORMAT_VAL_1CYCPERPIX) |
1 cycle per pixel
| #define CSL_DSS_VP_TDM_CYCLE_2PERPIXEL ((uint32_t) CSL_DSS_VP1_CONTROL_TDMCYCLEFORMAT_VAL_2CYCPERPIX) |
2 cycles per pixel
| #define CSL_DSS_VP_TDM_CYCLE_3PERPIXEL ((uint32_t) CSL_DSS_VP1_CONTROL_TDMCYCLEFORMAT_VAL_3CYCPERPIX) |
3 cycles per pixel
| #define CSL_DSS_VP_TDM_CYCLE_3PER2PIXEL ((uint32_t) CSL_DSS_VP1_CONTROL_TDMCYCLEFORMAT_VAL_3CYCPER2PIX) |
3 cycles per 2 pixels
| #define CSL_DSS_VP_TDM_PARALLEL_OUTPUT_8BIT ((uint32_t) CSL_DSS_VP1_CONTROL_TDMPARALLELMODE_VAL_8BPARAINT) |
8-bit parallel output interface selected
| #define CSL_DSS_VP_TDM_PARALLEL_OUTPUT_9BIT ((uint32_t) CSL_DSS_VP1_CONTROL_TDMPARALLELMODE_VAL_9BPARAINT) |
9-bit parallel output interface selected
| #define CSL_DSS_VP_TDM_PARALLEL_OUTPUT_12BIT ((uint32_t) CSL_DSS_VP1_CONTROL_TDMPARALLELMODE_VAL_12BPARAINT) |
12-bit parallel output interface selected
| #define CSL_DSS_VP_TDM_PARALLEL_OUTPUT_16BIT ((uint32_t) CSL_DSS_VP1_CONTROL_TDMPARALLELMODE_VAL_16BPARAINT) |
16-bit parallel output interface selected
| #define CSL_DSS_VP_HVSYNC_NOT_ALIGNED ((uint32_t) CSL_DSS_VP1_POL_FREQ_ALIGN_VAL_NOTALIGNED) |
HSYNC and VSYNC are not aligned.
| #define CSL_DSS_VP_HVSYNC_ALIGNED ((uint32_t) CSL_DSS_VP1_POL_FREQ_ALIGN_VAL_ALIGNED) |
HSYNC and VSYNC assertions are aligned.
| #define CSL_DSS_VP_HVCLK_CONTROL_OFF ((uint32_t) CSL_DSS_VP1_POL_FREQ_ONOFF_VAL_DOPEDPCK) |
HSYNC and VSYNC are driven on opposite edges of the pixel clock than pixel data.
| #define CSL_DSS_VP_HVCLK_CONTROL_ON ((uint32_t) CSL_DSS_VP1_POL_FREQ_ONOFF_VAL_DBIT16) |
HSYNC and VSYNC are driven according to hVClkRiseFall value.
| #define CSL_DSS_VP_LPP_DELTA_ZERO ((uint32_t) CSL_DSS_VP1_SIZE_SCREEN_DELTA_LPP_VAL_SAME) |
Odd field has same size as even.
| #define CSL_DSS_VP_LPP_DELTA_PLUSONE ((uint32_t) CSL_DSS_VP1_SIZE_SCREEN_DELTA_LPP_VAL_PLUSONE) |
Odd field is equal to even field + 1.
| #define CSL_DSS_VP_LPP_DELTA_MINUSONE ((uint32_t) CSL_DSS_VP1_SIZE_SCREEN_DELTA_LPP_VAL_MINUSONE) |
Odd field is equal to even field - 1.
| #define CSL_DSS_VP_FID_FIRST_EVEN ((uint32_t) CSL_DSS_VP1_CONFIG_FIDFIRST_VAL_EVEN) |
First field is even.
| #define CSL_DSS_VP_FID_FIRST_ODD ((uint32_t) CSL_DSS_VP1_CONFIG_FIDFIRST_VAL_ODD) |
First field is odd.
| #define CSL_DSS_VP_STALL_MODE_COMMAND ((uint32_t) CSL_DSS_VP1_CONTROL_STALLMODETYPE_VAL_COMMANDMODE) |
Stall mode is command.
| #define CSL_DSS_VP_STALL_MODE_VIDEO ((uint32_t) CSL_DSS_VP1_CONTROL_STALLMODETYPE_VAL_VIDEOMODE) |
Stall mode is video.
| #define CSL_DSS_VP_SAFETY_REGION_0 ((uint32_t) 0x0U) |
Safety Region 0.
| #define CSL_DSS_VP_SAFETY_REGION_1 ((uint32_t) 0x1U) |
Safety Region 1.
| #define CSL_DSS_VP_SAFETY_REGION_2 ((uint32_t) 0x2U) |
Safety Region 2.
| #define CSL_DSS_VP_SAFETY_REGION_3 ((uint32_t) 0x3U) |
Safety Region 3.
| #define CSL_DSS_VP_SAFETY_REGION_4 ((uint32_t) 0x4U) |
Safety Region 4.
| #define CSL_DSS_VP_SAFETY_REGION_5 ((uint32_t) 0x5U) |
Safety Region 5.
| #define CSL_DSS_VP_SAFETY_REGION_6 ((uint32_t) 0x6U) |
Safety Region 6.
| #define CSL_DSS_VP_SAFETY_REGION_7 ((uint32_t) 0x7U) |
Safety Region 7.
| #define CSL_DSS_VP_SAFETY_REGION_MAX ((uint32_t) 0x8U) |
Safety Region Max.
| #define CSL_DSS_VP_SAFETY_REGION_INVALID ((uint32_t) 0xFFU) |
Invalid Safety Region.
| typedef CSL_dss_vp1Regs CSL_dss_vpRegs |
DSS Video Port Registers.
DSS7 has four identical VP blocks, hence define a generic structure to have common APIs
| void CSL_dssVpEnable | ( | CSL_dss_vpRegs * | vpRegs, |
| uint32_t | enable | ||
| ) |
Enable the DSS Video Port.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| enable | Enable or disable the Video Port TRUE: Enable FALSE: Disable |
| void CSL_dssVpSetGoBit | ( | CSL_dss_vpRegs * | vpRegs | ) |
GO Command for the VP output. It is used to synchronize the pipelines associated with the VP output.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| void CSL_dssVpSetLcdTdmConfig | ( | CSL_dss_vpRegs * | vpRegs, |
| const CSL_DssVpLcdTdmCfg * | lcdTdmCfg | ||
| ) |
Configure the LCD TDM(Time division multiplexing) parameters.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| lcdTdmCfg | Pointer to the CSL_DssVpLcdTdmCfg structure. This parameter should not be NULL |
| void CSL_dssVpSetLcdLineNum | ( | CSL_dss_vpRegs * | vpRegs, |
| uint32_t | lineNum | ||
| ) |
Set the Line Number at which the interrupt should be generated.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| lineNum | Line Number that should be programmed in the register |
| int32_t CSL_dssVpSetLcdOpTimingConfig | ( | CSL_dss_vpRegs * | vpRegs, |
| const CSL_DssVpLcdOpTimingCfg * | lcdCfg | ||
| ) |
Configure the LCD Timing parameters.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| lcdCfg | Pointer to the CSL_DssVpLcdOpTimingCfg structure. This parameter should not be NULL |
| int32_t CSL_dssVpSetLcdBlankTiming | ( | CSL_dss_vpRegs * | vpRegs, |
| const CSL_DssVpLcdBlankTimingCfg * | blankCfg, | ||
| uint32_t | dvoFormat, | ||
| uint32_t | scanFormat, | ||
| uint32_t | isCustomTiming | ||
| ) |
Configure the LCD Blank Timing parameters.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| blankCfg | Pointer to the CSL_DssVpLcdBlankTimingCfg structure. This parameter should not be NULL |
| dvoFormat | Digital output format. For valid values see Fvid2_DVFormat |
| scanFormat | Scan format. For valid values see Fvid2_ScanFormat |
| isCustomTiming | Variable to determine whether custom timing is used. It should always be set to TRUE when this API is called by application. |
| void CSL_dssVpSetLcdAdvSignalConfig | ( | CSL_dss_vpRegs * | vpRegs, |
| const CSL_DssVpLcdAdvSignalCfg * | advSignalCfg | ||
| ) |
Configure the advance LCD Signal parameters.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| advSignalCfg | Pointer to CSL_DssVpLcdAdvSignalCfg structure. This parameter should not be NULL |
| void CSL_dssVpSetLcdSignalPolarityConfig | ( | CSL_dss_vpRegs * | vpRegs, |
| const CSL_DssVpLcdSignalPolarityCfg * | polarityCfg | ||
| ) |
Configure the Polarity of LCD signals(HSYNC, VSYNC, PCLK, Data)
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| polarityCfg | Pointer to CSL_DssVpLcdSignalPolarityCfg structure. This parameter should not be NULL |
| void CSL_dssVpEnableTvGamma | ( | CSL_dss_vpRegs * | vpRegs, |
| const CSL_DssVpGammaCfg * | gammaCfg | ||
| ) |
Enable/Bypass TV Gamma Table.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| gammaCfg | Pointer to CSL_DssVpGammaCfg structure. This parameter should not be NULL |
| void CSL_dssVpSetCSCCoeff | ( | CSL_dss_vpRegs * | vpRegs, |
| const CSL_DssCscCoeff * | cscCoeff, | ||
| uint32_t | cscPos, | ||
| uint32_t | cscEnable | ||
| ) |
Configure the coefficients for Color Space Conversion.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| cscCoeff | Pointer to CSL_DssCscCoeff structure. This parameter should not be NULL |
| cscPos | Position of CSC block wrt GAMMA module. Refer CSL_DssVpCscPos for values |
| cscEnable | CSC Enable TRUE: Enable CSC FALSE: Disable CSC |
| void CSL_dssVpSetSafetySignSeedVal | ( | CSL_dss_vpRegs * | vpRegs, |
| uint32_t | signSeedVal | ||
| ) |
Set the seed value for the signature calculation.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| signSeedVal | Signature Seed Value to be Set |
| void CSL_dssVpSetSafetyReferenceSign | ( | CSL_dss_vpRegs * | vpRegs, |
| uint32_t | referenceSign, | ||
| uint32_t | regionId | ||
| ) |
Set the reference safety signature for data correctness check.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| referenceSign | Reference Safety Signature |
| regionId | Region for which safety check should be done. Refer CSL_DssVpSafetyRegionId for values |
| void CSL_dssVpSetSafetyChkConfig | ( | CSL_dss_vpRegs * | vpRegs, |
| const CSL_DssSafetyChkCfg * | safetyCfg, | ||
| uint32_t | regionId | ||
| ) |
Configure the Safety Check parameters.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| safetyCfg | Pointer to CSL_DssSafetyChkCfg structure. This parameter should not be NULL |
| regionId | Region for which safety check should be done. Refer CSL_DssVpSafetyRegionId for values |
| uint32_t CSL_dssVpGetSafetySign | ( | const CSL_dss_vpRegs * | vpRegs, |
| uint32_t | regionId | ||
| ) |
Get the Safety Signature of the sub region.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| regionId | Region for which safety check should be done. Refer CSL_DssVpSafetyRegionId for values |
| void CSL_dssVpStallModeEnable | ( | CSL_dss_vpRegs * | vpRegs, |
| uint32_t | enable, | ||
| uint32_t | stallModeType | ||
| ) |
Enable/disable the Video Port stall mode.
| vpRegs | Pointer to a CSL_dss_vpRegs structure containing the video port configuration |
| enable | Enable or disable the stall mode of Video Port TRUE: Enable FALSE: Disable |
| stallModeType | Stall Mode Type Refer CSL_DssVpStallMode for values |
|
inlinestatic |
CSL_DssVpGammaCfg structure init function.
| gammaCfg | Pointer to CSL_DssVpGammaCfg structure |
|
inlinestatic |
CSL_DssVpLcdTdmCfg structure init function.
| tdmCfg | Pointer to CSL_DssVpLcdTdmCfg structure |
|
inlinestatic |
CSL_DssVpLcdSignalPolarityCfg structure init function.
| polarityCfg | Pointer to CSL_DssVpLcdSignalPolarityCfg structure |
|
inlinestatic |
CSL_DssVpLcdAdvSignalCfg structure init function.
| advSignalCfg | Pointer to CSL_DssVpLcdAdvSignalCfg structure |
|
inlinestatic |
CSL_DssVpLcdOpTimingCfg structure init function.
| lcdCfg | Pointer to CSL_DssVpLcdOpTimingCfg structure |
|
inlinestatic |
CSL_DssVpLcdBlankTimingCfg structure init function.
| blankCfg | Pointer to CSL_DssVpLcdBlankTimingCfg structure |