PDK Documentation
CSI TX Sub-System

Introduction

Files

file  csitx_ss.h
 This file contains the prototypes of the APIs present in the device abstraction layer file of CSI TX SS. This also contains some related macros.
 

Data Structures

struct  CSL_CsitxRevisionId
 Structure for accessing Revision ID and Core Release Info. of CSI Tx module. More...
 
struct  CSL_CsitxColorbarGenCfg
 Structure for Color-bar generation configurations. More...
 
struct  CSL_CsitxRetransCfg
 Structure for re-transmission streams configurations. More...
 
struct  CSL_CsitxStrmStatus
 Structure for streams status. More...
 
struct  CSL_CsitxDMAConfig
 Structure for PSI-L/DMA configuration for CSI Tx SS. More...
 

Functions

void CSL_csitxGetRevisionId (const CSL_csi_tx_ifRegs *ifRegisters, CSL_CsitxRevisionId *revId)
 This API is used get the CSI Tx revision ID. More...
 
int32_t CSL_csitxColorbarCfg (const CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxColorbarGenCfg *cfg)
 This API is used program the color bar generation parameters. More...
 
void CSL_csitxEnableColorbarGen (CSL_csi_tx_ifRegs *ifRegisters, uint32_t enable)
 This API is used enable/disable Color-bar generation. More...
 
int32_t CSL_csitxRetransCfg (const CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxRetransCfg *cfg)
 This API is used program the re-transmission streams parameters. More...
 
void CSL_csitxAssertPixelIfReset (CSL_csi_tx_ifRegs *ifRegisters, uint32_t assert)
 This API is used assert/de-assert reset for pixel interface. More...
 
void CSL_csitxGetStrmStatus (const CSL_csi_tx_ifRegs *ifRegisters, CSL_CsitxStrmStatus *status)
 This API is used get the current stream status. More...
 
int32_t CSL_csitxFrmToFrmDelayCfg (const CSL_csi_tx_ifRegs *ifRegisters, const uint32_t vc, const uint32_t delay)
 This API is used program frame to frame delay. More...
 
int32_t CSL_csitxConfigDMA (CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxDMAConfig *cfg)
 This API is used to configure DMA/PSIL thread. More...
 

Macros

#define CSL_CSITX_PSI_L_THREAD_NUM_MAX   ((uint32_t)32U)
 Maximum number of PSI-L Threads supported by CSI Tx SS. More...
 

CSITX DMA Data Size Shift

DMA data size shift for unpacking.

#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_8BITS   (0U)
 DMA Data Size Shift: 8 bits. More...
 
#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_16BITS   (1U)
 DMA Data Size Shift: 16 bits. More...
 
#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_32BITS   (2U)
 DMA Data Size Shift: 32 bits. More...
 

CSITX YUV422 Mode

Storage class specifier for YUV422 data.

#define CSL_CSITX_YUV422_MODE_UYVY   (0U)
 YUV422 Mode: UYVY. More...
 
#define CSL_CSITX_YUV422_MODE_YUYV   (2U)
 YUV422 Mode: VYUY. More...
 
#define CSL_CSITX_YUV422_MODE_VYUY   (1U)
 YUV422 Mode: YUYV. More...
 
#define CSL_CSITX_YUV422_MODE_YVYU   (3U)
 YUV422 Mode: YVYU. More...
 

Macro Definition Documentation

◆ CSL_CSITX_PSI_L_THREAD_NUM_MAX

#define CSL_CSITX_PSI_L_THREAD_NUM_MAX   ((uint32_t)32U)

Maximum number of PSI-L Threads supported by CSI Tx SS.

◆ CSL_CSITX_DMA_DATA_SIZE_SHIFT_8BITS

#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_8BITS   (0U)

DMA Data Size Shift: 8 bits.

◆ CSL_CSITX_DMA_DATA_SIZE_SHIFT_16BITS

#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_16BITS   (1U)

DMA Data Size Shift: 16 bits.

◆ CSL_CSITX_DMA_DATA_SIZE_SHIFT_32BITS

#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_32BITS   (2U)

DMA Data Size Shift: 32 bits.

◆ CSL_CSITX_YUV422_MODE_UYVY

#define CSL_CSITX_YUV422_MODE_UYVY   (0U)

YUV422 Mode: UYVY.

◆ CSL_CSITX_YUV422_MODE_YUYV

#define CSL_CSITX_YUV422_MODE_YUYV   (2U)

YUV422 Mode: VYUY.

◆ CSL_CSITX_YUV422_MODE_VYUY

#define CSL_CSITX_YUV422_MODE_VYUY   (1U)

YUV422 Mode: YUYV.

◆ CSL_CSITX_YUV422_MODE_YVYU

#define CSL_CSITX_YUV422_MODE_YVYU   (3U)

YUV422 Mode: YVYU.

Function Documentation

◆ CSL_csitxGetRevisionId()

void CSL_csitxGetRevisionId ( const CSL_csi_tx_ifRegs ifRegisters,
CSL_CsitxRevisionId revId 
)

This API is used get the CSI Tx revision ID.

Parameters
ifRegistersBase Address of the CSI Tx SS Registers.
revIdContains Revision ID of CSI Tx module. Refer to CSL_CsitxRevisionId.
Returns
None.

◆ CSL_csitxColorbarCfg()

int32_t CSL_csitxColorbarCfg ( const CSL_csi_tx_ifRegs ifRegisters,
const CSL_CsitxColorbarGenCfg cfg 
)

This API is used program the color bar generation parameters.

Parameters
ifRegistersBase Address of the CSI Tx SS Registers.
cfgColor-bar generation configurations. Refer to CSL_CsitxColorbarGenCfg.
Returns
status CSL_PASS if successful otherwise CSL_EFAIL.

◆ CSL_csitxEnableColorbarGen()

void CSL_csitxEnableColorbarGen ( CSL_csi_tx_ifRegs ifRegisters,
uint32_t  enable 
)

This API is used enable/disable Color-bar generation.

Parameters
ifRegistersBase Address of the CSI Tx SS Registers.
enableColor-bar generation is enabled if it is TRUE. Color-bar generation is disabled if it is FALSE.
Returns
None.

◆ CSL_csitxRetransCfg()

int32_t CSL_csitxRetransCfg ( const CSL_csi_tx_ifRegs ifRegisters,
const CSL_CsitxRetransCfg cfg 
)

This API is used program the re-transmission streams parameters.

Parameters
ifRegistersBase Address of the CSI Tx SS Registers.
cfgRe-transmission streams configurations. Refer to CSL_CsitxRetransCfg.
Returns
status CSL_PASS if successful otherwise CSL_EFAIL.

◆ CSL_csitxAssertPixelIfReset()

void CSL_csitxAssertPixelIfReset ( CSL_csi_tx_ifRegs ifRegisters,
uint32_t  assert 
)

This API is used assert/de-assert reset for pixel interface.

Parameters
ifRegistersBase Address of the CSI Tx SS Registers.
assertReset is asserted if it is TRUE. Reset is not asserted if it is FALSE.
Returns
None.

◆ CSL_csitxGetStrmStatus()

void CSL_csitxGetStrmStatus ( const CSL_csi_tx_ifRegs ifRegisters,
CSL_CsitxStrmStatus status 
)

This API is used get the current stream status.

Parameters
ifRegistersBase Address of the CSI Tx SS Registers.
statusStream status. Refer to CSL_CsitxStrmStatus.
Returns
None.

◆ CSL_csitxFrmToFrmDelayCfg()

int32_t CSL_csitxFrmToFrmDelayCfg ( const CSL_csi_tx_ifRegs ifRegisters,
const uint32_t  vc,
const uint32_t  delay 
)

This API is used program frame to frame delay.

Parameters
ifRegistersBase Address of the CSI Tx SS Registers.
vcVirtual channel number for which delay needs to configured.
delayDelay in number of main clock cyles from start of last frame line to start of next frame first line.
Returns
status CSL_PASS if successful otherwise CSL_EFAIL.

◆ CSL_csitxConfigDMA()

int32_t CSL_csitxConfigDMA ( CSL_csi_tx_ifRegs ifRegisters,
const CSL_CsitxDMAConfig cfg 
)

This API is used to configure DMA/PSIL thread.

Parameters
ifRegistersBase Address of the CSI Tx SS Registers.
cfgPointer to DMA/PSIL Configurations. Refer to CSL_CsitxDMAConfig
Returns
status CSL_PASS if successful otherwise CSL_EFAIL.