![]() |
MCUSW
|
The Can Driver MCAL provides low level access to onbaord MCAN peripheral present on Device.
The Can Driver implements a standardized interface specified in the AUTOSAR_SWS_CANDriver document.
The Can Driver is part of the Communication Stack in the AUTOSAR Basic Software (BSW)
The CAN Hardware Unit cntrolled by CAN Driver combines one or several CAN controllers,
which may be located on-chip or as external standalone devices of the same type, with common or separate Hardware Objects
Sub Modules | |
| Can Configuration | |
Functions | |
| void | Can_GetVersionInfo (Std_VersionInfoType *VersionInfo) |
| Function returns the version information of this module. More... | |
| void | Can_Init (const Can_ConfigType *CfgPtr) |
| This function initializes the module. More... | |
| Can_ReturnType | Can_SetControllerMode (uint8 Controller, Can_StateTransitionType Transition) |
| This function performs software triggered state transitions of the CAN controller State machine. More... | |
| Can_ReturnType | Can_Write (Can_HwHandleType Hth, const Can_PduType *PduInfo) |
| This function is called by CanIf to pass a CAN message to CanDrv for transmission. More... | |
| void | Can_DisableControllerInterrupts (uint8 Controller) |
| This function disables all interrupts for this CAN controller. More... | |
| void | Can_EnableControllerInterrupts (uint8 Controller) |
| This function enables all allowed interrupts. More... | |
| void | Can_MainFunction_Write (void) |
| This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING. More... | |
| void | Can_MainFunction_BusOff (void) |
| This function performs the polling of bus-off events that are configured statically as 'to be polled'. More... | |
| void | Can_MainFunction_Read (void) |
| This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING. More... | |
| void | Can_MainFunction_Wakeup (void) |
| This function performs the polling of wake-up events that are configured statically as 'to be polled'. More... | |
| void | Can_MainFunction_Mode (void) |
| This function performs the polling of CAN controller mode transitions. More... | |
| Std_ReturnType | Can_ChangeBaudrate (uint8 Controller, uint16 Baudrate) |
| TThis service shall change the baudrate of the CAN controllerr. More... | |
| Std_ReturnType | Can_CheckBaudrate (uint8 Controller, uint16 Baudrate) |
| This service shall check, if a certain CAN controller supports a requested baudrate. More... | |
| Std_ReturnType | Can_SetBaudrate (uint8 Controller, uint16 BaudRateConfigID) |
| This service shall set the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset. More... | |
| Std_ReturnType | Can_TestLoopBackModeEnable (uint8 Controller, uint8 Mode) |
| This service will enable CAN loopback mode. More... | |
| Std_ReturnType | Can_TestLoopBackModeDisable (uint8 Controller, uint8 Mode) |
| This service will disable CAN loopback mode. More... | |
| Std_ReturnType | Can_RegisterReadback (VAR(uint8,) Controller, Can_RegisterReadbackType *RegRbPtr) |
| This service will readback CAN registers. More... | |
| void | Can_DeInit (void) |
| This service is only used for UT testing and not for app use. More... | |
Macros | |
| #define | CAN_SW_PATCH_VERSION (0U) |
| Driver Implementation Patch Version. More... | |
| #define | CAN_AR_RELEASE_REVISION_VERSION (1U) |
| AUTOSAR Patch version specification implemented by CanDriver. More... | |
Can Driver Module SW Version Info | |
Defines for CAN Driver version used for compatibility checks | |
| #define | CAN_SW_MAJOR_VERSION (0U) |
| Driver Implementation Major Version.Used for version compatibiltiy check. More... | |
| #define | CAN_SW_MINOR_VERSION (1U) |
| Driver Implementation Minor Version.Used for version compatibiltiy check. More... | |
Can Driver Module AUTOSAR Version Info | |
Defines for CAN Driver AUTOSAR version used for compatibility checks | |
| #define | CAN_AR_RELEASE_MAJOR_VERSION (4U) |
| AUTOSAR Major version specification implemented by CanDriver. More... | |
| #define | CAN_AR_RELEASE_MINOR_VERSION (2U) |
| AUTOSAR Minor version specification implemented by CanDriver. More... | |
Can Driver ID Info | |
| #define | CAN_VENDOR_ID (44U) |
| Texas Instruments Vendor ID. More... | |
| #define | CAN_MODULE_ID (80U) |
| Can Driver Module ID. More... | |
| #define | CAN_INSTANCE_ID (0U) |
| CAN Driver Instance ID. More... | |
CAN Driver states. | |
| #define | CAN_UNINIT ((uint8)0U) |
| CAN Driver is NOT initialized. More... | |
| #define | CAN_READY ((uint8)1U) |
| CAN Driver is initialized. More... | |
Can Error Codes | |
| #define | CAN_E_PARAM_POINTER (0x01U) |
| #define | CAN_E_PARAM_HANDLE (0x02U) |
| ERROR:NULL_PTR passed as parameter. More... | |
| #define | CAN_E_PARAM_DLC (0x03U) |
| ERROR:Invalid Controller Handle. More... | |
| #define | CAN_E_PARAM_CONTROLLER (0x04U) |
| ERROR:Invalid length of msg. More... | |
| #define | CAN_E_UNINIT (0x05U) |
| ERROR:Invalid controller id. More... | |
| #define | CAN_E_TRANSITION (0x06U) |
| ERROR:Eror due to API invoked without performing Can_Init() More... | |
| #define | CAN_E_DATALOST (0x07U) |
| ERROR:Eror during Controller state transition. More... | |
| #define | CAN_E_PARAM_BAUDRATE (0x08U) |
| ERROR:Data lost/dropped. More... | |
| #define | CAN_E_ICOM_CONFIG_INVALID (0x09U) |
| ERROR:Timeout occured. More... | |
| #define | CAN_E_INIT_FAILED (0x0AU) |
| ERROR:Invalid Baudrate configuration. More... | |
CAN Config Ids | |
ERROR:Invalid configuration set selection The Config Ids used for different CAN Configuration builds | |
| #define | CAN_CFG_ID_0 (0x01U) |
| Config 0 (All configurations ON) More... | |
| #define | CAN_CFG_ID_1 (0x02U) |
| Config 1 (All configurations OFF). CAN_CFG_ID_1 is used only for compile check. More... | |
| #define | CAN_CFG_ID_2 (0x04U) |
| Config 2 (All configurations ON except DET OFF) More... | |
| #define | CAN_CFG_ID_3 (0x08U) |
| Config 3 (Configurator auto generated file) More... | |
| #define | CAN_CFG_ID_4 (0x10U) |
| Config 4 (Configurator auto generated file MCAN instead of DCAN2 with pre-compile variant ON) More... | |
| #define | CAN_CFG_ID_5 (0x20U) |
| Config 5 (All configurations ON but used only for testing WakeUp by external HW event and Performance tests) More... | |
| #define | CAN_CFG_ID_6 (0x40U) |
| Config 6 (Used for MCAN Testing) More... | |
| #define CAN_SW_MAJOR_VERSION (0U) |
Driver Implementation Major Version.Used for version compatibiltiy check.
| #define CAN_SW_MINOR_VERSION (1U) |
Driver Implementation Minor Version.Used for version compatibiltiy check.
| #define CAN_SW_PATCH_VERSION (0U) |
Driver Implementation Patch Version.
| #define CAN_AR_RELEASE_MAJOR_VERSION (4U) |
AUTOSAR Major version specification implemented by CanDriver.
| #define CAN_AR_RELEASE_MINOR_VERSION (2U) |
AUTOSAR Minor version specification implemented by CanDriver.
| #define CAN_AR_RELEASE_REVISION_VERSION (1U) |
AUTOSAR Patch version specification implemented by CanDriver.
| #define CAN_VENDOR_ID (44U) |
Texas Instruments Vendor ID.
| #define CAN_MODULE_ID (80U) |
Can Driver Module ID.
| #define CAN_INSTANCE_ID (0U) |
CAN Driver Instance ID.
| #define CAN_UNINIT ((uint8)0U) |
CAN Driver is NOT initialized.
| #define CAN_READY ((uint8)1U) |
CAN Driver is initialized.
| #define CAN_INIT_ID (0x00U) |
| #define CAN_MAINFCT_WRITE_ID (0x01U) |
| #define CAN_SETCTR_ID (0x03U) |
| #define CAN_DIINT_ID (0x04U) |
| #define CAN_ENINT_ID (0x05U) |
| #define CAN_WRITE_ID (0x06U) |
| #define CAN_VERSION_ID (0x07U) |
| #define CAN_MAINFCT_READ_ID (0x08U) |
| #define CAN_MAINFCT_BO_ID (0x09U) |
| #define CAN_MAINFCT_WU_ID (0x0AU) |
| #define CAN_CKWAKEUP_ID (0x0BU) |
Can_CheckWakeup()
| #define CAN_CHKBAUDRATE_ID (0x0EU) |
| #define CAN_CHNGBAUDRATE_ID (0x0DU) |
| #define CAN_MAINFCT_MODE_ID (0x0CU) |
| #define CAN_LOOPBACK_ID (0x12U) |
| #define CAN_RXPROCESS_ID (0x10U) |
Can_RxProcess()
| #define CAN_SETBAUDRATE_ID (0x0FU) |
| #define CAN_DEINIT_ID (0x13U) |
| #define CAN_E_PARAM_POINTER (0x01U) |
| #define CAN_E_PARAM_HANDLE (0x02U) |
ERROR:NULL_PTR passed as parameter.
| #define CAN_E_PARAM_DLC (0x03U) |
ERROR:Invalid Controller Handle.
| #define CAN_E_PARAM_CONTROLLER (0x04U) |
ERROR:Invalid length of msg.
| #define CAN_E_UNINIT (0x05U) |
ERROR:Invalid controller id.
| #define CAN_E_TRANSITION (0x06U) |
ERROR:Eror due to API invoked without performing Can_Init()
| #define CAN_E_DATALOST (0x07U) |
ERROR:Eror during Controller state transition.
| #define CAN_E_PARAM_BAUDRATE (0x08U) |
ERROR:Data lost/dropped.
| #define CAN_E_ICOM_CONFIG_INVALID (0x09U) |
ERROR:Timeout occured.
| #define CAN_E_INIT_FAILED (0x0AU) |
ERROR:Invalid Baudrate configuration.
| #define CAN_CFG_ID_0 (0x01U) |
Config 0 (All configurations ON)
| #define CAN_CFG_ID_1 (0x02U) |
Config 1 (All configurations OFF). CAN_CFG_ID_1 is used only for compile check.
| #define CAN_CFG_ID_2 (0x04U) |
Config 2 (All configurations ON except DET OFF)
| #define CAN_CFG_ID_3 (0x08U) |
Config 3 (Configurator auto generated file)
| #define CAN_CFG_ID_4 (0x10U) |
Config 4 (Configurator auto generated file MCAN instead of DCAN2 with pre-compile variant ON)
| #define CAN_CFG_ID_5 (0x20U) |
Config 5 (All configurations ON but used only for testing WakeUp by external HW event and Performance tests)
| #define CAN_CFG_ID_6 (0x40U) |
Config 6 (Used for MCAN Testing)
| void Can_GetVersionInfo | ( | Std_VersionInfoType * | VersionInfo | ) |
Function returns the version information of this module.
* Service name : Can_GetVersionInfo * Syntax : void Can_GetVersionInfo(Std_VersionInfoType* versioninfo) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : versioninfo * Pointer to where to store the version information of this * module. * Return value : None * Description : This function returns the version information of this * module *
| void Can_Init | ( | const Can_ConfigType * | CfgPtr | ) |
This function initializes the module.
* Service name : Can_Init * Syntax : void Can_Init(const Can_ConfigType* CfgPtr) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : CfgPtr * Pointer to driver configuration. * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function initializes the module. *
| Can_ReturnType Can_SetControllerMode | ( | uint8 | Controller, |
| Can_StateTransitionType | Transition | ||
| ) |
This function performs software triggered state transitions of the CAN controller State machine.
* Service name: Can_SetControllerMode * Syntax: Can_ReturnType Can_SetControllerMode(uint8 Controller, * Can_StateTransitionType Transition) * Service ID[hex]: 0x03 * Sync/Async: Asynchronous * Reentrancy: Non Reentrant * Parameters (in): Controller * - CAN controller for which the status shall be changed * Transition * - Transition value to request new CAN controller state * Parameters (inout): None * Parameters (out): None * Return value: Can_ReturnType * - CAN_OK: request accepted * - CAN_NOT_OK: request not accepted, a development error * occurred * Description: This function performs software triggered state transitions of * the CAN controller State machine. *
| Can_ReturnType Can_Write | ( | Can_HwHandleType | Hth, |
| const Can_PduType * | PduInfo | ||
| ) |
This function is called by CanIf to pass a CAN message to CanDrv for transmission.
* Service name: Can_Write * Syntax : Can_ReturnType Can_Write(Can_HwHandleType Hth, const * Can_PduType* PduInfo) * Service ID[hex]: 0x06 * Sync/Async : Synchronous * Reentrancy : Reentrant (thread-safe) * Parameters (in): Hth * - Information which HW-transmit handle shall be used for * transmit. Implicitly this is also the information about * the controller to use because the Hth numbers are unique * inside one hardware unit. * PduInfo * - Pointer to SDU user memory, DLC and Identifier. * Parameters (inout): None * Parameters (out) : None * Return value: Can_ReturnType * - CAN_OK: Write command has been accepted * - CAN_NOT_OK: development error occurred * - CAN_BUSY: No TX hardware buffer available or pre-emptive call * of Can_Write that can't be implemented re-entrant * Description: This function is called by CanIf to pass a CAN message to CanDrv * for transmission. *
| void Can_DisableControllerInterrupts | ( | uint8 | Controller | ) |
This function disables all interrupts for this CAN controller.
* Service name : Can_DisableControllerInterrupts * Syntax : void Can_DisableControllerInterrupts(uint8 Controller) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN controller for which interrupts shall be disabled. * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function disables all interrupts for this CAN * controller * *
| void Can_EnableControllerInterrupts | ( | uint8 | Controller | ) |
This function enables all allowed interrupts.
* Service name : Can_EnableControllerInterrupts * Syntax : void Can_EnableControllerInterrupts(uint8 Controller) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN controller for which interrupts shall be re-enabled. * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function enables all allowed interrupts * *
| void Can_MainFunction_Write | ( | void | ) |
This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.
* Service name : Can_MainFunction_Write * Syntax : void Can_MainFunction_Write(void) * Service ID[hex]: 0x01 * Description : This function performs the polling of TX confirmation when * CAN_TX_PROCESSING is set to POLLING. * *
| void Can_MainFunction_BusOff | ( | void | ) |
This function performs the polling of bus-off events that are configured statically as 'to be polled'.
* Service name : Can_MainFunction_BusOff * Syntax : void Can_MainFunction_BusOff(void) * Service ID[hex]: 0x09 * Description : This function performs the polling of bus-off events that are * configured statically as 'to be polled'. * *
| void Can_MainFunction_Read | ( | void | ) |
This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.
* Service name : Can_MainFunction_Read * Syntax : void Can_MainFunction_Read(void) * Service ID[hex]: 0x08 * Description : This function performs the polling of RX indications when * CAN_RX_PROCESSING is set to POLLING. * *
| void Can_MainFunction_Wakeup | ( | void | ) |
This function performs the polling of wake-up events that are configured statically as 'to be polled'.
* Service name : Can_MainFunction_Wakeup * Syntax : void Can_MainFunction_Wakeup(void) * Service ID[hex]: 0x0A * Description : This function performs the polling of wake-up events that are * configured statically as 'to be polled'. * *
| void Can_MainFunction_Mode | ( | void | ) |
This function performs the polling of CAN controller mode transitions.
* Service name : Can_MainFunction_Mode * Syntax : void Can_MainFunction_Mode(void) * Service ID[hex]: 0x0C * Description : This function performs the polling of CAN controller mode * transitions. * *
| Std_ReturnType Can_ChangeBaudrate | ( | uint8 | Controller, |
| uint16 | Baudrate | ||
| ) |
TThis service shall change the baudrate of the CAN controllerr.
* * Service name: Can_ChangeBaudrate * Syntax: Std_ReturnType Can_ChangeBaudrate(uint8 Controller, uint16 Baudrate) * Service ID[hex]: 0x0d * Sync/Async: Synchronous * Reentrancy: Non Reentrant * Parameters (in): Controller * CAN Controller, whose baudrate shall be changed * Baudrate * Requested baudrate in kbps * Parameters (inout): None * Parameters (out): None * Return value: Std_ReturnType * E_OK: Service request accepted, baudrate change started * E_NOT_OK: Service request not accepted * Description: * This service shall change the baudrate of the CAN controller. <br> * Please note that this API is deprecated and is kept only for * backward compatibility reasons.<br> * Can_SetBaudrate API shall be used instead to change the baud rate * configuration. <br> * In the next major release this API will be deleted.<br> * *
| Std_ReturnType Can_CheckBaudrate | ( | uint8 | Controller, |
| uint16 | Baudrate | ||
| ) |
This service shall check, if a certain CAN controller supports a requested baudrate.
* * Service name : Can_CheckBaudrate * Syntax : Std_ReturnType Can_CheckBaudrate(uint8 Controller, * uint16 Baudrate) * Service ID[hex] : 0x0e * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * CAN Controller to check for the support of a certain baudrate * Baudrate * Baudrate to check in kbps * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Baudrate supported by the CAN Controller * - E_NOT_OK: Baudrate not supported / invalid CAN * Description : This service shall check, if a certain CAN controller * supports a requested baudrate *
| Std_ReturnType Can_SetBaudrate | ( | uint8 | Controller, |
| uint16 | BaudRateConfigID | ||
| ) |
This service shall set the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset.
* * Function name : Can_SetBaudrate * Syntax : FUNC(Std_ReturnType, CAN_CODE) Can_SetBaudrate(uint8 * Controller, uint16 BaudRateConfigID) * Service ID[hex] : 0x0f * Sync/Async : Synchronous * Reentrancy : Reentrant for different Controllers. * Non reentrant for the same Controller. * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This service shall set the baud rate configuration * of the CAN controller. Depending on necessary baud rate * modifications the controller might have to reset. * *
| Std_ReturnType Can_TestLoopBackModeEnable | ( | uint8 | Controller, |
| uint8 | Mode | ||
| ) |
This service will enable CAN loopback mode.
* * Service name : Can_TestLoopBackModeEnable * Syntax : Std_ReturnType Can_TestLoopBackModeEnable(uint8 * Controller, uint8 mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN Controller to enable loopback mode * mode * - Loopback mode * -# 0 - Digital Loopback * -# 1 - Analog Loopback * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Baudrate supported by the CAN Controller * - E_NOT_OK: Baudrate not supported / invalid CAN * Description : This service will enable CAN loopback mode. *
| Std_ReturnType Can_TestLoopBackModeDisable | ( | uint8 | Controller, |
| uint8 | Mode | ||
| ) |
This service will disable CAN loopback mode.
* * Service name : Can_TestLoopBackModeDisable * Syntax : Std_ReturnType Can_TestLoopBackModeDisable(uint8 * Controller, uint8 Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN Controller to enable loopback mode * mode * Loopback mode * -# 0 - Digital Loopback * -# 1 - Analog Loopback * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Loopback mode enabled in the CAN Controller * - E_NOT_OK: Loopback mode enable failed * Description : This service will disable CAN loopback mode. *
| Std_ReturnType Can_RegisterReadback | ( | VAR(uint8,) | Controller, |
| Can_RegisterReadbackType * | RegRbPtr | ||
| ) |
This service will readback CAN registers.
* * Service name : Can_RegisterReadback * Syntax : Std_ReturnType Can_RegisterReadback(uint8 Controller) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN Controller to readback registers from * Parameters (inout): RegRbPtr - Pointer to where to store the readback * values. If this pointer is NULL_PTR, then the API * will return E_NOT_OK. * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Loopback mode disabled in the CAN Controller * - E_NOT_OK: Loopback mode disable failed * Description : This service will disable CAN loopback mode. *
| void Can_DeInit | ( | void | ) |
This service is only used for UT testing and not for app use.
* Service name : Can_DeInit * Syntax : void Can_DeInit(void) * Sync/Async : Synchronous * Reentrancy : Non-Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This API is not standard AUTOSAR API. * This service sets the internal Can Controller state to * UNINIT state so that Can_Init can be invoked again. * This is required for UT test cases with diff Config. *