MCUSW
Pwm Design Document

Introduction


This document describes the functionality, API and configuration of the AUTOSAR BSW module PWM

  • Supported AUTOSAR Release : 4.2.1
  • Supported Configuration Variants : Pre-Compile & Post-Build
  • Vendor ID : PWM_VENDOR_ID (44)
  • Module ID : PWM_MODULE_ID (121)

Overview

The figure below depicts the AUTOSAR layered architecture as 3 distinct layers,

  • Application
  • Runtime Environment (RTE) and
  • Basic Software (BSW).

The BSW is further divided into 4 layers:

  • Services
  • Electronic Control Unit Abstraction
  • MicroController Abstraction (MCAL) and
  • Complex Drivers.
autosar_acrhitecture_common.png
AUTOSAR Architecture

MCAL is the lowest abstraction layer of the Basic Software. It contains software modules that interact with the Microcontroller and its internal peripherals directly. The PWM driver is a part of the microcontroller (peripheral) Driver module which is a part of the Basic Software. The figure below shows the position of the PWM driver in the AUTOSAR Architecture.

autosar_acrhitecture_pwm.png
AUTOSAR Architecture – PWM MCAL

PWM Overview

The PWM module implements an interface in C programming language for handling the PWM functionality of the device.This PWM driver takes care of initializing and de-initializing the PWM unit and offers services to:

  • Generate pulses with variable pulse width(Duty Cycle)
  • Set parameters of a PWM channels waveform(Duty Cycle and Period)
  • Enable/Disable notifications
pwm_signal_description.png
PWM Signal Description

In this design, the PWM Functionality is achieved by using the DM Timers available on the device. TDA4x, AM65XX class of devices includes multiple timers, some of the key features provided are listed below:

  • Free running 32 bit up counter
  • Auto reload mode (can be used for continuous counter operation)
  • Support dynamic Start / Stop counter operation
  • Programmable clock dividers (2n, where n = [0-8])
  • 2 timers modules could be operated in cascaded mode to provide 64bit counter
  • Programmable interrupt generation on overflow, compare and capture
  • Programmable clock source

There is Support for 3 basic functional modes Timer mode, Capture mode & Compare mode. Refer section 12.8.3 in 2 for more details on timer operation.

Timer pins can be configured to be used as PWM output pins. However, not all timer pins can be configured to be PWM output, please refer TRM for specific pins (section 12.8.3.1 in 2)

The following image shows the block diagram of Timer which can generate a PWM output:

pwm_timer_block_diagram.png
Timer Block Diagram

References

Sl No Specification Comment / Link
1 AUTOSAR 4.2.1 AUTOSAR Specification for PWM Driver Intranet Link
2 AM65XX and TDA4x TRM Technical Reference Manual, DRA80X, TDA4X PWM/DM Timer Module is detailed
3 BSW General Requirements / Coding guidelines Intranet Link
4 Software Product Specification (SPS) Intranet Link Requirements are derived from 1

Requirements

The PWM driver shall implement as per requirements detailed in 4, 1 and 3. It is recommended to refer 1 for clarification.


Features Supported

Below listed are some of the key features that are expected to be supported

  • Changing of frequency and duty cycle for a PWM channel at runtime besides the default configuration.
  • The PWM signal that can be generated is a square wave with variable duty cycle and period .
Design ID DES_PWM_001
Requirements Covered MCAL-965, MCAL-3503, MCAL-3509, MCAL-3511, MCAL-3536, MCAL-3537, MCAL-3538, MCAL-3539, MCAL-3540, MCAL-3554, MCAL-3646, MCAL-3647, MCAL-3510, MCAL-3631, MCAL-3535, MCAL-920, MCAL-921, MCAL-922, MCAL-923, MCAL-925,MCAL-929, MCAL-930, MCAL-932, MCAL-933, MCAL-937, MCAL-938, MCAL-939,MCAL-942, MCAL-947, MCAL-980, MCAL-945, MCAL-1056 , MCAL-3502, MCAL-3503, MCAL-3509, MCAL-3511, MCAL-3646, MCAL-3647, MCAL-3535, MCAL-3631

Back To Top


caution.png

Features Not Supported / NON Compliance

  • [NON Compliance] APIs related to setting or getting power state of the device is not supported, as hardware itself doesn’t support this feature.
  • [NON Compliance] PwmMcuClockReferencePoint doesn’t refer to McuClockReferencePoint. Refer section (Constraints) for details.
  • PWM_FIXED_PERIOD_SHIFTED Pwm Channel Class type is not supported
  • Standard AUTOSAR PWM specification 1, categorizes few BSW General Requirements as non-requirements, please refer MCAL-3648 for details
  • Supports additional configuration parameters, refer section (Pwm_RegisterReadback)
Design ID DES_PWM_002
Non Requirements MCAL-3648,MCAL-3642,MCAL-3493,MCAL-3482,MCAL-3522,MCAL-3532,MCAL-3531, MCAL-3512,MCAL-3614,MCAL-3481,MCAL-3613,MCAL-3515,MCAL-3626,MCAL-3478, MCAL-3513,MCAL-3628,MCAL-3629,MCAL-3606,MCAL-3617,MCAL-3602,MCAL-3516, MCAL-3638,MCAL-3608,MCAL-3619,MCAL-3609,MCAL-3514,MCAL-3518,MCAL-3519, MCAL-3630,MCAL-3543,MCAL-3604,MCAL-3517,MCAL-3544,MCAL-3610,MCAL-3627, MCAL-3618,MCAL-3605,MCAL-3639,MCAL-3620,MCAL-3603,MCAL-3521,MCAL-3621, MCAL-3607,MCAL-3484,MCAL-3615,MCAL-3483,MCAL-3622,MCAL-3611,MCAL-3530, MCAL-3520,MCAL-3601,MCAL-3612,MCAL-3623,MCAL-3529,MCAL-3616,MCAL-3489, MCAL-3588,MCAL-3589,MCAL-3591,MCAL-3590,MCAL-3497

Back To Top


Assumptions

Below listed are assumed to valid for this design/implementation, exceptions and other deviations are listed for each explicitly. Care should be taken to ensure these assumptions are addressed.

  1. The functional clock to the PWM module is expected to be on before calling any PWM module API.
  2. The PWM driver as such doesn’t perform any PRCM programming to get the functional clock.
  3. The clock-source selection for PWM is not performed by the PWM driver, other entities such as SBL, MCAL module MCU shall perform the same.

Back To Top


Constraints

Some of the critical constraints of this design are listed below

  • In cases where MCU module is not employed (supported) to configure the clock source for PWM module (refer Assumptions sub-item 3). The PWM module configurator shall refer to MCU clock source as listed in specification.
  • The PWM SWS does not cover PWM emulation on general purpose I/O
  • Timer when configured for toggle mode with TCLR[11-10] TRG = 0x2 (overflow and match), and TCLR[7] SCPWM Bit = 1 for polarity Low, the first event that toggles the PWM line is an overflow event. If a match event occurs first,it does not toggle the PWM line
    Design ID DES_PWM_003
    Requirements Covered MCAL-3493, MCAL-3502

Back To Top


Design Description


Fundamental Operation

The timer can be configured to provide a programmable PWM output. The timer PWM (POTIMERPWM) output pin can be configured to toggle on an event. The TCLR[11-10] TRG bit field determines on which register value the PWM pin toggles. Either overflow or both overflow and match can be selected to toggle the timer PWM pin when a compare condition occurs. TMAR, TLDR The internal overflow pulse is set each time the (0xFFFF FFFF – TLDR[31-0] LOAD_VALUE + 1) value is reached, and the internal match pulse is set when the counter reaches the value of TMAR. Depending on the value of the TCLR[12] PT bit and TCLR[11-10] TRG bit field, the timer provides pulse or PWM event on the output pin (POTIMERPWM). The TLDR and TMAR must keep values below the overflow value (0xFFFF FFFF) by at least two units. If the PWM trigger events are both overflow and match, the difference between the values kept in the TMAR and the value in the TLDR must be at least two units. When match event is used, the compare mode TCLR[6] CE bit must be set.

The following sequence of steps needs to be performed, before the timer can be started

  • Timer is programmed as configured (in continuous mode or Autoreload mode)
  • The initial count of the counter TCLR needs to be loaded
  • The reload register (TLDR) needs to be loaded
  • The timer is started and the counter (register TCRR), starts counting on every pulse
    • As depicted in above figure, TCRR has moved w.r.t to TLDR
gpt_design_timer_expired.png
Timer expired
  • When the timer expires, the TCRR is loaded with value present in TLDR as show above
  • An interrupt can be triggered at this point

For generating a PWM signal from the timer interrupts, the following cases w.r.t. duty cycle are considered:

Case 1: Duty cycle of 0%

  • The PWM pulse is always at the polarity configured at initialization. For example, if the polarity is configured as LOW, the PWM signal will always be LOW.

CASE 2: Duty cycle of 100%

  • The PWM pulse is always at the opposite to the polarity configured at initialization. For example, if the polarity is configured as LOW, the PWM signal will always be HIGH.

Case 3: Duty cycle of 50%

  • When the When a duty cycle of 50% for a PWM signal is required, both the time that the pulse remains HIGH and LOW is equal. In this case, the timer is operated in overflow mode alone (without compare). In one cycle of the PWM signal, the timer should generate an interrupt twice. Hence, the overflow rate for the timer (OVF_Rate) is half the period of the PWM signal required. The load value for TLDR register can be calculated using the following formula:

       OVF_Rate = (0xFFFF FFFF – TLDR + 1) × (timer-functional clock period) × PS
    

    where

    • OVF_Rate = (PWM Period /2 )
    • Timer-functional clock period is the period of the input clock to the timer
    • PS is the Prescaler Clock Ratio Value used to divide the timer counter input clock frequency as shown below:
pwm_timer_prescalar.png
Prescaler Clock Ratio Values

Case 4: 0%< Duty cycle < 100%

  • When PWM signal with 0%< duty cycle < 100% for a is required, the timer is operated in overflow and match mode (with compare). In one cycle of the PWM signal, the timer generates an interrupt twice, one when the match condition is met and one when overflow is triggered as shown in the figure below.Hence, in this scenario, the overflow rate for the timer (OVF_Rate) is same as the period of the PWM signal required.

    pwm_timer_func.png
    Generation of PWM signal using Timer

    The load value for TLDR and TMAR registers can be calculated using the following formula:

    OVF_Rate = (0xFFFF FFFF – TLDR + 1) × (timer-functional clock period) × PS
    OVF_Rate * (1- (Dutycyle/100)) = (0xFFFF FFFF – TMAR + 1) × (timer-functional clock period) × PS
    

    where

    • OVF_Rate = (PWM Period )
    • Timer-functional clock period is the period of the input clock to the timer
    • PS is the Prescaler Clock Ratio Value.

    Two example cases are shown in the following figure. The TCLR[7] SCPWM bit is set to 0 in one case and to 1 in the other case. To obtain the desired wave form, start the counter at 0xFFFF FFFE value (to ensure an overflow first) or adjust the line polarity (TCLR[7] SCPWM bit).

    pwm_from_timer.png
    Timing Diagram for PWM through Timer

    NOTE

    • The Functional frequency range dictates the usage of posted and non-posted write modes for the timer. Incase of posted mode of operation, If a write access is pending for a register, reading from this register does not yield a correct result. Software synchronization must be used to avoid incorrect results. Functional frequency range: freq(timer clock) < freq(interface clock)/4.

Back To Top


Dynamic Behavior

States

As the PWM module is implemeted using a timer, as detailed in section 7.1 of 5, a timer would be in one of the following states. Initialized, running, stopped, expired. The diagram below shows transitions of states:

gpt_design_timer_state.png
Timer States : Sourced from TIMER AUTOSAR Spec

Back To Top


Time Unit Ticks

Refer 1 specifically section 7.2 of the specification for more details All time units used within the API services of the PWM module shall be of the unit ticks.

Design ID DES_PWM_004
Requirements Covered MCAL-3511

Back To Top


Duty Cycle Resolution and Scaling

Refer 1 specifically section 7.7 of the specification for more details The width of the duty cycle parameter is 16 Bits and the parameter follows the following scaling scheme:

  • 0x0000 means 0%.
  • 0x8000 means 100%. 0x8000 gives the highest resolution while allowing 100% duty cycle to be represented with a 16 bit value.

As an implementation guide, the following source code example is given:

AbsoluteDutyCycle =((uint32)AbsolutePeriodTime * RelativeDutyCycle) >> 15;
Design ID DES_PWM_005
Requirements Covered MCAL-3533,MCAL-3534

Back To Top


Directory Structure

The directory structure is as depicted in figures below, the source files can be categorized under “Driver Implementation” and “Example Application”

Driver Implemented by

  • Pwm.h and Pwm_Irq.h: Shall implement the interface provided by the driver
  • Pwm.c, Pwm_Irq.c, Pwm_Gptimer.c, Pwm_Priv.c and Pwm_Priv.h: Shall implement the driver functionality

Example Application

  • Pwm_Cfg.h and Pwm_Cfg.c: Shall implement the generated configuration for pre-compile variant
  • Pwm_PBcfg.c: Shall implement the generated configuration for post-build variant
  • PwmApp.c and PwmApp.h: Shall implement the example application that demonstrates the use of the driver
pwm_design_dir.png
Directory Structure
pwm_design_dir_detailed.png
Detailed Directory Structure
Design ID DES_PWM_006
Requirements Covered MCAL-3503,MCAL-3507,MCAL-3506,MCAL-3504,MCAL-3508,MCAL-3505

Back To Top


Configurator

The AUTOSAR PWM Driver Specification details mandatory parameters that shall be configurable via the configurator. Please refer section 10 of 1

Design ID DES_PWM_007
Requirements Covered MCAL-3474,MCAL-3475,MCAL-3476,MCAL-3477,MCAL-3478,MCAL-3479,MCAL-3480, MCAL-3481,MCAL-3482,MCAL-3483,MCAL-3484,MCAL-3485,MCAL-3486,MCAL-3487, MCAL-3488,MCAL-3489,MCAL-3490,MCAL-3491,MCAL-3492,MCAL-3493,MCAL-3494, MCAL-3495,MCAL-3496,MCAL-3497,MCAL-3498,MCAL-3499,MCAL-3500,MCAL-3501, MCAL-3652

NON Standard configurable parameters

The design's specific configurable parameters are as follows:

Parameter Usage comment
PwmDeviceVariant This shall allow integrators to select the device variant for which integration is being performed. This parameter shall be used by driver to impose device specific constraints. The user guide shall detail the device specific constraints
PwmFunctionalClock This is the value of the System clock frequency in Hz
PwmTypeofInterruptFunction This parameter allows the selection of Type of ISR function
PwmEnableRegisterReadbackApi This parameter enables the API to readback PWM critical registers
PwmClkPrescaler This parameter allows the selection of pre-scalar value.The prescaler stage is clocked with the pwm clock and acts as a clock divider for the time-base clock.
PwmPolarity This parameter stores the initial polarity configured for a channel
PwmIdleStateThis parameter stores whether the channel is in idle state
PwmDefaultOSCounterIdThis parameter stores Default Os Counter Id if node reference to OsCounter ref PwmOsCounterRef is not set
PwmOsCounterRefThis parameter contains a reference to the OsCounter, which is used by the Timer driver
PwmTimeoutDurationThis parameter contains the Timer timeout upper limit
Design ID DES_PWM_008
Requirements Covered MCAL-3653, MCAL-3654, MCAL-3660, MCAL-3657, MCAL-3752 ,MCAL-3753, MCAL-3754, MCAL-3655

Back To Top


Variant Support

The driver shall support both VARIANT-POST-BUILD & VARIANT-PRE-COMPILE

Design ID DES_PWM_009
Requirements Covered MCAL-3647, MCAL-3647

Back To Top


Dependency on other modules

In addition to dependencies listed in section 5 of 1, PWM driver shall depend on these modules to realize the required functionality. PWM uses Timer hardware present in the device to realize the functionality, this peripheral requires 2 different clock to be operational, namely ICLK and FCLK.

SBL

  • ICLK: Interface clock required for internal operation of the peripheral. This is not expected to change and typically programmed by SBL, please refer the device specific manual for details and valid value.
  • FCLK: Functional clock, used to drive the counter of the timer module. As per AUTOSAR PWM module specification 1, the PWM driver shall refer MCU Clock reference point. As detailed in section (Constraints), other entity would require to select the right clock source for the peripheral.

Back To Top


Error Classification

Errors are classified in two categories, development error and runtime / production error.


Development Errors

Type of Error Related Error code Value (Hex) Refer Req
API Pwm_Init service called with wrong parameter PWM_E_PARAM_CONFIG 0x10 MCAL-3523
API service used without module initialization PWM_E_UNINIT 0x11 MCAL-3524
API service used with an invalid channel Identifier PWM_E_PARAM_CHANNEL 0x12 MCAL-3525
Usage of unauthorized PWM service on PWM channel configured a fixed period PWM_E_PERIOD_UNCHANGEABLE 0x13 MCAL-3526
API Pwm_Init service called while the PWM driver has already been initialised PWM_E_ALREADY_INITIALIZED 0x14 MCAL-3527
API Pwm_GetVersionInfo is called with a NULL parameter. PWM_E_PARAM_POINTER 0x15 MCAL-3528
Design ID DES_PWM_010
Requirements Covered MCAL-3523, MCAL-3524, MCAL-3525, MCAL-3526, MCAL-3527, MCAL-3528

Error Detection

The detection of development errors is configurable (ON / OFF) at pre-compile time. The switch PwmDevErrorDetect will activate or deactivate the detection of all development errors.

Error notification (DET)

All detected development errors are reported to Det_ReportError service of the Development Error Tracer (DET).

Back To Top


Resource Behavior

  • Code Size : Implementation of this driver shall not exceed 40 kilo bytes of code and 1 KB of data section.
Design ID DES_PWM_011
Requirements Covered MCAL-3649
  • Stack Size : Worst case stack utilization shall not exceed 2 kilo bytes.
Design ID DES_PWM_012
Requirements Covered MCAL-3650

Back To Top


Supporting PWM for AUTOSAR versioned 4.4.0

This PWM design is based on the requirements specification for AUTOSAR versioned 4.2.1 and sections below highlight some of the critical changes that would be required between these two versions.

Note that this design doesn’t comprehend or account for other versions of AUTOSAR.

Deleted

Probably easiest of all to implement. The following have been removed from the requirements specification for AUTOSAR versioned 4.4.0:

  • [MCAL-3523] : Developement error classification : PWM_E_PARAM_CONFIG
  • [MCAL-3528] : Developement error classification : PWM_E_PARAM_POINTER
  • [MCAL-3553] : If development error detection is enabled for the Pwm module, the function Pwm_Init shall raise development error PWM_E_PARAM_CONFIG if ConfigPtr is a null pointer.
  • [MCAL-3556] : For pre-compile and link time configuration variants, a NULL pointer s hall be passed to the initialization routine
  • [MCAL-3557] : related to above point In this case the check for this NULL pointer has to be omitted.
  • [MCAL-3625] : The function Pwm_GetVersionInfo shall be configurable On/Off by the configuration parameter: PwmVersionInfoApi {PWM_VERSION_INFO_API
  • [MCAL-3642] : If development error detection for the Pwm module is enabled, and a development error occurs, then the corresponding PWM function shall return PWM_LOW for the function Pwm_GetOutputState
  • [MCAL-3646] : VARIANT-PRE-COMPILE (Pre Compile) is limited to pre-compile configuration parameters only.
  • [MCAL-3647] :VARIANT-POST-BUILD includes a mix of pre-compile, link time and post build configuration parameters. Also, note that Directory structure would require an update for the removal of the following:
  • [MCAL-3504] : Pwm.h shall include Pwm_Cfg.h
  • [MCAL-3505] : Pwm_Lcfg.c shall include Pwm.h and Pwm_Memmap.h.
  • [MCAL-3507] :Pwm_PBcfg.c shall include Pwm_MemMap.h and Pwm.h)

Added

The following changes have been added in the configurator in the requirements specification for AUTOSAR versioned 4.4.0

  • Module : Configuration of Pwm Module
  • PwmEcucPartitionRef : this requirement is still in draft state
  • PwmKernelEcucPartitionRef : this requirement is still in draft state
  • PwmChannelEcucPartitionRef : this requirement is still in draft state

The following changes have been added in the requirements specification for AUTOSAR versioned 4.4.0 :

  • Development Error Types Added
  • Runtime Error Types Added
  • Service name: Pwm_SetDutyCycle (in draft state) as MCAL-3565 has been made obsolete
  • Service name: Pwm_SetPeriodAndDuty (in draft state) as MCAL-3573 has been made obsolete
  • Service name: Pwm_SetOutputToIdle (in draft state) as MCAL-3581 has been made obsolete
  • [MCAL-3642] :If Pwm_GetOutputState is called before module initialization,or with an invalid channel, it shall return PWM_LOW
  • Service name: Pwm_DisableNotification (draft) please check MCAL-3592 made obsolete
  • Service name: Pwm_EnableNotification (draft) please check MCAL-3596 made obsolete
  • In DRAFT The PWM module shall reject configurations with partition mappings which are not supported by the implementation
  • In DRAFT The ECUC partitions referenced by PwmKernelEcucPartitionRef shall be a subset of the ECUC partitions referenced by PwmEcucPartitionRef

Low Level Definitions


The detailed API and interface description is available as part of 1 & 4. This section describes the API supported by the MCAL driver and the requirements covered by each of the API.

MACROS, Data Types & Structures

The sections below lists some of key data structures that shall be implemented and used in driver implementation

Maximum number of channels

Type Identifier Comments
uint32 PWM_MAX_CHANNELS Defines the maximum number of channels that are configured. Its required that configurations for all channel specified is valid.

Pwm_ChannelType

Used to specify the numeric identifier for a channel, please refer section 8.2.1 of 1

Pwm_PeriodType

Used to specify the period of a PWM channel, refer section 8.2.2 of 1

Pwm_OutputStateType

Used to specify the Output state of a PWM channel, refer section 8.2.3 of 1

Pwm_EdgeNotificationType

Enumeration used to specify the type of edge notification of a PWM channel. Refer section 8.2.4 of 1

Pwm_ChannelClassType

Enumeration used to specify the class of a PWM channel, whether the period is fixed or not. Refer section 8.2.5 of 1

Pwm_ConfigType

Hardware dependent structure used to specify the inital data for the PWM driver. Refer section 8.2.6 of 1

Pwm_RegisterReadbackType

Name Type Range Comments
pwmRev uint32 0 to 0xFFFFFFFF H/W version identifier, will not change for a given SoC
pwmTtgr uint32 0 to 0xFFFFFFFF Shall always read 0xFFFFFFFF
pwmTimerSynCtrl uint32 0 to 0xFFFFFFFF Interface control register, will read 0x00000000
Design ID DES_PWM_013
Requirements Covered MCAL-3536, MCAL-3537 ,MCAL-3538, MCAL-3539, MCAL-3540, MCAL-3541, MCAL-3542,MCAL-3662

APIs

For the standard APIs please refer 8.3 of 1. Sections below highlight other design considerations for the implementation.


Pwm_Init

Refer section 8.3.1 of 1

Design ID DES_PWM_014
Requirements Covered MCAL-3553, MCAL-3554, MCAL-3555, MCAL-3558, MCAL-3545, MCAL-3546, MCAL-3547, MCAL-3548, MCAL-3551, MCAL-3552, MCAL-3556, MCAL-3557,MCAL-3549,MCAL-3550

Back To Top


Pwm_DeInit

Refer section 8.3.2 of 1

Design ID DES_PWM_015
Requirements Covered MCAL-3560, MCAL-3559, MCAL-3561,MCAL-3562,MCAL-3563, MCAL-3564,MCAL-3643, MCAL-3640, MCAL-3641, MCAL-3642

Back To Top


Pwm_SetDutyCycle

Refer section 8.3.3 of 1

Design ID DES_PWM_016
Requirements Covered MCAL-3565,MCAL-3566, MCAL-3567,MCAL-3568,MCAL-3569, MCAL-3533,MCAL-3534,MCAL-3570,MCAL-3643, MCAL-3645, MCAL-3640, MCAL-3641,MCAL-3642,MCAL-3571,MCAL-3572

Back To Top


Pwm_SetPeriodAndDuty

Refer section 8.3.4 of 1

Design ID DES_PWM_017
Requirements Covered MCAL-3573,MCAL-3574,MCAL-3575, MCAL-3576,MCAL-3533 ,MCAL-3534,MCAL-3643, MCAL-3644, MCAL-3645, MCAL-3640, MCAL-3641, MCAL-3642,MCAL-3577,MCAL-3578,MCAL-3579, MCAL-3580

Back To Top


Pwm_SetOutputToIdle

Refer section 8.3.5 of 1

Design ID DES_PWM_018
Requirements Covered MCAL-3581, MCAL-3582, MCAL-3583, MCAL-3584, MCAL-3585 MCAL-3586,MCAL-3587

Back To Top


Pwm_DisableNotification

Refer section 8.3.7 of 1

Design ID DES_PWM_019
Requirements Covered MCAL-3592,MCAL-3593,MCAL-3594,MCAL-3595, MCAL-3643, MCAL-3645, MCAL-3640, MCAL-3641, MCAL-3642

Back To Top


Pwm_EnableNotification

Refer section 8.3.8 of 1

Design ID DES_PWM_020
Requirements Covered MCAL-3596, MCAL-3597,MCAL-3598, MCAL-3599,MCAL-3600, MCAL-3643, MCAL-3645, MCAL-3640, MCAL-3641, MCAL-3642

Back To Top


Pwm_GetVersionInfo

Refer section 8.3.13 of 1

Design ID DES_PWM_021
Requirements Covered MCAL-3624,MCAL-3625

Back To Top


Pwm_RegisterReadback

As noted from previous implementation, the timer configuration registers could potentially be corrupted by other entities (s/w or h/w). One of the recommended detection methods would be to periodically read-back the configuration and confirm configuration is consistent. The service API defined below shall be implemented to enable this detection.

Description Comments
Service Name Pwm_RegisterReadback Can potentially be turned OFF
Syntax Std_ReturnType Pwm_RegisterReadback(Pwm_ChannelType PwmChannel, Pwm_RegisterReadbackType *RegRbPtr) Pwm_RegisterReadbackType defines the type, that holds critical values, refer below
Service ID 0x0F
Sync / Async Sync
Reentrancy Non Reentrant
Parameter in PwmChannel Identifies a unique valid channel
Parameters out RegRbPtr A pointer of type Pwm_RegisterReadbackType, which holds the read back values
Return Value Standard return type E_OK or E_NOT_OK in case of invalid channel id

The critical register listed is a recommendation and implementation shall determine appropriate registers.

This service could potentially be turned OFF in the configurator.

Design ID DES_PWM_022
Requirements Covered MCAL-3662,MCAL-3656

Back To Top


Global Variables

This design expects that implementation will require to use following global variables.

Variable Type Description Default Value
Pwm_DrvStatus uint8 PWM driver statusPWM_STATUS_UNINIT
Pwm_ChObj Pwm_ChObjType PWM channel object -

Back To Top


Decision Analysis & Resolution (DAR)

Section below list some of the important design decisions and rational behind those decisions.

Timer Mode configuration in Overflow Only Mode for Duty cycle of 50%

The PWM signal generation when duty cycle is 50% and 0% < duty cylcle < 100% can be done in the following ways:

  • Configure the timer in oveflow only mode in the case where the duty cycle is 50%. In this case, the overflow rate of the timer is kept at half the desired PWM period. When 0% < duty cylcle < 100%, the timer is configured in overflow and compare mode with overflow rate kept at the desired period of PWM signal and the formulas given in (Fundamental Operation) are used to calculate the compare and reload register values.
  • Configure the timer in overflow and compare mode always irrespective of duty cycle and the overflow rate is kept at the PWM period and in the case of 50% duty cycle, the compare register TMAR can be kept at half the reload register value.

DAR Criteria

The PWM signal generation from the timer should be optimized.

Available Alternatives

  • Use timer in either Overflow Mode or ( Overflow and Compare Mode) configuration depending on duty cycle
    • Advantages:
      • Incase of 50% duty cycle, only the overflow register condition needs to be checked to generate the interrrupts and PWM signal.
    • Disadvantages:
      • Seperate one time Mode configuration depending on the duty cycle needs to be done in software.
  • Use of Timer in compare and overflow Mode configurations irrespective of duty cycle
    • Advantages:
      • No need to have seperate Mode configuration of timer for different duty cycles. Timer can be configured in overflow and compare mode.
    • Disadvantages:
      • In 50% duty cycle, register compare to TMAR register needs to be performed continuously to detect the compare condition.

Decision

The PWM module is more efficeintly implemented by operating timer in overflow mode alone when duty cycle of 50% is required as this avoids the continuous register compare to TMAR to generate the trigger at compare condition. The configuration to overflow or overflow and compare in different duty cycles needs to be done one time, and is a lesser overhead.

Design ID DES_PWM_023
Requirements Covered MCAL-3533,MCAL-3534

Back To Top


Test Criteria

The sections below identify some of the aspects of design that would require emphasis during testing of this design implementation

  • PWM Wave generation : Polarities
    • Test cases shall check the generation of PWM wave based on different initial polarities configured. This will be verified on the CRO.
  • PWM Wave generation : Duty Cycle, Period and Input clock frequency
    • Test cases shall perform equivalence class test and ensure different duty cycles, periods for a PWM signal can be supported based on input clock frequencies.
    • Test cases should also check for conditions where the PWM parameters are reconfigured while the timer is running.
  • PWM Wave generation :Reset (Period = 0)
    • Test cases should check the behaviour on reset and with Period = 0
  • PWM Multiple Instances
    • Configure multiple PWM instances with duty cycle of 75% and 25%, reset and vary the duty cycles to ensure that the re-entrancy is maintained.

Back To Top


Document Revision History

Revision Date Author Description Status
0.1 25 Feb 2019 Vibha Pant First version Pending Review
0.2 26 Feb 2019 Vibha Pant Review Comments Addressed Approved