![]() |
TI J7ES Imaging User Guide
|
AutoExposure results data structure.
Data Fields | |
| uint32_t | chId |
| uint32_t | expRatio |
| uint32_t | exposureTime [ISS_SENSOR_MAX_EXPOSURE] |
| uint32_t | analogGain [ISS_SENSOR_MAX_EXPOSURE] |
| uint32_t IssSensor_ExposureParams::chId |
Channel Id
| uint32_t IssSensor_ExposureParams::expRatio |
Exposure ration for WDR output format, not used for linear mode
| uint32_t IssSensor_ExposureParams::exposureTime[ISS_SENSOR_MAX_EXPOSURE] |
Exposure time in ms for all exposure outputs, For Linear mode output, only Long exposure entry is used
| uint32_t IssSensor_ExposureParams::analogGain[ISS_SENSOR_MAX_EXPOSURE] |
Exposure time in ms for all exposure outputs, For Linear mode output, only Long exposure entry is used