![]() |
TI Deep Learning Library User Guide
|
TIDL is Texas Instruments' deep learning ecosystem which can be used to import networks trained to solve problems like image classification, object detection and semantic segmentation and execute the networks for inference on Jacinto7 SoC exercising the C7x/MMA cores.
Using TIDL, you are expected to be able to:
.bin files that can be used by TIDL. The following model formats are currently supported:.caffemodel and .prototxt files).pb or .tflite files).onnx files)Note
The networks trained via open frameworks like Caffe or Tensorflow can be exported to files and saved for later use. These files store the network model in a format that can be imported back using the same framework.
In order for TIDL to execute these networks, these files must be imported and converted to a format that TIDL can understand.
.bin files and validate the results.bin files and validate the results
This guide demonstrates the above features and documents the steps that will help you get started on TIDL framework.
Note
If you are not familiar with concepts of deep learning or machine learning, and if this is your first experience with convolutional neural networks (CNN), it is suggested that you start here.
TIDL is installed by SDK installation and can be found inside ${PSDKRA_PATH}/tidl_j7_01_00_00_00. Run the following steps to export required variables and install tools for ease of use.
For Linux Users
Export the path of TIDL root directory as
TIDL_INSTALL_PATH. All examples in this guide will use paths and filenames relative to this directory.user@ubuntu-pc$ export TIDL_INSTALL_PATH=${PSDKRA_PATH}/tidl_j7_01_00_00_00
If you want to visualize the network after importing, it is required to build tidlModelGraphviz tool after installation. The visualisation tool generates .svg files indicating the network flow. The details of the network visualisation tool can be found here
For Linux Users
To build
tidlModelGraphviztool, installgraphviz-devpackage (needed for buildingtidlModelGraphviz) and export the variableTIDL_GRAPHVIZ_PATH.user@ubuntu-pc$ sudo apt install graphviz-dev user@ubuntu-pc$ export TIDL_GRAPHVIZ_PATH=/usrBuild the
tidlModelGraphviztool by runningmakeinti_dl/utils/tidlModelGraphvizdirectory.user@ubuntu-pc$ cd ${TIDL_INSTALL_PATH}/ti_dl/utils/tidlModelGraphviz user@ubuntu-pc$ make
For Windows Users
tidlModelGraphvizis not supported on Windows.
In this section, we will show you some examples of how to import models trained with Caffe and Tensorflow into TIDL. We will use the following models in this guide:
Note
The installation does not create the directories required for storing the downloaded models mentioned in this guide. You should create the directories as required, if they are not already present.
Note
The paths used in this guide are for the purpose of representation alone. You can create your own configuration file (containing the appropriate paths for collecting input models and storing output files), and pass that file's location as an argument to thetidlModelImporttool.
Downloading model
Download the tarball containing the trained model from here..
You need to extract mobilenet_v2_1.0_224_frozen.pb from the tarball and put it inside ti_dl/test/testvecs/models/public/tensorflow/mobilenet_v2 directory.
The downloaded tensorflow models cannot be imported until they are optimized for inference. Run optimize_for_inference.py (distributed with tensorflow installation) to create an optimized model file.
Importing model
To import models using tidlModelImport tool, you need to use a configuration file that provides the import parameters to the tool. The various parameters and the supported values for each parameters are documented here.
You can use the configuration file ti_dl/test/testvecs/config/import/public/tensorflow/tidl_import_mobileNetv2.txt (distributed with the installation) to import this model.
Note
MobileNetV2 trained on tensorflow needs 16 bits for better accuracy. Modify the configuration file to use 16 bits for import.modelType = 1 numParamBits = 15 quantizationStyle = 2 ...
Run the import tool to import the model.
For Linux Users
user@ubuntu-pc$ cd ${TIDL_INSTALL_PATH}/ti_dl/utils/tidlModelImport user@ubuntu-pc$ ./out/tidl_model_import.out ${TIDL_INSTALL_PATH}/ti_dl/test/testvecs/config/import/public/tensorflow/tidl_import_mobileNetv2.txt
For Windows Users
C:\> cd %TIDL_INSTALL_PATH%\ti_dl\utils\tidlModelImport C:\> out/tidl_model_import.out.exe %TIDL_INSTALL_PATH%\ti_dl\test\testvecs\config\import\public\tensorflow\tidl_import_mobileNetv2.txt
The import tool will run quantization, network compilation and performance simulation internally and generate the following files:
.bin files used for inferenceti_dl/test/testvecs/config/tidl_models/tensorflow/tidl_net_mobilenet_v2_1.0_224.binti_dl/test/testvecs/config/tidl_models/tensorflow/tidl_net_mobilenet_v2_1.0_2241.binti_dl/utils/perfsim/tidl_import_mobileNetv2.txt/tidl_import_mobileNetv2.txt_Analysis_DSP1_FRQ1000_DATA1_MSMCS7936_DDRE0.60_EMIFP1_DDRMTS3733_224x224.csvIf you built the tidlModelGraphviz tool as described in Setting up the environment, the network graph representation is also generated in ti_dl/test/testvecs/config/tidl_models/tensorflow/tidl_net_mobilenet_v2_1.0_224.bin.svg.
Downloading model
Download the tarball containing the trained model from here.
You need to extract pelee_304x304_acc7094.caffemodel and deploy.prototxt from the tarball and put it inside ti_dl/test/testvecs/models/public/caffe/peele/pelee_voc/ directory.
The downloaded pelee model should be imported with a higher confidence_threshold parameter for better performance. Modify the file ti_dl/test/testvecs/models/public/caffe/peele/pelee_voc/deploy.prototxt to use 0.4 as confidence_threshold.
Importing model
After the above changes are made to the model, it can be imported by following the steps similar to the ones described in Importing MobileNetV2 model for image classification. You can use ti_dl/test/testvecs/config/import/public/caffe/tidl_import_peeleNet.txt (distributed with the installation) to import the model.
For Linux Users
user@ubuntu-pc$ cd ${TIDL_INSTALL_PATH}/ti_dl/utils/tidlModelImport user@ubuntu-pc$ ./out/tidl_model_import.out ${TIDL_INSTALL_PATH}/ti_dl/test/testvecs/config/import/public/caffe/tidl_import_peeleNet.txt
For Windows Users
C:\> cd %TIDL_INSTALL_PATH%\ti_dl\utils\tidlModelImport C:\> out/tidl_model_import.out.exe %TIDL_INSTALL_PATH%\ti_dl\test\testvecs\config\import\public\caffe\tidl_import_peeleNet.txt
The following files are generated by the import:
.bin files used for inferenceti_dl/test/testvecs/config/tidl_models/caffe/tidl_net_peele_300.binti_dl/test/testvecs/config/tidl_models/caffe/tidl_io_peele_300_1.binti_dl/utils/perfsim/tidl_import_peeleNet.txt/tidl_import_peeleNet.txt_Analysis_DSP1_FRQ1000_DATA0_MSMCS7936_DDRE0.60_EMIFP1_DDRMTS3733_1024x512.csvIf you built the tidlModelGraphviz tool as described in Setting up the environment, the network graph representation is also generated in ti_dl/test/testvecs/config/tidl_models/caffe/tidl_net_peele_300.bin.svg.
Downloading model
Download the trained model from here and put it in ti_dl/test/testvecs/models/public/caffe/jsegNet21 directory.
Note
Do not usesave link asorcopy link locationoptions to download binary files from github.com, use theDownloadbutton instead.
Download the deploy.prototxt file from here and put it in ti_dl/test/testvecs/models/public/caffe/jsegNet21 directory.
Note
Do not usesave link asorcopy link locationoptions to download text files from github.com, use theRawbutton to open the file and then usesave as ...option.
Importing model
The model can be imported by following steps similar to the the ones described in Importing MobileNetV2 model for image classification. You can use ti_dl/test/testvecs/config/import/public/caffe/tidl_import_jSegNet.txt (distributed with the installation) to import the model.
For Linux Users
user@ubuntu-pc$ cd ${TIDL_INSTALL_PATH}/ti_dl/utils/tidlModelImport user@ubuntu-pc$ ./out/tidl_model_import.out ${TIDL_INSTALL_PATH}/ti_dl/test/testvecs/config/import/public/caffe/tidl_import_jSegNet.txt
For Windows Users
C:\> cd %TIDL_INSTALL_PATH%/ti_dl/utils/tidlModelImport C:\> out/tidl_model_import.out.exe %TIDL_INSTALL_PATH%\ti_dl\test\testvecs\config\import\public\caffe\tidl_import_jSegNet.txt
The following files are generated by the import:
.bin files used for inferenceti_dl/test/testvecs/config/tidl_models/caffe/tidl_net_jSegNet_1024x512.binti_dl/test/testvecs/config/tidl_models/caffe/tidl_io_jSegNet_1024x512_1.binti_dl/utils/perfsim/tidl_import_jSegNet.txt/tidl_import_jSegNet.txt_Analysis_DSP1_FRQ1000_DATA0_MSMCS7936_DDRE0.60_EMIFP1_DDRMTS3733_1024x512.csvIf you built the tidlModelGraphviz tool as described in Setting up the environment, the network graph representation is also generated in ti_dl/test/testvecs/config/tidl_models/caffe/tidl_net_jSegNet_1024x512.bin.svg.
The installation comes with a PC simulation tool ti_dl/test/PC_dsp_test_dl_algo.out that can be used to execute imported .bin files and verify the inference result before running them on TI Jacinto7 SoC. This helps in easily identifying the issues with the model and debugging.
The PC simulation tool uses the file ti_dl/test/testvecs/config/config_list.txt to read the list of inference tests to run. The format of the file is as follows:
Each line that starts with 1 must point to a file containing the inference parameters to run an imported model. The various parameters and the supported values for each parameters are documented here.
Note
The lines that start with2are ignored.
The test sequence stops when it hits a line that starts with0.
Note
The paths in the fileti_dl/test/testvecs/config/config_list.txt(e.g./path/to/inference/parameter/file/to/be/executed/1) must be relative toti_dl/utils/test.
For example, to add the inference parameter fileti_dl/test/testvecs/config/infer/public/caffe/tidl_infer_pelee.txtto the list, you must add the following:1 testvecs/config/infer/public/caffe/tidl_infer_pelee.txt
In this section, we will test the models imported in Importing models using the inference parameter files distributed with the installation.
Add the following lines at the beginning of ti_dl/test/testvecs/config/config_list.txt:
Run PC_dsp_test_dl_algo.out from ti_dl/test directory.
Decoding the output
The test uses the ti_dl/test/testvecs/input/airshow.bmp as input image and 896 as test label.
Note
This information is obtained from the input configuration fileti_dl/test/testvecs/config/classification_list_1.txt.
The input configuration file is provided asinDataparameter inti_dl/test/testvecs/config/infer/public/tensorflow/tidl_infer_mobileNetv2.txt
The numbers printed by the classification test represent the following information:
For example, the above output indicates that the simulation took 655.09 milliseconds, the test input label was 896, the infered label was 896, and the TOP-1 and TOP-5 accuracies are both 1.0.
Add the following lines at the beginning of ti_dl/test/testvecs/config/config_list.txt:
Run PC_dsp_test_dl_algo.out from ti_dl/test directory.
Decoding the output
The test uses the ti_dl/test/testvecs/input/ti_lindau_000020.bmp as input image for object detection.
The test prints the time taken by PC simulation and stores the list of detected objects and the coordinates for each detected object in ti_dl/test/testvecs/output/pelee.bin_ti_lindau_000020.bmp_000000.txt. It also generates a post-processed output image at ti_dl/test/testvecs/output/pelee.bin_ti_lindau_000020.bmp_000000_tidl_post_proc2.png that shows the detected objects and the bounding boxes.
| Input | output --------------------— |
|---|---|
Input image to object detection application |
output of object detection application |
Add the following lines at the beginning of ti_dl/test/testvecs/config/config_list.txt:
Run PC_dsp_test_dl_algo.out from ti_dl/test directory.
The test uses the ti_dl/test/testvecs/input/ti_lindau_I00000.bmp as input image for semantic segmentation.
The test prints the time taken by PC simulation and stores the generates a post-processed output image at ti_dl/test/testvecs/output/jsegNet1024x512.bin_ti_lindau_I00000.bmp_000000_tidl_post_proc3.png that shows the generated segmentation masks for the detected objects.
| Input | output --------------------— |
|---|---|
Input image to semantic segmentation application |
output of semantic segmentation application |
Note
You can also run all 3 of the above tests in a single run ofPC_dsp_test_dl_algo.outby adding the following lines in the beginning ofti_dl/test/testvecs/config/config_list.txt:1 testvecs/config/infer/public/tensorflow/tidl_infer_mobileNetv2.txt 1 testvecs/config/infer/public/caffe/tidl_infer_pelee.txt 1 testvecs/config/infer/public/caffe/tidl_infer_jSegNet.txt 0
The .bin files generated by tidlModelImport can be tested on Jacinto7 SoC using the TI_DEVICE_dsp_test_dl_algo.out binary (distributed with the installation). This section will describe the steps required to run the imported models on target. We will use the three models from Importing models.
H/W requirements
Preparing the SD card
Copy ti_dl/test/testvecs directory to SD card. Also, create a directory named trace in the SD card.
For Linux Users
user@ubuntu-pc$ cd /path/to/SD/card/mount user@ubuntu-pc$ export SDCARD_MOUNT_DIR=${PWD} user@ubuntu-pc$ user@ubuntu-pc$ mkdir trace user@ubuntu-pc$ cp -ar ${TIDL_INSTALL_PATH}/ti_dl/test/testvecs . user@ubuntu-pc$ rm -Rf testvecs/output/* user@ubuntu-pc$ sync
Note
Export the variableSDCARD_MOUNT_DIRto point to the directory where the SD Card is mounted. This variable will be used in this guide to modify files in the SD Card.
As an additional step, delete the contents of${SDCARD_MOUNT_DIR}/testvecs/output. The output data and postprocessed images from Running imported models in PC simulation are also copied to the SD Card which will be overwritten byTI_DEVICE_dsp_test_dl_algo.out.
TI_DEVICE_dsp_test_dl_algo.out reads the file testvecs/config/config_list.txt from SD card to create a list of inference configurations that should be run back-to-back. Add the following lines in the beginning of ${SDCARD_MOUNT_DIR}/testvecs/config/config_list.txt:
Note
If you have followed the steps in Running imported models in PC simulation and copied the files without any modification, these lines will be present in the copied file.
Booting up the EVM
Insert the SD card in to the EVM and power on the EVM. Start CCS and run the steps as described in SDK user guide to initialise sciclient.
Loading Test application to C7x/MMA
Note
Before you launch${TIDL_INSTALL_PATH}/ti_dl/utils/targetTest/launch_tidl.js, you will need to changetidlPathvariable so that it points to${TIDL_INSTALL_PATH}... } //TIDL path. Edit this tidlPath = "/path/to/tidl_j7_01_00_00_00"; //path to board config elf fastfileIO_a72_out_file = tidlPath+"/ti_dl/utils/targetTest/vx_app_tirtos_fileio_mpu1.out" ...
Run ${TIDL_INSTALL_DIR}/ti_dl/utils/targetTest/launch_tidl.js in CCS to load the TI_DEVICE_dsp_test_dl_algo.out binary to C7x/MMA core. This script also loads vx_app_tirtos_fileio_mpu1.out binary to A72 core for reading / writing files rom SD Card.
After this step, C7x/MMA core will be halted at tidlMultiInstanceTest() function and is ready for running.
Running tests on C7x/MMA
Delete / disable the breakpoint at tidlMultiInstanceTest() and click Resume button on CCS to set the C7x/MMA core to running. The application will run all tests in testvecs/config/config_list.txt one-by-one.
Decoding the output
The test output is printed on CCS console which shows the number of megacycles taken for each test case. Assuming C7x is running at 1 GHz, the time-taken-per-frame and FPS for each test can be calculated as:
Time-taken-per-frame in milliseconds = (1000 / C7x CPU clock in MHz) x Number of mega cycles
FPS = 1 / Time-taken-per-frame in milliseconds
For example, From the output above:
| Test | Mega cycles count | Time taken pe | |
|---|---|---|---|
| JSegNet21V2 | 8.58 | 8.58 | 116.55 |
| PeleeNet | 104.13 | 104.13 | 9.60 |
| MobileNetV2 | 6.33 | 6.33 | 157.98 |
For image classification tests, the input class and the inferred class is also printed (e.g. in MobileNetV2 test).
After all the tests are complete, the postprocessed images for object detection and semantic segmentation are stored in testvecs/output.
Note
The post processing code for PeleeNet is not optimized and therefore it takes a longer time to execute.
Please refer to Data sheet for the performance summary of validated networks
Validating test output
Take the SD card out of the EVM and plug it into PC. After the SD card is mounted in ${SDCARD_MOUNT_DIR}, you can check the contents in ${SDCARD_MOUNT_DIR}/testvecs/output.
The postprocessed output files should be presnt in
${SDCARD_MOUNT_DIR}/testvecs/output/pelee.bin_ti_lindau_000020.bmp_000000_tidl_post_proc2.bmp${SDCARD_MOUNT_DIR}/testvecs/output/jsegNet1024x512.bin_ti_lindau_I00000.bmp_000000_tidl_post_proc3.bmpThis document provides a step-by-step approach towards getting started with TIDL.
.bin files using tidlModelImport tool on PC.tidlModelImport can be found here