![]() |
Perception Tool Kit (PTK) API Guide
|
|
Data Structures | |
| struct | PTK_Alg_FusedOgmapTime |
| Containes for holding time stamps for different sensors. More... | |
| struct | PTK_Alg_FusedOgmapParams |
| Configuration parameters. More... | |
Functions | |
| void | PTK_Alg_FusedOgmapGetMapConfig (const PTK_Alg_FusedOgmapParams *cfgParams, PTK_MapConfig *config) |
| Initializes the map configuration based on the given algorithm configuration parameters. More... | |
| int32_t | PTK_Alg_FusedOgmapConfig (const PTK_Alg_FusedOgmapParams *cfgParams, PTK_Api_MemoryReq *memReq) |
| Computes the memory requirements based on the given algorithm configuration parameters. More... | |
| PTK_AlgHandle | PTK_Alg_FusedOgmapInit (const PTK_Alg_FusedOgmapParams *cfgParams, const PTK_Api_MemoryRsp *memRsp) |
| Initializes the library based on the given algorithm configuration parameters and allocated memory blocks. More... | |
| int32_t | PTK_Alg_FusedOgmapProcess (PTK_AlgHandle *algHandle, PTK_Alg_FusedOgmapParams *cfgParams, const PTK_Grid *cameraGrid, const PTK_Grid *radarGrid, const PTK_Grid *lidarGrid, PTK_INS_Record *insRec, const PTK_RigidTransform_d *Md_ecef_w, PTK_Grid *outGrid, PTK_Grid *fusedDSGrid) |
| Processes the given point cloud and performs the Occupancy grid mapping. More... | |
| void | PTK_Alg_FusedOgmapDeInit (PTK_AlgHandle algHandle) |
| De-initializes the algorithm context. More... | |
Macros | |
| #define | PTK_ALG_FUSED_OGMAP_METHOD_VOTING (0U) |
| Voting method based fusion. More... | |
| #define | PTK_ALG_FUSED_OGMAP_METHOD_DS (1U) |
| Dempster-Shafer method based fusion. More... | |
| #define | PTK_ALG_FUSED_OGMAP_FUSIONTABLE_SIZE (26U) |
| Voting based fusion table size. More... | |
| #define | PTK_ALG_FUSED_OGMAP_DSWEIGHTS_SIZE (9U) |
| Dempster-Shafer weight table size. More... | |
| #define | PTK_ALG_FUSED_OGMAP_DSTHRESH_SIZE (9U) |
| Dempster-Shafer threshold table size. More... | |
| #define PTK_ALG_FUSED_OGMAP_METHOD_VOTING (0U) |
Voting method based fusion.
| #define PTK_ALG_FUSED_OGMAP_METHOD_DS (1U) |
Dempster-Shafer method based fusion.
| #define PTK_ALG_FUSED_OGMAP_FUSIONTABLE_SIZE (26U) |
Voting based fusion table size.
| #define PTK_ALG_FUSED_OGMAP_DSWEIGHTS_SIZE (9U) |
Dempster-Shafer weight table size.
| #define PTK_ALG_FUSED_OGMAP_DSTHRESH_SIZE (9U) |
Dempster-Shafer threshold table size.
| void PTK_Alg_FusedOgmapGetMapConfig | ( | const PTK_Alg_FusedOgmapParams * | cfgParams, |
| PTK_MapConfig * | config | ||
| ) |
Initializes the map configuration based on the given algorithm configuration parameters.
| [in] | cfgParams | Algorithm configuration parameters. |
| [out] | config | Map configuration |
| int32_t PTK_Alg_FusedOgmapConfig | ( | const PTK_Alg_FusedOgmapParams * | cfgParams, |
| PTK_Api_MemoryReq * | memReq | ||
| ) |
Computes the memory requirements based on the given algorithm configuration parameters.
| [in] | cfgParams | Algorithm configuration parameters. |
| [out] | memReq | Memory requirements as specified below
|
| PTK_AlgHandle PTK_Alg_FusedOgmapInit | ( | const PTK_Alg_FusedOgmapParams * | cfgParams, |
| const PTK_Api_MemoryRsp * | memRsp | ||
| ) |
Initializes the library based on the given algorithm configuration parameters and allocated memory blocks.
| [in] | cfgParams | Algorithm configuration parameters. It is ecpected that the same configuration parameters passed in the PTK_Alg_FusedOgmapConfig() API are given. No check can be made to make sure these are the same. Failure to provide the same parameter set might result in an unexpected behavior (ex:- memory requirements could be different for different parameter set). |
| [in] | memRsp | Memory blocks as specified below
|
| int32_t PTK_Alg_FusedOgmapProcess | ( | PTK_AlgHandle * | algHandle, |
| PTK_Alg_FusedOgmapParams * | cfgParams, | ||
| const PTK_Grid * | cameraGrid, | ||
| const PTK_Grid * | radarGrid, | ||
| const PTK_Grid * | lidarGrid, | ||
| PTK_INS_Record * | insRec, | ||
| const PTK_RigidTransform_d * | Md_ecef_w, | ||
| PTK_Grid * | outGrid, | ||
| PTK_Grid * | fusedDSGrid | ||
| ) |
Processes the given point cloud and performs the Occupancy grid mapping.
| [in,out] | algHandle | Algorithm handle. |
| [in] | cfgParams | Configuration parameters. |
| [in] | cameraGrid | OGMAP grid from camera processing |
| [in] | radarGrid | OGMAP grid from radar processing |
| [in] | lidarGrid | OGMAP grid from lidar processing |
| [in] | insRec | INS record corresponding to the sensor maps. |
| [in] | insRec | INS record corresponding to the sensor maps. |
| [in] | Md_ecef_w | Transform from world to ECEF. |
| [out] | outGrid | Fused output OGMAP grid. |
| [out] | fusedDSGrid | Output Dempster-Shafer grid. |
| void PTK_Alg_FusedOgmapDeInit | ( | PTK_AlgHandle | algHandle | ) |
De-initializes the algorithm context.
| [in,out] | algHandle | Algorithm handle. |