![]() |
PDK Documentation
|
DSS Video Pipe Luma Key Config parameters.
Data Fields | |
| uint32_t | lumaKeyEnable |
| uint32_t | lumaKeyMinVal |
| uint32_t | lumaKeyMaxVal |
| uint32_t CSL_DssVidPipeLumaCfg::lumaKeyEnable |
Enable Luma Key transparency matching FALSE: Disable luma key operation TRUE: Enable luma key operation
| uint32_t CSL_DssVidPipeLumaCfg::lumaKeyMinVal |
12 bit Luma Key Min Value. luma_key_min <= Pixel's y <= luma_key_max. If condition is true alpha value will be forced to ZERO
| uint32_t CSL_DssVidPipeLumaCfg::lumaKeyMaxVal |
12 bit Luma Key Max Value. luma_key_min <= Pixel's y <= luma_key_max. If condition is true alpha value will be forced to ZERO