![]() |
PDK Documentation
|
DMSC controls the power management, security and resource management of the device.
Files | |
| file | tisci_protocol.h |
| This file contains: | |
Data Structures | |
| struct | Sciclient_RomFirmwareLoadHdr_t |
| Header that prefixes all TISCI messages. More... | |
| struct | tisci_sec_header |
| Header that prefixes all TISCI messages sent via secure transport. More... | |
Variables | |
| struct tisci_header | __attribute__ |
| #define TISCI_MSG_FLAG_RESERVED0 TISCI_BIT(0) |
This flag is reserved and not to be used.
| #define TISCI_MSG_FLAG_AOP TISCI_BIT(1) |
ACK on Processed: Send a response to a message after it has been processed with TISCI_MSG_FLAG_ACK set if the processing succeeded, or a NAK otherwise. This response contains the complete response to the message with the result of the actual action that was requested.
| #define TISCI_MSG_FLAG_SEC TISCI_BIT(2) |
Indicate that this message is marked secure
| #define TISCI_MSG_FLAG_ACK TISCI_BIT(1) |
Response flag for a message that indicates success. If this flag is NOT set then that is to be interpreted as a NAK.
| #define TISCI_MSG_VERSION (0x0002U) |
| #define TISCI_MSG_BOOT_NOTIFICATION (0x000AU) |
| #define TISCI_MSG_BOARD_CONFIG (0x000BU) |
| #define TISCI_MSG_BOARD_CONFIG_RM (0x000CU) |
| #define TISCI_MSG_BOARD_CONFIG_SECURITY (0x000DU) |
| #define TISCI_MSG_BOARD_CONFIG_PM (0x000EU) |
| #define TISCI_MSG_ENABLE_WDT (0x0000U) |
| #define TISCI_MSG_WAKE_RESET (0x0001U) |
| #define TISCI_MSG_WAKE_REASON (0x0003U) |
| #define TISCI_MSG_GOODBYE (0x0004U) |
| #define TISCI_MSG_SYS_RESET (0x0005U) |
| #define TISCI_MSG_QUERY_MSMC (0x0020U) |
| #define TISCI_MSG_SET_CLOCK (0x0100U) |
| #define TISCI_MSG_GET_CLOCK (0x0101U) |
| #define TISCI_MSG_SET_CLOCK_PARENT (0x0102U) |
| #define TISCI_MSG_GET_CLOCK_PARENT (0x0103U) |
| #define TISCI_MSG_GET_NUM_CLOCK_PARENTS (0x0104U) |
| #define TISCI_MSG_SET_FREQ (0x010cU) |
| #define TISCI_MSG_QUERY_FREQ (0x010dU) |
| #define TISCI_MSG_GET_FREQ (0x010eU) |
| #define TISCI_MSG_SET_DEVICE (0x0200U) |
| #define TISCI_MSG_GET_DEVICE (0x0201U) |
| #define TISCI_MSG_SET_DEVICE_RESETS (0x0202U) |
| #define TISCI_MSG_DEVICE_DROP_POWERUP_REF (0x0203U) |
| #define TISCI_MSG_SET_FWL_REGION (0x9000U) |
Message to set a firewall region configuration
| #define TISCI_MSG_GET_FWL_REGION (0x9001U) |
Message to get a firewall region configuration
| #define TISCI_MSG_CHANGE_FWL_OWNER (0x9002U) |
Message to change firewall region owner
| #define TISCI_MSG_SA2UL_SET_DKEK (0x9003U) |
Message to derive a KEK and set SA2UL DKEK register
| #define TISCI_MSG_SA2UL_RELEASE_DKEK (0x9004U) |
Message to erase the DKEK register
| #define TISCI_MSG_KEYSTORE_IMPORT_SKEY (0x9005U) |
Message to import a symmetric key to the keystore
| #define TISCI_MSG_KEYSTORE_ERASE_SKEY (0x9006U) |
Message to erase a imported symmetric key in the keystore
| #define TISCI_MSG_KEYSTORE_IMPORT_ASKEY (0x9007U) |
Message to import a asymmetric key to the keystore
| #define TISCI_MSG_KEYSTORE_ERASE_ASKEY (0x9008U) |
Message to erase a imported asymmetric key in the keystore
| #define TISCI_MSG_SET_ISC_REGION (0x9009U) |
Message to set a ISC region configuration
| #define TISCI_MSG_GET_ISC_REGION (0x900AU) |
Message to get a ISC region configuration
| #define TISCI_MSG_FWL_EXCP_NOTIFICATION (0x900BU) |
Notification for firewall exception
| #define TISCI_MSG_OPEN_DEBUG_FWLS (0x900CU) |
Message to open debug firewalls using a certificate
| #define TISCI_MSG_KEYSTORE_WRITE (0x900DU) |
Message to write partitioning data and provisioned keys to the keystore memory
| #define TISCI_MSG_KEYSTORE_EXPORT_ALL (0x900EU) |
Message to encrypt and export the full keystore contents for saving to external storage
| #define TISCI_MSG_KEYSTORE_IMPORT_ALL (0x900FU) |
Message to import and decrypt a previously exported keystore blob
| #define TISCI_MSG_SA2UL_PKA_RSA_SIGN_PRIM (0x9010U) |
Message to perform the RSA signature primitive
| #define TISCI_MSG_SA2UL_PKA_RSA_VERIFY_PRIM (0x9011U) |
Message to perform the RSA verification primitive
| #define TISCI_MSG_SA2UL_PKA_RSA_ENCRYPT_PRIM (0x9012U) |
Message to perform the RSA encryption primitive
| #define TISCI_MSG_SA2UL_PKA_RSA_DECRYPT_PRIM (0x9013U) |
Message to perform the RSA decryption primitive
| #define TISCI_MSG_SA2UL_PKA_ECDSA_SIGN (0x9014U) |
Message to sign a message hash with an EC private key
| #define TISCI_MSG_SA2UL_PKA_ECDSA_VERIFY (0x9015U) |
Message to verify an EC signature
| #define TISCI_MSG_KEYSTORE_GEN_SKEY_FROM_RNG (0x9016U) |
Message to generate a symmetric key via RNG and save it in the runtime keystore
| #define TISCI_MSG_GET_RANDOM (0x9020U) |
Message to get random numbers
| #define TISCI_MSG_PROC_REQUEST (0xC000U) |
Message to get a Processor
| #define TISCI_MSG_PROC_RELEASE (0xC001U) |
Message to release a Processor
| #define TISCI_MSG_PROC_HANDOVER (0xC005U) |
Message to handover a Processor
| #define TISCI_MSG_PROC_SET_CONFIG (0xC100U) |
Message to Set the processor configuration
| #define TISCI_MSG_PROC_SET_CONTROL (0xC101U) |
Message to Set the processor control
| #define TISCI_MSG_PROC_GET_STATUS (0xC400U) |
Message to Get the processor status
| #define TISCI_MSG_PROC_WAIT_STATUS (0xC401U) |
Message to Wait for processor status
| #define TISCI_MSG_PROC_AUTH_BOOT (0xC120U) |
Message to do authenticated boot configuration of a processor
| #define TISCI_MSG_RM_GET_RESOURCE_RANGE (0x1500U) |
RM TISCI message to request a resource range assignment for a host
| #define TISCI_MSG_RM_IRQ_SET (0x1000U) |
RM TISCI message to set an IRQ between a peripheral and host processor
| #define TISCI_MSG_RM_IRQ_RELEASE (0x1001U) |
RM TISCI message to release a configured IRQ
| #define TISCI_MSG_RM_RESERVED_1100 (0x1100U) |
| #define TISCI_MSG_RM_RESERVED_1101 (0x1101U) |
| #define TISCI_MSG_RM_RESERVED_1102 (0x1102U) |
| #define TISCI_MSG_RM_RESERVED_1103 (0x1103U) |
| #define TISCI_MSG_RM_RING_CFG (0x1110U) |
RM TISCI message to configure a Navigator Subsystem ring
| #define TISCI_MSG_RM_RING_GET_CFG (0x1111U) |
RM TISCI message to get the register cfg for a Navigator Subsystem ring
| #define TISCI_MSG_RM_RING_MON_CFG (0x1120U) |
RM TISCI message to configure a Navigator Subsystem ring monitor
| #define TISCI_MSG_RM_RESERVED_1200 (0x1200U) |
| #define TISCI_MSG_RM_RESERVED_1201 (0x1201U) |
| #define TISCI_MSG_RM_UDMAP_TX_CH_CFG (0x1205U) |
RM TISCI message to configure a Navigator Subsystem UDMAP transmit channel
| #define TISCI_MSG_RM_UDMAP_TX_CH_GET_CFG (0x1206U) |
RM TISCI message to get the register cfg for a Navigator Subsystem UDMAP transmit channel
| #define TISCI_MSG_RM_RESERVED_1210 (0x1210U) |
| #define TISCI_MSG_RM_RESERVED_1211 (0x1211U) |
| #define TISCI_MSG_RM_UDMAP_RX_CH_CFG (0x1215U) |
RM TISCI message to configure a Navigator Subsystem UDMAP receive channel
| #define TISCI_MSG_RM_UDMAP_RX_CH_GET_CFG (0x1216U) |
RM TISCI message to get the register cfg for a Navigator Subsystem UDMAP receive channel
| #define TISCI_MSG_RM_RESERVED_1220 (0x1220U) |
| #define TISCI_MSG_RM_RESERVED_1221 (0x1221U) |
| #define TISCI_MSG_RM_UDMAP_FLOW_CFG (0x1230U) |
RM TISCI message to configure a Navigator Subsystem UDMAP receive flow
| #define TISCI_MSG_RM_UDMAP_FLOW_SIZE_THRESH_CFG (0x1231U) |
RM TISCI message to configure a Navigator Subsystem UDMAP receive flow's optional, size based free descriptor queue registers
| #define TISCI_MSG_RM_UDMAP_FLOW_GET_CFG (0x1232U) |
RM TISCI message to get the register cfg for a Navigator Subsystem UDMAP receive flow's standard registers
| #define TISCI_MSG_RM_UDMAP_FLOW_SIZE_THRESH_GET_CFG (0x1233U) |
RM TISCI message to get the register cfg for a Navigator Subsystem UDMAP receive flow's size based free descriptor queue registers
| #define TISCI_MSG_RM_UDMAP_GCFG_CFG (0x1240U) |
RM TISCI message to configure a Navigator Subsystem UDMAP global configuration
| #define TISCI_MSG_RM_UDMAP_GCFG_GET_CFG (0x1241U) |
RM TISCI message to get the register cfg for a Navigator Subsystem UDMAP global configuration
| #define TISCI_MSG_RM_PSIL_PAIR (0x1280U) |
RM TISCI message to pair PSI-L source and destination threads
| #define TISCI_MSG_RM_PSIL_UNPAIR (0x1281U) |
RM TISCI message to unpair PSI-L source and destination threads
| #define TISCI_MSG_RM_PSIL_READ (0x1282U) |
RM TISCI message to read PSI-L thread RT registers via the PSI-L proxy
| #define TISCI_MSG_RM_PSIL_WRITE (0x1283U) |
RM TISCI message to write PSI-L thread RT registers via the PSI-L proxy
| struct tisci_header __attribute__ |