PDK Documentation

Introduction

Functions

void CSL_MDIO_getVersionInfo (CSL_mdioHandle hMdioRegs, CSL_MDIO_VERSION *mdioVersionInfo)
 
uint16_t CSL_MDIO_getClkDivVal (CSL_mdioHandle hMdioRegs)
 
void CSL_MDIO_setClkDivVal (CSL_mdioHandle hMdioRegs, uint16_t clkDivVal)
 
uint32_t CSL_MDIO_isStateMachineEnabled (CSL_mdioHandle hMdioRegs)
 
void CSL_MDIO_enableStateMachine (CSL_mdioHandle hMdioRegs)
 
void CSL_MDIO_disableStateMachine (CSL_mdioHandle hMdioRegs)
 
uint32_t CSL_MDIO_isPhyAlive (CSL_mdioHandle hMdioRegs, uint32_t phyAddr)
 
uint32_t CSL_MDIO_isPhyLinked (CSL_mdioHandle hMdioRegs, uint32_t phyAddr)
 
uint32_t CSL_MDIO_isUnmaskedLinkStatusChangeIntSet (CSL_mdioHandle hMdioRegs, uint32_t index)
 
void CSL_MDIO_clearUnmaskedLinkStatusChangeInt (CSL_mdioHandle hMdioRegs, uint32_t index)
 
uint32_t CSL_MDIO_phyRegRead (uint32_t baseAddr, uint32_t phyAddr, uint32_t regNum, uint16_t *pData)
 
void CSL_MDIO_phyRegWrite (uint32_t baseAddr, uint32_t phyAddr, uint32_t regNum, uint16_t wrVal)
 This API writes a PHY register using MDIO. More...
 
uint32_t CSL_MDIO_phyLinkStatus (uint32_t baseAddr, uint32_t phyAddr)
 This API reads the link status of all PHY connected to this MDIO. The bit corresponding to the PHY address will be set if the PHY link is active. More...
 
void CSL_MDIO_enableLinkStatusChangeInterrupt (CSL_mdioHandle hMdioRegs, Uint32 index, Uint32 phyAddr)
 Enable MDIO link interrupt (MDIO_LINKINT) for PHY monitoring. More...
 
void CSL_MDIO_disableLinkStatusChangeInterrupt (CSL_mdioHandle hMdioRegs, Uint32 index, Uint32 phyAddr)
 Disable MDIO link interrupt (MDIO_LINKINT) for PHY monitoring. More...
 
void CSL_MDIO_enableFaultDetect (CSL_mdioHandle hMdioRegs)
 
void CSL_MDIO_disableFaultDetect (CSL_mdioHandle hMdioRegs)
 
void CSL_MDIO_enablePreamble (CSL_mdioHandle hMdioRegs)
 
void CSL_MDIO_disablePreamble (CSL_mdioHandle hMdioRegs)
 
uint32_t CSL_MDIO_phyRegRead2 (CSL_mdioHandle hMdioRegs, uint32_t userGroup, uint32_t phyAddr, uint32_t regNum, uint16_t *pData)
 
void CSL_MDIO_phyRegWrite2 (CSL_mdioHandle hMdioRegs, uint32_t userGroup, uint32_t phyAddr, uint32_t regNum, uint16_t wrVal)
 This API writes a PHY register using MDIO. More...
 
uint32_t CSL_MDIO_phyLinkStatus2 (CSL_mdioHandle hMdioRegs, uint32_t phyAddr)
 This API reads the link status of all PHY connected to this MDIO. The bit corresponding to the PHY address will be set if the PHY link is active. More...
 
uint32_t CSL_MDIO_isStatusChangeModeInterruptEnabled (CSL_mdioHandle hMdioRegs)
 Check if the MDIO link interrupt (MDIO_LINKINT) is enabled. More...
 
void CSL_MDIO_enableStatusChangeModeInterrupt (CSL_mdioHandle hMdioRegs)
 Enable MDIO link interrupt (MDIO_LINKINT) More...
 
void CSL_MDIO_disableStatusChangeModeInterrupt (CSL_mdioHandle hMdioRegs)
 Disable MDIO link interrupt (MDIO_LINKINT) More...
 
Uint32 CSL_MDIO_getLinkStatusChangePhyAddr (CSL_mdioHandle hMdioRegs, Uint32 index)
 Get the PHY address being monitored. More...
 
int32_t CSL_MDIO_phyRegInitiateWrite (CSL_mdioHandle hMdioRegs, uint32_t userGroup, uint32_t phyAddr, uint32_t regNum, uint16_t wrVal)
 This API inititates a write to PHY register using MDIO. More...
 
uint32_t CSL_MDIO_isStateChangeModeEnabled (CSL_mdioHandle hMdioRegs)
 Checks if the State Change Mode is enabled or not. More...
 
void CSL_MDIO_enableStateChangeMode (CSL_mdioHandle hMdioRegs)
 This function enables the MDIO State Change Mode. More...
 
void CSL_MDIO_disableStateChangeMode (CSL_mdioHandle hMdioRegs)
 This function disables the MDIO State Change Mode. More...
 
void CSL_MDIO_setPollIPG (CSL_mdioHandle hMdioRegs, uint8_t ipgVal)
 Set Polling Inter Packet Gap value. More...
 
uint8_t CSL_MDIO_getPollIPG (CSL_mdioHandle hMdioRegs)
 Get Polling Inter Packet Gap value. More...
 
void CSL_MDIO_setPollEnableMask (CSL_mdioHandle hMdioRegs, uint32_t pollEnableMask)
 Set poll enable mask. More...
 
uint32_t CSL_MDIO_getPollEnableMask (CSL_mdioHandle hMdioRegs)
 Get poll enable mask. More...
 

Function Documentation

◆ CSL_MDIO_getVersionInfo()

void CSL_MDIO_getVersionInfo ( CSL_mdioHandle  hMdioRegs,
CSL_MDIO_VERSION *  mdioVersionInfo 
)

============================================================================
CSL_MDIO_getVersionInfo

Description
This function retrieves the MDIO version information.

Arguments

       mdioVersionInfo     CSL_MDIO_VERSION structure that needs to be populated
                           with the version info read from the hardware.
*     

Return Value
None

Pre Condition
None

Post Condition
None

Reads
MDIO_VERSION_REG_REVMINOR, MDIO_VERSION_REG_REVMAJ, MDIO_VERSION_REG_MODID

Example

       CSL_MDIO_VERSION    mdioVersionInfo;

       CSL_MDIO_getVersion (&mdioVersionInfo);

◆ CSL_MDIO_getClkDivVal()

uint16_t CSL_MDIO_getClkDivVal ( CSL_mdioHandle  hMdioRegs)

=================================================================================================
CSL_MDIO_getClkDivVal

Description
This function retrieves the clock divider value (CLKDIV) from the MDIO control register.

Arguments None

Return Value uint32_t

Pre Condition
None

Post Condition
None

Reads
MDIO_CONTROL_REG_CLKDIV

Example

 *      uint16_t      clkDivVal;

        clkDivVal   =   CSL_MDIO_getClkDivVal ();

◆ CSL_MDIO_setClkDivVal()

void CSL_MDIO_setClkDivVal ( CSL_mdioHandle  hMdioRegs,
uint16_t  clkDivVal 
)

============================================================================
CSL_MDIO_setClkDivVal

Description
This function configures the clock divider value (CLKDIV) in the MDIO control register with the value specified.

Arguments

       clkDivVal           The value to use for clock divider configuration.
                           When this set to 0, the MDIO clock is disabled.
*     

Return Value
None

Pre Condition
None

Post Condition
CONTROL_REG configured with the clock divider value. Configures the MDIO clock frequency.

Writes
MDIO_CONTROL_REG_CLKDIV

Example

*      uint16_t      clkDivVal;

       clkDivVal = 165;

       // Setup the MDIO clock frequency
       CSL_MDIO_setClkDivVal (clkDivVal);

◆ CSL_MDIO_isStateMachineEnabled()

uint32_t CSL_MDIO_isStateMachineEnabled ( CSL_mdioHandle  hMdioRegs)

============================================================================
CSL_MDIO_isStateMachineEnabled

Description
This function returns the value of the Enable bit of the MDIO control register. It returns 1 to indicate that the MDIO state machine is enabled and is active and 0 to indicate otherwise.

Arguments None

Return Value uint32_t

Pre Condition
None

Post Condition
None

Reads
MDIO_CONTROL_REG_ENABLE

Example

     if (CSL_MDIO_isStateMachineEnabled ())
     {
         // MDIO state machine enabled
     }
     else
     {
         // MDIO state machine disabled
     }

◆ CSL_MDIO_enableStateMachine()

void CSL_MDIO_enableStateMachine ( CSL_mdioHandle  hMdioRegs)

============================================================================
CSL_MDIO_enableStateMachine

Description
This function enables the MDIO state machine if not already active.

Arguments None

Return Value
None

Pre Condition
None

Post Condition
Enables MDIO State machine.

Writes
MDIO_CONTROL_REG_ENABLE

Example

*
       // Enable MDIO state machine
       CSL_MDIO_enableStateMachine ();

◆ CSL_MDIO_disableStateMachine()

void CSL_MDIO_disableStateMachine ( CSL_mdioHandle  hMdioRegs)

============================================================================
CSL_MDIO_disableStateMachine

Description
This function sets the 'ENABLE' bit of the MDIO control register to 0, triggering the disable of MDIO state machine if active.

Arguments None

Return Value
None

Pre Condition
None

Post Condition
If the MDIO state machine is active at the time it is disabled, will complete the current operation before halting it and setting the idle bit.

Writes
MDIO_CONTROL_REG_ENABLE=0

Example

*
       // Disable MDIO state machine
       CSL_MDIO_disableStateMachine ();

◆ CSL_MDIO_isPhyAlive()

uint32_t CSL_MDIO_isPhyAlive ( CSL_mdioHandle  hMdioRegs,
uint32_t  phyAddr 
)

============================================================================
CSL_MDIO_isPhyAlive

Description
For a given PHY address provided to this function in 'phyAddr', this function reads the 'ALIVE' bit corresponding to that PHY; The function returns 1 to indicate that the most recent access for the address was acknowledged by the PHY and 0 otherwise.

Arguments

*      phyAddr             The PHY address number (0-31) for which the alive bit
*                          status must be checked and returned by this function.
*   

Return Value uint32_t

Pre Condition
None

Post Condition
None

Reads
MDIO_ALIVE_REG

Example

*      uint32_t      phyAddr = 0;

       // Check if PHY Address 0 is alive
       if (CSL_MDIO_isPhyAlive (phyAddr))
       {
           // MDIO PHY 0 access succeeded
       }
       else
       {
           // MDIO PHY 0 access failed
       }

◆ CSL_MDIO_isPhyLinked()

uint32_t CSL_MDIO_isPhyLinked ( CSL_mdioHandle  hMdioRegs,
uint32_t  phyAddr 
)

============================================================================
CSL_MDIO_isPhyLinked

Description
For a given PHY address provided to this function in 'phyAddr', this function reads the 'LINK' bit corresponding to that PHY; The function returns 1 to indicate that the corresponding PHY address has a link.

Arguments

*      phyAddr             The PHY address number (0-31) for which the link bit
*                          status must be checked and returned by this function.
*   

Return Value uint32_t

Pre Condition
None

Post Condition
None

Reads
MDIO_LINK_REG

Example

*      uint32_t      phyAddr = 0;

       // Check if PHY Address 0 link is up
       if (CSL_MDIO_isPhyLinked (phyAddr))
       {
           // MDIO PHY 0 link up
       }
       else
       {
           // MDIO PHY 0 link not up
       }

◆ CSL_MDIO_isUnmaskedLinkStatusChangeIntSet()

uint32_t CSL_MDIO_isUnmaskedLinkStatusChangeIntSet ( CSL_mdioHandle  hMdioRegs,
uint32_t  index 
)

============================================================================
CSL_MDIO_isUnmaskedLinkStatusChangeIntSet

Description
For a given PHY selector(0-1) provided corresponding to the PHY address in USERPHYSEL register, this function returns the 'LINKINTRAW' register contents corresponding to it. This functions returns a 1 to indicate that the link status has changed for the PHY provided and 0 otherwise.

Arguments

*      index              The PHY selector (0-1) for which the link status change
*                          bit must be read. Phy selector value 0 corresponds to the
*                          PHY address programmed in USERPHYSEL0 register and a Phy
*                          selector value 1 corresponds to the PHY address in
*                          USERPHYSEL1 register.
*   

Return Value uint32_t

Pre Condition
None

Post Condition
None

Reads
MDIO_ALIVE_REG

Example

*      uint32_t      index = 0;

       if (CSL_MDIO_isUnmaskedLinkStatusChangeIntSet (index))
       {
           // Link status has changed
       }
       else
       {
           // Link status has not changed
       }
       }

◆ CSL_MDIO_clearUnmaskedLinkStatusChangeInt()

void CSL_MDIO_clearUnmaskedLinkStatusChangeInt ( CSL_mdioHandle  hMdioRegs,
uint32_t  index 
)

============================================================================
CSL_MDIO_clearUnmaskedLinkStatusChangeInt

Description
For a given PHY selector(0-1) provided corresponding to the PHY address in USERPHYSEL register, this function clears the 'LINKINTRAW' register contents corresponding to it.

Arguments

*      index              The PHY selector (0-1) for which the link status change
*                          bit must be read. Phy selector value 0 corresponds to the
*                          PHY address programmed in USERPHYSEL0 register and a Phy
*                          selector value 1 corresponds to the PHY address in
*                          USERPHYSEL1 register.
*   

Return Value
None

Pre Condition
None

Post Condition
Clears the Link change interrupt.

Writes
MDIO_LINK_INT_RAW_REG

Example

*      uint32_t      index = 0;

       CSL_MDIO_clearUnmaskedLinkStatusChangeInt (index);

◆ CSL_MDIO_phyRegRead()

uint32_t CSL_MDIO_phyRegRead ( uint32_t  baseAddr,
uint32_t  phyAddr,
uint32_t  regNum,
uint16_t *  pData 
)

============================================================================
CSL_MDIO_phyRegRead

Parameters
baseAddrBase Address of the MDIO module.
phyAddrPHY Address.
regNumRegister Number to be read.
pDataPointer where the read value shall be written.
Return values
TRUERead is successful.
FALSERead is not acknowledged properly.

◆ CSL_MDIO_phyRegWrite()

void CSL_MDIO_phyRegWrite ( uint32_t  baseAddr,
uint32_t  phyAddr,
uint32_t  regNum,
uint16_t  wrVal 
)

This API writes a PHY register using MDIO.

============================================================================
CSL_MDIO_phyRegWrite

Parameters
baseAddrBase Address of the MDIO module.
phyAddrPHY Address.
regNumRegister Number to be written.
wrValValue to be written.

◆ CSL_MDIO_phyLinkStatus()

uint32_t CSL_MDIO_phyLinkStatus ( uint32_t  baseAddr,
uint32_t  phyAddr 
)

This API reads the link status of all PHY connected to this MDIO. The bit corresponding to the PHY address will be set if the PHY link is active.

============================================================================
CSL_MDIO_phyLinkStatus

Parameters
baseAddrBase Address of the MDIO module.
phyAddrPHY Address.
Returns
TRUE PHY link is active.
FALSE PHY link is inactive.

◆ CSL_MDIO_enableLinkStatusChangeInterrupt()

void CSL_MDIO_enableLinkStatusChangeInterrupt ( CSL_mdioHandle  hMdioRegs,
Uint32  index,
Uint32  phyAddr 
)

Enable MDIO link interrupt (MDIO_LINKINT) for PHY monitoring.

============================================================================
CSL_MDIO_enableLinkStatusChangeInterrupt

This function enables the MDIO link interrupt (MDIO_LINKINT). This function is applicable only when MDIO is operating in Normal Mode.

In Normal Mode, MDIO_LINKINT[0] event is set upon link change on the first PHY being monitored. MDIO_LINKINT[1] event is set upon link change on the second PHY being monitored.

Parameters
hMdioRegsHandle to MDIO module register overlay
indexUser group index (0 or 1)
phyAddrPHY address

◆ CSL_MDIO_disableLinkStatusChangeInterrupt()

void CSL_MDIO_disableLinkStatusChangeInterrupt ( CSL_mdioHandle  hMdioRegs,
Uint32  index,
Uint32  phyAddr 
)

Disable MDIO link interrupt (MDIO_LINKINT) for PHY monitoring.

============================================================================
CSL_MDIO_disableLinkStatusChangeInterrupt

This function disables the MDIO link interrupt (MDIO_LINKINT). This function is applicable only when MDIO is operating in Normal Mode.

Parameters
hMdioRegsHandle to MDIO module register overlay
indexUser group index (0 or 1)
phyAddrPHY address

◆ CSL_MDIO_enableFaultDetect()

void CSL_MDIO_enableFaultDetect ( CSL_mdioHandle  hMdioRegs)

============================================================================
CSL_MDIO_enableFaultDetect

Description
This function enables the Physical layer fault detection mechanism by setting 'FAULTENB' bit of the MDIO Control register to 1.

Arguments None

Return Value
None

Pre Condition
None

Post Condition
Enables PHY layer fault detection.

Writes
MDIO_CONTROL_REG_FAULT_DETECT_ENABLE=1

Example

*
       // Enable Phy Layer fault detection
       CSL_MDIO_enableFaultDetect ();

◆ CSL_MDIO_disableFaultDetect()

void CSL_MDIO_disableFaultDetect ( CSL_mdioHandle  hMdioRegs)

============================================================================
CSL_MDIO_disableFaultDetect

Description
This function disables the Physical layer fault detection mechanism by setting 'FAULTENB' bit of the MDIO Control register to 0.

Arguments None

Return Value
None

Pre Condition
None

Post Condition
Disables PHY layer fault detection.

Writes
MDIO_CONTROL_REG_FAULT_DETECT_ENABLE=0

Example

*
       // Disable Phy Layer fault detection
       CSL_MDIO_disableFaultDetect ();

◆ CSL_MDIO_enablePreamble()

void CSL_MDIO_enablePreamble ( CSL_mdioHandle  hMdioRegs)

============================================================================
CSL_MDIO_enablePreamble

Description
This function enables the MDIO preamble.

Arguments None

Return Value
None

Pre Condition
None

Post Condition
Enables MDIO Preamble frames.

Writes
MDIO_CONTROL_REG_PREAMBLE=0

Example

*
       // Enable MDIO preamble frames
       CSL_MDIO_enablePreamble ();

◆ CSL_MDIO_disablePreamble()

void CSL_MDIO_disablePreamble ( CSL_mdioHandle  hMdioRegs)

============================================================================
CSL_MDIO_disablePreamble

Description
This function disables the MDIO preamble.

Arguments None

Return Value
None

Pre Condition
None

Post Condition
Disables MDIO Preamble frames.

Writes
MDIO_CONTROL_REG_PREAMBLE=1

Example

*
       // Disable MDIO preamble frames
       CSL_MDIO_disablePreamble ();

◆ CSL_MDIO_phyRegRead2()

uint32_t CSL_MDIO_phyRegRead2 ( CSL_mdioHandle  hMdioRegs,
uint32_t  userGroup,
uint32_t  phyAddr,
uint32_t  regNum,
uint16_t *  pData 
)

============================================================================
CSL_MDIO_phyRegRead2

Parameters
hMdioRegsHandle to MDIO module register overlay.
userGroupUser group to use
phyAddrPHY Address.
regNumRegister Number to be read.
pDataPointer where the read value shall be written.
Returns
TRUE Read is successful.
FALSE Read is not acknowledged properly.

◆ CSL_MDIO_phyRegWrite2()

void CSL_MDIO_phyRegWrite2 ( CSL_mdioHandle  hMdioRegs,
uint32_t  userGroup,
uint32_t  phyAddr,
uint32_t  regNum,
uint16_t  wrVal 
)

This API writes a PHY register using MDIO.

============================================================================
CSL_MDIO_phyRegWrite2

Parameters
hMdioRegsHandle to MDIO module register overlay.
userGroupUser group to use
phyAddrPHY Address.
regNumRegister Number to be written.
wrValValue to be written.

◆ CSL_MDIO_phyLinkStatus2()

uint32_t CSL_MDIO_phyLinkStatus2 ( CSL_mdioHandle  hMdioRegs,
uint32_t  phyAddr 
)

This API reads the link status of all PHY connected to this MDIO. The bit corresponding to the PHY address will be set if the PHY link is active.

============================================================================
CSL_MDIO_phyLinkStatus2

Parameters
hMdioRegsBase Address of the MDIO module.
phyAddrPHY Address.
Returns
TRUE PHY link is active.
FALSE PHY link is inactive.

◆ CSL_MDIO_isStatusChangeModeInterruptEnabled()

uint32_t CSL_MDIO_isStatusChangeModeInterruptEnabled ( CSL_mdioHandle  hMdioRegs)

Check if the MDIO link interrupt (MDIO_LINKINT) is enabled.

============================================================================
CSL_MDIO_isStatusChangeModeInterruptEnabled

This function checks if the MDIO link interrupt (MDIO_LINKINT) is enabled or not. This function is applicable only when MDIO is operating in State Change Mode.

Parameters
hMdioRegsHandle to MDIO module register overlay
Returns
1 if MDIO link interrupt is enabled 0 if MDIO link interrupt is disabled

◆ CSL_MDIO_enableStatusChangeModeInterrupt()

void CSL_MDIO_enableStatusChangeModeInterrupt ( CSL_mdioHandle  hMdioRegs)

Enable MDIO link interrupt (MDIO_LINKINT)

============================================================================
CSL_MDIO_enableStatusChangeModeInterrupt

This function enables the MDIO link interrupt (MDIO_LINKINT). This function is applicable only when MDIO is operating in State Change Mode.

In State Change Mode, MDIO_LINKINT[0] is set when any bit in the ALIVE or LINK registers is set. MDIO_LINKINT[1] is not used.

Parameters
hMdioRegsHandle to MDIO module register overlay

◆ CSL_MDIO_disableStatusChangeModeInterrupt()

void CSL_MDIO_disableStatusChangeModeInterrupt ( CSL_mdioHandle  hMdioRegs)

Disable MDIO link interrupt (MDIO_LINKINT)

============================================================================
CSL_MDIO_disableLinkStatusChangeInterrupt

This function disables the MDIO link interrupt (MDIO_LINKINT). This function is applicable only when MDIO is operating in State Change Mode.

Parameters
hMdioRegsHandle to MDIO module register overlay

◆ CSL_MDIO_getLinkStatusChangePhyAddr()

Uint32 CSL_MDIO_getLinkStatusChangePhyAddr ( CSL_mdioHandle  hMdioRegs,
Uint32  index 
)

Get the PHY address being monitored.

============================================================================
CSL_MDIO_getLinkStatusChangePhyAddr

This function gets the address of the PHY whose state change is being monitored. This function is applicable only when MDIO is operating in Normal Mode.

Parameters
hMdioRegsHandle to MDIO module register overlay
indexUser group index (0 or 1)
Returns
PHY address

◆ CSL_MDIO_phyRegInitiateWrite()

int32_t CSL_MDIO_phyRegInitiateWrite ( CSL_mdioHandle  hMdioRegs,
uint32_t  userGroup,
uint32_t  phyAddr,
uint32_t  regNum,
uint16_t  wrVal 
)

This API inititates a write to PHY register using MDIO.

============================================================================
CSL_MDIO_phyRegInitiateWrite

Unlike CSL_MDIO_phyRegWrite this API does not wait for command completion Also this function will return error if previous phy command is active

Parameters
hMdioRegsHandle to MDIO module register overlay
userGroupUser group to use
phyAddrPHY Address.
regNumRegister Number to be written.
wrValValue to be written.
Returns
CSL_PASS on SUCCESS CSL_EFAIL if PHY GO bit is not cleared

◆ CSL_MDIO_isStateChangeModeEnabled()

uint32_t CSL_MDIO_isStateChangeModeEnabled ( CSL_mdioHandle  hMdioRegs)

Checks if the State Change Mode is enabled or not.

============================================================================
CSL_MDIO_isStateChangeModeEnabled

This function checks if the State Change Mode is enabled as per STATECHANGEMODE bit of the MDIO Poll register. It returns 1 to indicate that State Change Mode is enabled, or 0 to indicate that Normal Mode is enabled.

Parameters
hMdioRegsHandle to MDIO module register overlay
Returns
1 if State Change Mode is enabled 0 if Normal Mode is enabled

◆ CSL_MDIO_enableStateChangeMode()

void CSL_MDIO_enableStateChangeMode ( CSL_mdioHandle  hMdioRegs)

This function enables the MDIO State Change Mode.

============================================================================
CSL_MDIO_enableStateChangeMode

This function enables the State Change Mode which is used to detect change events on any PHY: MDIO_LINKINT[0] when any bit in MDIOAlive or MDIOLink registers is set MDIO_LINKINT[1] is not used MDIO_UserPhySel0/1 registers are not used

Parameters
hMdioRegsHandle to MDIO module register overlay

◆ CSL_MDIO_disableStateChangeMode()

void CSL_MDIO_disableStateChangeMode ( CSL_mdioHandle  hMdioRegs)

This function disables the MDIO State Change Mode.

============================================================================
CSL_MDIO_disableStateChangeMode

This function disabled the State Change Mode, effectively enabling Normal Mode which can be used to monitor only two PHYs.

Parameters
hMdioRegsHandle to MDIO module register overlay

◆ CSL_MDIO_setPollIPG()

void CSL_MDIO_setPollIPG ( CSL_mdioHandle  hMdioRegs,
uint8_t  ipgVal 
)

Set Polling Inter Packet Gap value.

============================================================================
CSL_MDIO_setPollIPG

This function sets the polling Inter Packet Gap (IPG) value which is the number of MDCLK_O clocks between each poll when polling is enabled.

Parameters
hMdioRegsHandle to MDIO module register overlay
ipgValIPG value (in MDCLK_O clock pulses)

◆ CSL_MDIO_getPollIPG()

uint8_t CSL_MDIO_getPollIPG ( CSL_mdioHandle  hMdioRegs)

Get Polling Inter Packet Gap value.

============================================================================
CSL_MDIO_getPollIPG

This function gets the polling Inter Packet Gap (IPG) value which is the number of MDCLK_O clocks between each poll when polling is enabled.

Parameters
hMdioRegsHandle to MDIO module register overlay
Returns
IPG value (in MDCLK_O clock pulses)

◆ CSL_MDIO_setPollEnableMask()

void CSL_MDIO_setPollEnableMask ( CSL_mdioHandle  hMdioRegs,
uint32_t  pollEnableMask 
)

Set poll enable mask.

============================================================================
CSL_MDIO_setPollEnableMask

This function sets the poll enable mask. When set, each bit of the mask indicates that the associated PHY will be included in the polling operations.

Due to a hardware limitation, bit 31 is always set internally by this function.

Parameters
hMdioRegsHandle to MDIO module register overlay
pollEnableMaskPoll enable mask

◆ CSL_MDIO_getPollEnableMask()

uint32_t CSL_MDIO_getPollEnableMask ( CSL_mdioHandle  hMdioRegs)

Get poll enable mask.

============================================================================
CSL_MDIO_getPollEnableMask

This function gets the poll enable mask. When set, each bit of the mask indicates that the associated PHY will be included in the polling operations.

Parameters
hMdioRegsHandle to MDIO module register overlay
Returns
Poll enable mask