![]() |
PDK Documentation
|
This header file contains function prototypes which interface interactively with the user through the serial console to perform some utility operations.
Go to the source code of this file.
Macros | |
| #define | E_PASS ((int32_t)(0)) |
| #define | E_FAIL (-((int32_t)1)) |
| #define | S_PASS (0) |
Functions | |
| uint32_t | UART_puts (const char *pTxBuffer, int32_t numBytesToWrite) |
| This function writes data from a specified buffer onto the transmitter FIFO of UART. More... | |
| uint32_t | UART_gets (char *pRxBuffer, int32_t numBytesToRead) |
| This function reads data from the receiver FIFO to a buffer in the receiver. More... | |
| int32_t | UART_dataWrite (const char *pcBuf, uint32_t ulLen) |
| void | UART_printf (const char *pcString,...) |
| void | UART_putc (uint8_t byteTx) |
| uint8_t | UART_getc (void) |
| void | UART_stdioInit2 (uint32_t instance, UART_Params *uartParams) |
| This function initializes the specified UART instance for use for console operations , with a configuration specified by 'uartParams'. More... | |
| void | UART_stdioInit (uint32_t value) |
| This function initializes the specified UART instance for use for console operations. More... | |
| int32_t | UART_scanFmt (const char *pString,...) |
| This function shall read the formatted input from UART console. Format specifier follows %[fill][width]specifier Following formatting specifier are supported. More... | |
| void | UART_stdioDeInit (void) |
| This function de-initializes the UART instance that is opened for console operations. More... | |
| void | UART_printStatus (const char *statusString) |
| This function prints the status on the UART instance that is opened for console operations. More... | |
| #define E_PASS ((int32_t)(0)) |
| #define E_FAIL (-((int32_t)1)) |
| #define S_PASS (0) |
| uint32_t UART_puts | ( | const char * | pTxBuffer, |
| int32_t | numBytesToWrite | ||
| ) |
This function writes data from a specified buffer onto the transmitter FIFO of UART.
| pTxBuffer | Pointer to a buffer in the transmitter. |
| numBytesToWrite | Number of bytes to be transmitted to the transmitter FIFO. The user has the freedom to not specify any valid value for this if he wants to print until the occurence of a NULL character. In this case, he has to pass a negative value as this parameter. |
| uint32_t UART_gets | ( | char * | pRxBuffer, |
| int32_t | numBytesToRead | ||
| ) |
This function reads data from the receiver FIFO to a buffer in the receiver.
| pRxBuffer | Pointer to a buffer in the receiver. |
| numBytesToRead | The number of bytes the receiver buffer can hold. However, if the user wishes not to specify this parameter, he has freedom to do so. In that case, the user has to pass a negative value for this parameter. |
UARTGets(rxBuffer, -2): This reads characters from the receiver FIFO of UART until the occurence of a carriage return ('Enter' key on the keyboard pressed) or an ESC character.
UARTGets(rxBuffer, 12): This reads characters until 12 characters have been read or until an occurence of a carriage return or an ESC character, whichever occurs first.
| int32_t UART_dataWrite | ( | const char * | pcBuf, |
| uint32_t | ulLen | ||
| ) |
Writes a string of characters to the UART output.
| pcBuf | points to a buffer containing the string to transmit. |
| ulLen | is the length of the string to transmit. |
This function will transmit the string to the UART output. The number of characters transmitted is determined by the ulLen parameter. This function does no interpretation or translation of any characters. Since the output is sent to a UART, any LF (/n) characters encountered will be replaced with a CRLF pair.
Besides using the ulLen parameter to stop transmitting the string, if a null character (0) is encountered, then no more characters will be transmitted and the function will return.
In non-buffered mode, this function is blocking and will not return until all the characters have been written to the output FIFO. In buffered mode, the characters are written to the UART transmit buffer and the call returns immediately. If insufficient space remains in the transmit buffer, additional characters are discarded.
| void UART_printf | ( | const char * | pcString, |
| ... | |||
| ) |
A simple UART based printf function supporting %c, %d, %p, %s, %u, %x, and %X.
| pcString | is the format string. |
| ... | are the optional arguments, which depend on the contents of the format string. |
This function is very similar to the C library fprintf() function. All of its output will be sent to the UART. Only the following formatting characters are supported:
For %s, %d, %u, %p, %x, and %X, an optional number may reside between the % and the format character, which specifies the minimum number of characters to use for that value; if preceded by a 0 then the extra characters will be filled with zeros instead of spaces. For example, \%8d'' will use eight characters to print the decimal value with spaces added to reach eight;%08d'' will use eight characters as well but will add zeroes instead of spaces.
The type of the arguments after pcString must match the requirements of the format string. For example, if an integer was passed where a string was expected, an error of some kind will most likely occur.
| void UART_putc | ( | uint8_t | byteTx | ) |
| uint8_t UART_getc | ( | void | ) |
| void UART_stdioInit2 | ( | uint32_t | instance, |
| UART_Params * | uartParams | ||
| ) |
This function initializes the specified UART instance for use for console operations , with a configuration specified by 'uartParams'.
| instance | - uart instance ID. |
| uartParams | - Configuration parameters. |
| void UART_stdioInit | ( | uint32_t | value | ) |
This function initializes the specified UART instance for use for console operations.
| value | - the UART instance number |
| int32_t UART_scanFmt | ( | const char * | pString, |
| ... | |||
| ) |
This function shall read the formatted input from UART console. Format specifier follows %[fill][width]specifier Following formatting specifier are supported.
| pString | Pointer to the format string. |
| S_PASS | Sucessfully executed. |
| E_FAIL | If an error occurred. |
| void UART_stdioDeInit | ( | void | ) |
This function de-initializes the UART instance that is opened for console operations.
| void UART_printStatus | ( | const char * | statusString | ) |
This function prints the status on the UART instance that is opened for console operations.
| statusString | - string pointer. |