PDK Documentation
CacheP.h File Reference

Introduction

Cache Handling routines for the RTOS Porting Interface.

============================================================================


Go to the source code of this file.

Functions

void CacheP_wb (const void *addr, int32_t size)
 Function to write back cache lines. More...
 
void CacheP_Inv (const void *addr, int32_t size)
 Function to invalidate cache lines. More...
 
void CacheP_wbInv (const void *addr, int32_t size)
 Function to write back and invalidate cache lines. More...