This section contains APIs to use GStreamer CODEC Pipelines within demos.
◆ appGstInit()
Launches the GstPipeline described by user defined parameters. Initializes the gst_wrapper and calls gst_parse_launch() on the command string.
- Parameters
-
◆ appGstSrcInit()
| int32_t appGstSrcInit |
( |
void * |
data_ptr[CODEC_MAX_BUFFER_DEPTH][CODEC_MAX_NUM_CHANNELS][CODEC_MAX_NUM_PLANES] | ) |
|
Initializes the AppSrc elements to be able to push buffers to the GstPipeline. Wraps the given allocated memory as GstBuffers to push. The input parameters (in_*) must be properly initialised.
- Parameters
-
| [in] | data_ptr | memory that the GstBuffers will map to |
◆ appGstSinkInit()
| int32_t appGstSinkInit |
( |
void *(*) |
data_ptr[CODEC_MAX_NUM_CHANNELS][CODEC_MAX_NUM_PLANES] | ) |
|
Initializes the AppSink elements to be able to pull buffers from the GstPipeline. Registers the data_pointers that will map to the bufferpool of pulled GstBuffers. The output parameters (out_*) must be properly initialised.
- Parameters
-
| [in] | data_ptr | pointers to hold the pulled buffers |
◆ appGstStart()
Starts the GstPipeline that was launched previously.
◆ appGstEnqAppSrc()
| int32_t appGstEnqAppSrc |
( |
uint8_t |
idx | ) |
|
Push a buffer from the bufferpool to the AppSrc element.
- Parameters
-
| [in] | idx | the buffer id, from the bufferpool, to be pushed to the GstPipeline |
◆ appGstDeqAppSrc()
| int32_t appGstDeqAppSrc |
( |
uint8_t |
idx | ) |
|
Wait for a previously pushed buffer to be consumed by the GstPipeline.
- Parameters
-
| [in] | idx | the buffer id, from the bufferpool, to wait on |
◆ appGstEnqEosAppSrc()
| int32_t appGstEnqEosAppSrc |
( |
| ) |
|
Push EOS (End Of Stream) to the AppSrc element. Signals the elements to stop processing buffers after this.
◆ appGstDeqAppSink()
| int32_t appGstDeqAppSink |
( |
uint8_t |
idx | ) |
|
Pull a buffer from the AppSink element into the bufferpool.
- Parameters
-
| [in] | idx | the slot into which the pulled data is stored
in the pulled_data_ptr array, while maintaining a reference to the pulled GstBuffer |
◆ appGstEnqAppSink()
| int32_t appGstEnqAppSink |
( |
uint8_t |
idx | ) |
|
Release a previously pulled GstBuffer back to GStreamer and cleanup.
- Parameters
-
| [in] | idx | the slot from which the buffer is released back to Gstreamer. The data pointer for this slot is no longer valid |
◆ appGstStop()
Stops the GstPipeline that was in playing state. If there is no AppSink element, waits to recieve EOS before cleaning up.
◆ appGstDeInit()
Unmaps all buffers that were mapped and destroys all GStreamer objects.
◆ appGstPrintStats()
| void appGstPrintStats |
( |
| ) |
|
Prints the current count of the numbers of buffers pushed/pulled to/from the GstPipeline. Not multi-thread safe.