4.12. Release notes - 08_04_03 (Snapshot drop)¶
4.12.1. Features¶
Note
New features vs previous release are marked in bold
Important
This is a snapshop drop intended to give intra-release snapshot update. As such, only sanity testing was done and not all components have gotten updates from 8.2.2 release. Full testing will only come as part of 8.5.0 release.
Note
Major updates in this snapshot release are as follows:
Several bug fixes across components (especially tiovx, vision_apps and pdk), please refer to individual SDK Components release notes.
Bug fix for apps which use multi-channel camera (4 or more cameras) along with LDC
MCAL component updates
4.12.1.1. Hardware support¶
J784S4 E1 EVM support
J784S4 ES1.0 support
Fusion1 RevC daughter card with UB960 FPDLink deserializer
IMX390 2MP CSI2 image sensor + UB953 FPDLink serializer
Quad Port Ethernet daughter card (for CPSW9G support)
4.12.1.2. Software features¶
Important
Below is a summary of key features. Refer individual SDK Components release notes for more details
4.12.1.2.1. Vision Apps (ADAS, Vision, DL demos)¶
OpenVX based demos for ADAS, Vision, deep learning applications
FreeRTOS on C7x, R5F and Linux/QNX on A72
Integrates all major PSDK RTOS and PSDK LINUX SW components like TIDL, MMALIB, PDK, OpenVX, ETHFW, OpenGL, C7x algorithms, imaging/sensors, IPC, Linux, FreeRTOS, SPL/uboot.
Integrates all major HW components like CSI2 camera, eDP display, UART, I2C, ethernet, SD card
Deep Learning demos
Image Classification demo
File based
Camera based
Standalone Semantic Segmentation application
File based
Camera based
Standalone Object Detection application
File based
Camera based
Auto valet parking (AVP) demo
semantic segmentation, Parking spot detect and Vehicle detect algorithms
1 channel, 3 algo mode (AVP1 demo)
3 channel, 3 algo mode - combined network for parking spot and vehicle detect (AVP2 demo)
3 channel, 5 algo mode - combined network for parking spot and vehicle detect + Three task network for Semantic Segmentation, Motion Segmentation and Depth Estimation (AVP3 demo)
DKAZE-based Visual Localization application
Debug support for the ability to debug intermediate layer information from TIDL node
Surround view demos
3D surround view using GPU on 4x 2MP 30fps live camera input
3D surround view calibration application
ADAS/Vision demos
Dense optical flow (DOF) demo
Stereo disparity engine demo
Single and multi camera to display (CSI2RX + VISS + LDC + MSC + Display) demo
OpenVX target nodes
image pre-processing (YUV 2 RGB) nodes for DL demos
image post-processing and visualization nodes for deep learning, DOF, Stereo demos
OpenGL nodes for surround view
Profiling, logging and other utility APIs
All included MCU tasks are split between MCU2_0 (ETHFW, VPAC0 HWA), MCU2_1 (DMPAC HWA), and MCU4_0 (VPAC1), leaving MCU3_0, MCU3_1, and MCU4_1 free on main domain
4.12.1.2.2. Platform Development Kit (PDK)¶
RTOS device drivers running on R5F, C7x
Supported drivers and modules
ENET CPSW (2G & 9G in Main domain, 2G in MCU domain), RGMII, lwIP
CSL-FL (Chip support library)
GPIO
I2C
IPC (inter processor communication)
MMCSD with FATFS
OSAL
SBL secondary bootloader
SCI Client (DMSC interface)
SPI driver (SPI, OSPI, NAND)
UART
UDMA and DRU
DSS display (eDP)
2xCSI2-RX camera (4 cameras per instance)
2xCSI2-TX
2xVPAC and DMAC (VHWA)
FreeRTOS Support on R5, DSPs
Refer to PDK release notes LINK for more details.
4.12.1.2.3. MCU Software (MCUSW)¶
AutoSAR 4.3.1 MCAL driver and MCU1_0 example applications running on R5F (TI Arm Clang Compiler).
AutoSAR MCAL driver for Adc, Can, Dio, Eth, Pwm & Wdg
4.12.1.2.4. TI Deep learning Product (TIDL) and MMALIB¶
TIDL deep learning inference engine library running on C7x/MMA
MMALIB for accelerating convolution, deconvolution layers on MMA (used by TIDL internally)
Supports Caffe, ONXX, TFlite network exchange formats
Supported layers: Convolution, deconvolution, pooling, ReLU, Elt-wise, Inner product, Soft-max, and many more, refer TIDL user guide (LINK)
Support for Additional layers - Sigmoid layer, Standalone Pad layer, Color conversion (YUV420SP to RGB) Layer, Depth to Space (Pixel Shuffle) Layer
Custom / User defined layer Call-back to plugin user specific layers
TIDL network import tool and graph visualizer tool
Post Training Quantization options for 8-bit, 16-bit and mixed precision inference
Support of batch processing
Support for auto C7x code generation with TVM
4.12.1.2.5. FFT Library for C7x/MMA (FFTLIB)¶
C7x-only kernels
C7x+MMA kernels
Note: This is packaged as a stand-alone library component, and is not integrated into any SDK level demos
4.12.1.2.6. TI OpenVX (TIOVX)¶
OpenVX v1.1 compliant implementation with graph pipelining and user data object extension support
OpenVX API on A72 running Linux/QNX
OpenVX target kernels on C7x, R5F, A72
OpenVX v1.1 C6x optimized kernels recompiled for C7x
OpenVX nodes for
TIDL (C7x-MMA)
VISS (R5F)
LDC (R5F)
MSC (multi-scalar) (R5F)
Pyramid (using MSC) (R5F)
Dense Optical Flow (R5F)
Stereo Disparity Engine (R5F)
BLNF (bilateral noise filter) (R5F)
CSI2-RX camera (R5F)
CSI2-TX (R5F)
Display (eDP) (R5F)
OpenVX tutorials for getting started
PyTIOVX tools for target kernel code generation
Performance Analyzer tool for run time logging of OpenVX graphs
VISS node supports heterogeneous cameras
4.12.1.2.7. Imaging¶
IMX390 2MP sensor driver (30/60fps) with IQ tuning
TI Auto-exposure and auto white-balance algorithms
Support for UB960 broadcast mode
Sensor framework supports heterogeneous cameras
4.12.1.2.8. Ethernet Switch Firmware (ETHFW)¶
Ethernet firmware interface API
Ethernet switch firmware running on R5F for CPSW9G
Layer 2 switching
FreeRTOS for Main R5F Core 0
lwIP TCP/IP stack integration
Remote switch configuration server
GUI switch configuration tool
Inter-VLAN routing
IP next header filtering
CPSW Proxy/Server layer for remote core integration
Integration with AUTOSAR Eth Virtual MAC driver
PTP support
MAC-only mode support
Shared memory based virtual Ethernet adapter
Multi-core broadcast/multicast traffic using software fan-out
4.12.1.2.9. TI Autonomous Driving Algorithms (TIADALG)¶
Image pre-processing APIs for color plane conversion and separation YUV to RGB for DL applications (C6x optimized. recompiled for C7x)
Camera Pose estimation API using solve pnp technique (C6x optimized. recompiled for C7x)
Visual localization algorithm (C6x optimized. recompiled for C7x)
Structure from Motion algorithm
4.12.1.2.10. FreeRTOS¶
FreeRTOS for R5F and C7x
lwIP TCP/IP stack integration for R5F
4.12.1.2.11. Code Gen Tools (CGT)¶
TI Compiler, assembler, linker for R5F, C7x
TI LLVM (CLANG) Compiler, assembler, linker for R5F
GCC compiler for A72 (needs to be downloaded separately)
4.12.2. Device Support and Validation Information¶
SoC |
Build Host (OS) |
Run Target (OS) |
Test Plaform |
|---|---|---|---|
J784S4 |
x86_64 (Linux Ubuntu 18.04) |
R5F, C7x running FreeRTOS A72 running Linux or QNX |
J784S4 EVM with daughter cards |
PC emulation mode (1) |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
(1) Requires download of addon package from mySecure Software
4.12.3. Upgrade and Compatibility¶
In this section, we only highlight a few significant changes in this SDK. For full list of upgrade and compatibility topics, please refer to individual components release notes SDK Components.
4.12.4. Known Issues¶
Record ID |
Summary |
Workaround |
Impact |
|---|---|---|---|
ADASVISION-5064 |
OCMC RAM init failure on MCU2-0 |
Init is disabled and memory previously mapped here is instead mapped to DDR |
Reduced performance of memory previously accessed from this region. In SDK this was only used by heterogeneous camera context save/restore |
Refer to individual SDK Components release notes for known issues in each component
4.12.6. Additional Reports¶
Test reports, traceability matrix not available in this snapshot drop.