Vision Apps User Guide
App_M2mSdeSl2AllocPrms Struct Reference

Detailed Description

Init Parameters required to allocate SDE driver. This should be identical to Vhwa_m2mSdeSl2AllocPrms. It is defined locally for application to use the same params.

struct App_m2mSdeSl2AllocPrms

Data Fields

uint32_t maxImgWidth
 
uint32_t inCcsf
 
uint32_t searchRange
 
uint32_t disBuffDepth
 

Field Documentation

◆ maxImgWidth

uint32_t App_M2mSdeSl2AllocPrms::maxImgWidth

These parameters are used by the driver to allocater SL2 memory, used all driver handles. Ensure to allocate max of all handles requirement.Maximun image width

◆ inCcsf

uint32_t App_M2mSdeSl2AllocPrms::inCcsf

CCSF for input image

◆ searchRange

uint32_t App_M2mSdeSl2AllocPrms::searchRange

Search range refer to SDE_DispSearchRange

◆ disBuffDepth

uint32_t App_M2mSdeSl2AllocPrms::disBuffDepth

Maximum disparity buffer depth