TIOVX User Guide

Detailed Description

Enumerations for configuration output routing in VPAC VISS structures.

Defines

#define TIVX_VPAC_VISS_FCP1_DISABLED   (0U)
 
#define TIVX_VPAC_VISS_FCP1_INPUT_RFE   (1U)
 
#define TIVX_VPAC_VISS_FCP1_INPUT_CAC   (2U)
 
#define TIVX_VPAC_VISS_FCP1_INPUT_NSF4   (3U)
 
#define TIVX_VPAC_VISS_FCP1_INPUT_GLBCE   (4U)
 
#define TIVX_VPAC_VISS_FCP0   (0U)
 
#define TIVX_VPAC_VISS_FCP1   (1U)
 
#define TIVX_VPAC_VISS_FCP_OUT0   (0U)
 
#define TIVX_VPAC_VISS_FCP_OUT1   (0U)
 
#define TIVX_VPAC_VISS_FCP_OUT2   (1U)
 
#define TIVX_VPAC_VISS_FCP_OUT3   (1U)
 
#define TIVX_VPAC_VISS_FCP_OUT4   (0U)
 
#define TIVX_VPAC_VISS_MAP_FCP_OUTPUT(fcp, output)   (output<<1 | fcp)
 

Macro Definition Documentation

◆ TIVX_VPAC_VISS_FCP1_DISABLED

#define TIVX_VPAC_VISS_FCP1_DISABLED   (0U)
See also
tivx_vpac_viss_params_t::fcp1_config

Definition at line 92 of file hwa_vpac_viss3.h.

◆ TIVX_VPAC_VISS_FCP1_INPUT_RFE

#define TIVX_VPAC_VISS_FCP1_INPUT_RFE   (1U)
See also
tivx_vpac_viss_params_t::fcp1_config

Definition at line 94 of file hwa_vpac_viss3.h.

◆ TIVX_VPAC_VISS_FCP1_INPUT_CAC

#define TIVX_VPAC_VISS_FCP1_INPUT_CAC   (2U)
See also
tivx_vpac_viss_params_t::fcp1_config

Definition at line 96 of file hwa_vpac_viss3.h.

◆ TIVX_VPAC_VISS_FCP1_INPUT_NSF4

#define TIVX_VPAC_VISS_FCP1_INPUT_NSF4   (3U)
See also
tivx_vpac_viss_params_t::fcp1_config

Definition at line 98 of file hwa_vpac_viss3.h.

◆ TIVX_VPAC_VISS_FCP1_INPUT_GLBCE

#define TIVX_VPAC_VISS_FCP1_INPUT_GLBCE   (4U)
See also
tivx_vpac_viss_params_t::fcp1_config

Definition at line 100 of file hwa_vpac_viss3.h.

◆ TIVX_VPAC_VISS_FCP0

#define TIVX_VPAC_VISS_FCP0   (0U)

◆ TIVX_VPAC_VISS_FCP1

#define TIVX_VPAC_VISS_FCP1   (1U)

◆ TIVX_VPAC_VISS_FCP_OUT0

#define TIVX_VPAC_VISS_FCP_OUT0   (0U)

◆ TIVX_VPAC_VISS_FCP_OUT1

#define TIVX_VPAC_VISS_FCP_OUT1   (0U)

◆ TIVX_VPAC_VISS_FCP_OUT2

#define TIVX_VPAC_VISS_FCP_OUT2   (1U)

◆ TIVX_VPAC_VISS_FCP_OUT3

#define TIVX_VPAC_VISS_FCP_OUT3   (1U)

◆ TIVX_VPAC_VISS_FCP_OUT4

#define TIVX_VPAC_VISS_FCP_OUT4   (0U)

◆ TIVX_VPAC_VISS_MAP_FCP_OUTPUT

#define TIVX_VPAC_VISS_MAP_FCP_OUTPUT (   fcp,
  output 
)    (output<<1 | fcp)

Macro to set the output_fcp_mapping

See also
tivx_vpac_viss_params_t::output_fcp_mapping

Definition at line 120 of file hwa_vpac_viss3.h.