TIOVX User Guide

Detailed Description

Enumerations for configuration parameters in VPAC VISS structures.

Defines

#define TIVX_VPAC_VISS_H3A_IN_RAW0   (0U)
 
#define TIVX_VPAC_VISS_H3A_IN_RAW1   (1U)
 
#define TIVX_VPAC_VISS_H3A_IN_RAW2   (2U)
 
#define TIVX_VPAC_VISS_H3A_IN_LSC   (3U)
 
#define TIVX_VPAC_VISS_H3A_MODE_AEWB   (0U)
 
#define TIVX_VPAC_VISS_H3A_MODE_AF   (1U)
 

Macro Definition Documentation

◆ TIVX_VPAC_VISS_H3A_IN_RAW0

#define TIVX_VPAC_VISS_H3A_IN_RAW0   (0U)

◆ TIVX_VPAC_VISS_H3A_IN_RAW1

#define TIVX_VPAC_VISS_H3A_IN_RAW1   (1U)

◆ TIVX_VPAC_VISS_H3A_IN_RAW2

#define TIVX_VPAC_VISS_H3A_IN_RAW2   (2U)

◆ TIVX_VPAC_VISS_H3A_IN_LSC

#define TIVX_VPAC_VISS_H3A_IN_LSC   (3U)

◆ TIVX_VPAC_VISS_H3A_MODE_AEWB

#define TIVX_VPAC_VISS_H3A_MODE_AEWB   (0U)
See also
tivx_vpac_viss_params_t::h3a_mode and tivx_h3a_data_t::aew_af_mode

Definition at line 179 of file hwa_vpac_viss.h.

◆ TIVX_VPAC_VISS_H3A_MODE_AF

#define TIVX_VPAC_VISS_H3A_MODE_AF   (1U)
See also
tivx_vpac_viss_params_t::h3a_mode and tivx_h3a_data_t::aew_af_mode

Definition at line 181 of file hwa_vpac_viss.h.