![]() |
TIOVX User Guide
|
APIs for application interface accessible only on host.
Modules | |
| Raw Image Data Type APIs | |
| APIs creating and using raw image data type. | |
| Super Node Framework Type APIs | |
| APIs creating and using super node framework type. | |
| Tensor Data Type APIs | |
| APIs creating and using tensor data type (note: this is not included in OpenVX 1.1 and thus added to TI extensions) | |
| Kernel Helper APIs | |
| Helper APIs used used for host side kernel validation. | |
| Utility APIs | |
| Utility APIs available for the application running on the host. | |
| Platform OSAL APIs | |
| Platform operating system abstraction layer on the host. | |
| Debug APIs | |
| APIs for debug operations on the host. | |
| Real-time Trace APIs | |
| APIs for real-time event trace operations on the host. | |
| Resource Logging APIs | |
| APIs for resource logging on the host. | |
Defines | |
| #define | TIVX_TARGET_MAX_NAME (64u) |
| Max possible name of a target. | |
| #define | TIVX_TARGET_HOST "HOST" |
| String to name a OpenVX Host. More... | |
| #define | TIVX_CONFIG_PATH_LENGTH (512u) |
| Max size of config file path. | |
| #define | TIVX_CONTROL_CMD_SEND_TO_ALL_REPLICATED_NODES ((uint32_t)-1) |
| When sending a control command to a replicated node, this can be used to send control command to all replicated node. More... | |
| #define | dimof(x) (sizeof(x)/sizeof(x[0])) |
| Macro to find size of array. | |
Enumerations | |
| enum | tivx_graph_attribute_extensions_e { TIVX_GRAPH_STREAM_EXECUTIONS = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_GRAPH) + 0x0 } |
| TI attribute extensions for the graph object. More... | |
| enum | tivx_node_attribute_extensions_e { TIVX_NODE_TARGET_STRING = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_NODE) + 0x0, TIVX_NODE_TIMEOUT = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_NODE) + 0x1, TIVX_NODE_IS_TIMED_OUT = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_NODE) + 0x2 } |
| TI attribute extensions for the node object. More... | |
| enum | tivx_reference_attribute_extensions_e { TIVX_REFERENCE_TIMESTAMP = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_REFERENCE) + 0x0, TIVX_REFERENCE_INVALID = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_REFERENCE) + 0x1, TIVX_REFERENCE_BUFFER_IS_ALLOCATED = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_REFERENCE) + 0x2 } |
| TI attribute extensions for the reference object. More... | |
| enum | tivx_kernel_attribute_extensions_e { TIVX_KERNEL_TIMEOUT = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_KERNEL) + 0x0 } |
| TI attribute extensions for the kernel object. More... | |
| enum | tivx_context_attribute_extensions_e { TIVX_CONTEXT_NUM_USER_KERNEL_ID = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_CONTEXT) + 0x0, TIVX_CONTEXT_NUM_USER_LIBRARY_ID = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_CONTEXT) + 0x1 } |
| TI attribute extensions for the context object. More... | |
| enum | tivx_image_attribute_extensions_e { TIVX_IMAGE_IMAGEPATCH_ADDRESSING = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_IMAGE) + 0x0, TIVX_IMAGE_STRIDE_Y_ALIGNMENT = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_IMAGE) + 0x1 } |
| TI attribute extensions for the image object. More... | |
| enum | tivx_tensor_attribute_extensions_e { TIVX_TENSOR_STRIDES = VX_ATTRIBUTE_BASE(VX_ID_TI, (vx_enum)VX_TYPE_TENSOR) + 0x0 } |
| TI attribute extensions for the tensor object. More... | |
| enum | tivx_df_image_e { TIVX_DF_IMAGE_P12 = VX_DF_IMAGE('P','0','1','2'), TIVX_DF_IMAGE_NV12_P12 = VX_DF_IMAGE('N','1','2','P'), TIVX_DF_IMAGE_RGB565 = VX_DF_IMAGE('R','5','6','5'), TIVX_DF_IMAGE_BGRX = VX_DF_IMAGE('B','G','R','A') } |
| Based on the VX_DF_IMAGE definition. More... | |
| enum | tivx_status_e { TIVX_STATUS_BASE = -(vx_int32)100 } |
| The enumeration of all TIVX operational error codes. More... | |
| enum | tivx_cpu_id_e { TIVX_CPU_ID_DSP_C7_2 = 0, TIVX_CPU_ID_DSP_C7_1 = 1, TIVX_CPU_ID_DSP1 = TIVX_CPU_ID_DSP_C7_2, TIVX_CPU_ID_MCU2_0 = 2, TIVX_CPU_ID_VPAC1 = TIVX_CPU_ID_MCU2_0, TIVX_CPU_ID_VIDEO_IO = TIVX_CPU_ID_MCU2_0, TIVX_CPU_ID_MCU2_1 = 3, TIVX_CPU_ID_DMPAC = TIVX_CPU_ID_MCU2_1, TIVX_CPU_ID_MPU_0 = 4, TIVX_CPU_ID_MCU3_0 = 5, TIVX_CPU_ID_MCU3_1 = 6, TIVX_CPU_ID_MCU4_0 = 7, TIVX_CPU_ID_VPAC2 = TIVX_CPU_ID_MCU4_0, TIVX_CPU_ID_MCU4_1 = 8, TIVX_CPU_ID_DSP_C7_3 = 9, TIVX_CPU_ID_DSP_C7_4 = 10, TIVX_CPU_ID_MAX = 11, TIVX_CPU_ID_INVALID = 0xFF } |
| CPU ID for supported CPUs. More... | |
Functions | |
| void | tivxInit (void) |
| Function to initialize OpenVX framework. More... | |
| void | tivxDeInit (void) |
| Function to de-initialize OpenVX framework. More... | |
| void | tivxHostInit (void) |
| Function to initialize OpenVX HOST side functionality. More... | |
| void | tivxHostDeInit (void) |
| Function to de-initialize OpenVX HOST side functionality. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxAddKernelTarget (vx_kernel kernel, const char *target_name) |
| Associate a target with a kernel. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxSetKernelSinkDepth (vx_kernel kernel, uint32_t num_sink_bufs) |
| Set the number of sink buffers. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxRegisterModule (const char *name, vx_publish_kernels_f publish, vx_unpublish_kernels_f unpublish) |
| Register publish and unpublish functions against a module name. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxUnRegisterModule (const char *name) |
| UnRegister publish and unpublish functions if previously registered. More... | |
| vx_enum | tivxGetSelfCpuId (void) |
| Return CPU ID of the CPU on which this API is called. More... | |
| vx_node | tivxCreateNodeByKernelEnum (vx_graph graph, vx_enum kernelenum, vx_reference params[], vx_uint32 num) |
| Utility function to create a node given parameter references and kernel enum. More... | |
| vx_node | tivxCreateNodeByKernelRef (vx_graph graph, vx_kernel kernel, vx_reference params[], vx_uint32 num) |
| Utility function to create a node given parameter references and kernel reference. More... | |
| vx_node | tivxCreateNodeByKernelName (vx_graph graph, const char *kernel_name, vx_reference params[], vx_uint32 num) |
| Utility function to create a node given parameter references and kernel name. More... | |
| vx_bool | tivxIsReferenceVirtual (vx_reference ref) |
| Utility function to check if the given reference is virtual or not. More... | |
| vx_reference | tivxGetReferenceParent (vx_reference child_ref) |
| Utility function to extract the parent reference from an element. More... | |
| vx_bool | tivxIsTargetEnabled (const char target_name[]) |
| Utility function to know if target is enabled or not. More... | |
| uint64_t | tivxPlatformGetTimeInUsecs (void) |
| Get the time in micro seconds. More... | |
| vx_status VX_API_CALL | tivxSetNodeParameterNumBufByIndex (vx_node node, vx_uint32 idx, vx_uint32 num_buf) |
| Set number of buffers to allocate at output of a node parameter. More... | |
| vx_status VX_API_CALL | tivxGetNodeParameterNumBufByIndex (vx_node node, vx_uint32 idx, vx_uint32 *num_buf) |
| Get number of buffers to allocate at output of a node parameter. More... | |
| vx_status VX_API_CALL | tivxSetGraphPipelineDepth (vx_graph graph, vx_uint32 pipeline_depth) |
| Indicates to the implementation the depth of the graph pipeline. More... | |
| vx_status VX_API_CALL | tivxNodeSendCommand (vx_node node, uint32_t replicate_nodex_idx, uint32_t node_cmd_id, vx_reference ref[], uint32_t num_refs) |
| Send node specific Control command. More... | |
| vx_status VX_API_CALL | tivxNodeSendCommandTimed (vx_node node, uint32_t replicate_nodex_idx, uint32_t node_cmd_id, vx_reference ref[], uint32_t num_refs, uint32_t timeout) |
| Send node specific Control command. More... | |
| vx_node | tivxGraphGetNode (vx_graph graph, uint32_t idx) |
| This API is used to get a reference to a node within a graph at a given index within the graph. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxSetNodeTileSize (vx_node node, vx_uint32 block_width, vx_uint32 block_height) |
| Sets the tile size for a given node in a graph. This is only valid for BAM-enabled kernels on C66 DSP. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxSetReferenceAttribute (vx_reference ref, vx_enum attribute, const void *ptr, vx_size size) |
| Sets reference attributes for the below enums: TIVX_REFERENCE_TIMESTAMP. More... | |
| VX_API_ENTRY vx_bool VX_API_CALL | tivxIsReferenceMetaFormatEqual (vx_reference ref1, vx_reference ref2) |
| Check for equivalence between the meta formats of two reference objects. More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxReferenceImportHandle (vx_reference ref, const void *addr[], const uint32_t size[], uint32_t num_entries) |
| Updates a reference object with the supplied handles (pointers to memory). More... | |
| VX_API_ENTRY vx_status VX_API_CALL | tivxReferenceExportHandle (const vx_reference ref, void *addr[], uint32_t size[], uint32_t max_num_entries, uint32_t *num_entries) |
| Exports the handles from a reference object. More... | |
| VX_API_ENTRY vx_reference VX_API_CALL | tivxCreateReferenceFromExemplar (vx_context context, vx_reference exemplar) |
| Create reference from a exemplar object. More... | |
| #define TIVX_TARGET_HOST "HOST" |
| #define TIVX_CONTROL_CMD_SEND_TO_ALL_REPLICATED_NODES ((uint32_t)-1) |
TI attribute extensions for the node object.
| Enumerator | |
|---|---|
| TIVX_NODE_TARGET_STRING | Returns the target string corresponding to the node. |
| TIVX_NODE_TIMEOUT | Set/Query the node level timeout parameter. Read-Write. Can be written at initialization as well as at runtime. This timeout attribute affects the operation of the node CREATE and DELETE target kernel functions. Use a |
| TIVX_NODE_IS_TIMED_OUT | Query the node to see if it has timed out. Read-Only. Can be read at initialization as well as at runtime. Use a |
TI attribute extensions for the reference object.
| Enumerator | |
|---|---|
| TIVX_REFERENCE_TIMESTAMP | Returns the timestamp in micro-seconds corresponding to the given reference. |
| TIVX_REFERENCE_INVALID | Returns a boolean indicating whether or not a reference is invalid. |
| TIVX_REFERENCE_BUFFER_IS_ALLOCATED | Query the reference to see if the associated buffer has been allocated. Note that this is only applicable in the case that the buffer has been allocated by the framework. It does update if the buffer has been imported to or exported from the vx_reference. Read-Only. Can be read at initialization as well as at runtime. Use a |
TI attribute extensions for the kernel object.
| Enumerator | |
|---|---|
| TIVX_KERNEL_TIMEOUT | Set/Query the kernel level timeout parameter. Read-Write. Can be written at initialization as well as at runtime. Use a |
TI attribute extensions for the context object.
| Enumerator | |
|---|---|
| TIVX_CONTEXT_NUM_USER_KERNEL_ID | Query the context number of user kernel ID's. Read-Only. Can be read at initialization as well as at runtime. Use a |
| TIVX_CONTEXT_NUM_USER_LIBRARY_ID | Query the context number of user library ID's. Read-Only. Can be read at initialization as well as at runtime. Use a |
TI attribute extensions for the image object.
| Enumerator | |
|---|---|
| TIVX_IMAGE_IMAGEPATCH_ADDRESSING | Query the imagepatch addressing structure from a vx_image. Read-Only. Can be read at initialization as well as at runtime. Use a |
| TIVX_IMAGE_STRIDE_Y_ALIGNMENT | Parameter allowing an application to query or set the stride Y alignment of a vx_image. By default, this value will be set to TIVX_DEFAULT_STRIDE_Y_ALIGN. Care must be taken to understand the requirements of the hardware which is consuming or producing the vx_image. Hardware which is being used via an OpenVX node has verification time errors thrown if the alignment is not in accordance with the requirements of the hardware, but alignment requirements of other hardware which is outside the scope of TIOVX (i.e., codecs) must be understood by the application developer and taken into consideration when creating the image consumed by that hardware. (For instance, the default value was originally chosen since this is a requirement of codec used on TI Jacinto devices) Read-Write. Can be read at any time, but only written to prior to the allocation of the buffer. Cannot be applied to subimages or images with subimages. If attempting to modify as a part of an object array, the exemplar itself shall be set rather than the elements of the object array Use a |
| enum tivx_df_image_e |
Based on the VX_DF_IMAGE definition.
vx_df_image to contain these values. | enum tivx_status_e |
| enum tivx_cpu_id_e |
CPU ID for supported CPUs.
CPU ID is defined in platform module since depending on platform the CPUs could be different
Current CPU IDs are defined assuming J721S2 SoC
Caution: This enum is used as index into the array #g_ipc_cpu_id_map, so change in this enum will require change in this array as well.
Definition at line 631 of file tivx_soc_j784s4.h.
| void tivxInit | ( | void | ) |
Function to initialize OpenVX framework.
Should be called during system init on all OpenVX HOST as well as OpenVX target CPUs
NOTE: In Vision SDK, this function is called during VIsion SDK system init so user need not call this explicitly
| void tivxDeInit | ( | void | ) |
Function to de-initialize OpenVX framework.
Should be called during system init on all OpenVX HOST as well as OpenVX target CPUs
NOTE: In Vision SDK, this function is called during VIsion SDK system init so user need not call this explicitly
| void tivxHostInit | ( | void | ) |
Function to initialize OpenVX HOST side functionality.
Should be called during system init after tivxInit() on HOST CPUs only
NOTE: In Vision SDK, this function is called during VIsion SDK system init so user need not call this explicitly
| void tivxHostDeInit | ( | void | ) |
Function to de-initialize OpenVX HOST side functionality.
Should be called during system init before tivxDeInit() on HOST CPUs only
NOTE: In Vision SDK, this function is called during VIsion SDK system init so user need not call this explicitly
| VX_API_ENTRY vx_status VX_API_CALL tivxAddKernelTarget | ( | vx_kernel | kernel, |
| const char * | target_name | ||
| ) |
Associate a target with a kernel.
Call multiple times for each supported target
If given target is not valid on current platform then error VX_ERROR_NOT_SUPPORTED is returned.
Typically VX_ERROR_NOT_SUPPORTED error should be ignored for this API, since this code is typically kept same across platforms
During graph verify however if user asks to run the kernel on a target not supported by this platform it results in a error and graph cannot execute.
| VX_API_ENTRY vx_status VX_API_CALL tivxSetKernelSinkDepth | ( | vx_kernel | kernel, |
| uint32_t | num_sink_bufs | ||
| ) |
Set the number of sink buffers.
| [in] | kernel | Kernel reference |
| [in] | num_sink_bufs | Number of sink buffers |
vx_status_e enumeration. | VX_SUCCESS | No errors. |
| VX_ERROR_INVALID_REFERENCE | kernel is not a valid reference |
| VX_API_ENTRY vx_status VX_API_CALL tivxRegisterModule | ( | const char * | name, |
| vx_publish_kernels_f | publish, | ||
| vx_unpublish_kernels_f | unpublish | ||
| ) |
Register publish and unpublish functions against a module name.
These functions are invoked when vxLoadKernels is called with the registered name.
This is alternative instead of dynamically loading kernels during vxLoadKernels
Duplicate module names not checked by this API.
API is not reentrant, user is recommended to call all tivxRegisterModule during system init before vxCreateContext() from a single thread.
Modules registered against TIVX_MODULE_NAME are called during vxCreateContext so user MUST ensure tivxRegisterModule() is called for TIVX_MODULE_NAME module
| VX_API_ENTRY vx_status VX_API_CALL tivxUnRegisterModule | ( | const char * | name | ) |
UnRegister publish and unpublish functions if previously registered.
| [in] | name | Module name to unregister |
vx_status_e enumeration. | VX_SUCCESS | No errors. |
| VX_FAILURE | Unable to find module "name" in list of registered modules |
| vx_enum tivxGetSelfCpuId | ( | void | ) |
Return CPU ID of the CPU on which this API is called.
vx_emum enumeration of the CPU_ID. | vx_node tivxCreateNodeByKernelEnum | ( | vx_graph | graph, |
| vx_enum | kernelenum, | ||
| vx_reference | params[], | ||
| vx_uint32 | num | ||
| ) |
Utility function to create a node given parameter references and kernel enum.
| [in] | graph | Graph reference |
| [in] | kernelenum | Enumeration specifying a specific kernel |
| [in] | params | List of parameter references corresponding to the enumerated kernel |
| [in] | num | Number of parameter references in params list |
vx_node. Any possible errors preventing a successful creation should be checked using vxGetStatus. | vx_node tivxCreateNodeByKernelRef | ( | vx_graph | graph, |
| vx_kernel | kernel, | ||
| vx_reference | params[], | ||
| vx_uint32 | num | ||
| ) |
Utility function to create a node given parameter references and kernel reference.
| [in] | graph | Graph reference |
| [in] | kernel | Kernel reference |
| [in] | params | List of parameter references corresponding to the kernel reference |
| [in] | num | Number of parameter references in params list |
vx_node. Any possible errors preventing a successful creation should be checked using vxGetStatus. | vx_node tivxCreateNodeByKernelName | ( | vx_graph | graph, |
| const char * | kernel_name, | ||
| vx_reference | params[], | ||
| vx_uint32 | num | ||
| ) |
Utility function to create a node given parameter references and kernel name.
| [in] | graph | Graph reference |
| [in] | kernel_name | String corresponding to the kernel name |
| [in] | params | List of parameter references corresponding to the kernel name |
| [in] | num | Number of parameter references in params list |
vx_node. Any possible errors preventing a successful creation should be checked using vxGetStatus. | vx_bool tivxIsReferenceVirtual | ( | vx_reference | ref | ) |
Utility function to check if the given reference is virtual or not.
| [in] | ref | Reference to query |
vx_bool value. | vx_true_e | The reference is virtual. |
| vx_false_e | The reference is not virtual. |
| vx_reference tivxGetReferenceParent | ( | vx_reference | child_ref | ) |
Utility function to extract the parent reference from an element.
| [in] | child_ref | Child reference to query |
| vx_bool tivxIsTargetEnabled | ( | const char | target_name[] | ) |
Utility function to know if target is enabled or not.
| [in] | target_name | String specifying the target name |
vx_bool value. | vx_true_e | The target is enabled |
| vx_false_e | The target is not enabled |
| uint64_t tivxPlatformGetTimeInUsecs | ( | void | ) |
Get the time in micro seconds.
| vx_status VX_API_CALL tivxSetNodeParameterNumBufByIndex | ( | vx_node | node, |
| vx_uint32 | idx, | ||
| vx_uint32 | num_buf | ||
| ) |
Set number of buffers to allocate at output of a node parameter.
This API acts as a hint and framework may override user specified settings in case any of above conditions are not met.
| [in] | node | Node reference |
| [in] | idx | Node parameter index |
| [in] | num_buf | Number of buffers to allocate |
| vx_status VX_API_CALL tivxGetNodeParameterNumBufByIndex | ( | vx_node | node, |
| vx_uint32 | idx, | ||
| vx_uint32 * | num_buf | ||
| ) |
Get number of buffers to allocate at output of a node parameter.
| [in] | node | Node reference |
| [in] | idx | Node parameter index |
| [out] | num_buf | Number of buffers allocated at output parameter |
| vx_status VX_API_CALL tivxSetGraphPipelineDepth | ( | vx_graph | graph, |
| vx_uint32 | pipeline_depth | ||
| ) |
Indicates to the implementation the depth of the graph pipeline.
| [in] | graph | Graph reference |
| [in] | pipeline_depth | Pipeline depth; Max value is (TIVX_GRAPH_MAX_PIPELINE_DEPTH-1) else it will return an error |
| vx_status VX_API_CALL tivxNodeSendCommand | ( | vx_node | node, |
| uint32_t | replicate_nodex_idx, | ||
| uint32_t | node_cmd_id, | ||
| vx_reference | ref[], | ||
| uint32_t | num_refs | ||
| ) |
Send node specific Control command.
This API is used to send specific control command to the node. Refer to Node documentation for specific control command. Note that this API is blocking and does not return until command is executed by the node. This API is thread safe, ie multi commands can be sent to same or different nodes from different threads
| [in] | node | Reference of the node to which this command is to be sent. |
| [in] | replicate_nodex_idx | In case of a non-replicated node this should be 0, For a replicated node this is the index of the replicated node to which the command is targeted. To send same command to all replicated nodes use TIVX_CONTROL_CMD_SEND_TO_ALL_REPLICATED_NODES |
| [in] | node_cmd_id | Node specific control command id, refer to node specific interface file |
| [in,out] | ref[] | Node parameter,
|
| [in] | num_refs | Number of valid entries/references in ref[] array |
| vx_status VX_API_CALL tivxNodeSendCommandTimed | ( | vx_node | node, |
| uint32_t | replicate_nodex_idx, | ||
| uint32_t | node_cmd_id, | ||
| vx_reference | ref[], | ||
| uint32_t | num_refs, | ||
| uint32_t | timeout | ||
| ) |
Send node specific Control command.
This API is used to send specific control command to the node. Refer to Node documentation for specific control command. Note that this API blocks for at most 'timeout' milli-seconds i.e. the API returns either when the command execution finishes or if the timeout occurs, whichever occurs first. This API is thread safe, ie multi commands can be sent to same or different nodes from different threads
| [in] | node | Reference of the node to which this command is to be sent. |
| [in] | replicate_nodex_idx | In case of a non-replicated node this should be 0, For a replicated node this is the index of the replicated node to which the command is targeted. To send same command to all replicated nodes use TIVX_CONTROL_CMD_SEND_TO_ALL_REPLICATED_NODES |
| [in] | node_cmd_id | Node specific control command id, refer to node specific interface file |
| [in,out] | ref[] | Node parameter,
|
| [in] | num_refs | Number of valid entries/references in ref[] array |
| [in] | timeout | Timeout in units of msecs, use VX_TIMEOUT_WAIT_FOREVER to wait forever |
This API is used to get a reference to a node within a graph at a given index within the graph.
Use vxQueryGraph with attribute VX_GRAPH_NUMNODES to get number of nodes within a graph. This API can be called only on a verified graph. Node returned by this API is not reference counted and should not be released by the user.
| [in] | graph | graph handle |
| [in] | idx | node index, value from 0 .. value returned by vxQueryGraph(VX_GRAPH_NUMNODES) - 1 |
| VX_API_ENTRY vx_status VX_API_CALL tivxSetNodeTileSize | ( | vx_node | node, |
| vx_uint32 | block_width, | ||
| vx_uint32 | block_height | ||
| ) |
Sets the tile size for a given node in a graph. This is only valid for BAM-enabled kernels on C66 DSP.
| [in] | node | The reference to the vx_node object. |
| [in] | block_width | The tile width in pixels. |
| [in] | block_height | The tile height in lines. |
vx_status_e enumeration. | VX_SUCCESS | if the tile size is set correctly. |
| VX_API_ENTRY vx_status VX_API_CALL tivxSetReferenceAttribute | ( | vx_reference | ref, |
| vx_enum | attribute, | ||
| const void * | ptr, | ||
| vx_size | size | ||
| ) |
Sets reference attributes for the below enums: TIVX_REFERENCE_TIMESTAMP.
| [in] | ref | The reference object. |
| [in] | attribute | The attribute of the reference to be set. |
| [in] | ptr | The value of the reference attribute to be set. |
| [in] | size | The size of the value of the reference attribute to be set. |
vx_status_e enumeration. | VX_SUCCESS | if the attribute was set correctly. |
| VX_API_ENTRY vx_bool VX_API_CALL tivxIsReferenceMetaFormatEqual | ( | vx_reference | ref1, |
| vx_reference | ref2 | ||
| ) |
Check for equivalence between the meta formats of two reference objects.
This API is used to check for equivalence between the meta formats of two reference objects. The function returns true if they are equal and false if not.
| [in] | ref1 | First reference object to be compared. |
| [in] | ref2 | Second reference object to be compared. |
_vx_bool_e enumeration. | VX_API_ENTRY vx_status VX_API_CALL tivxReferenceImportHandle | ( | vx_reference | ref, |
| const void * | addr[], | ||
| const uint32_t | size[], | ||
| uint32_t | num_entries | ||
| ) |
Updates a reference object with the supplied handles (pointers to memory).
Any existing handles in the reference object will be over-written with the new handles provided. No error will be reported. If the caller chooses to preserve the existing handles then the caller should use tivxReferenceExportHandle for retrieving the current handles before invoking this function.
The following conditions regarding 'addr' must be TRUE:
Only the following reference object types are supported:
The memory being imported to an OpenVX reference must adhere to the semantics of how the framework allocates memory. This is of particular note for a few OpenVX objects listed below.
Please note the important details below on semantics about the usage of the reference import and export. Errors will occur if the below requirements are not adhered to.
Finally, please refer to the usage section of the TIOVX documentation for further information and diagrams showcasing the proper usage of these API's.
| [in,out] | ref | The reference object to be updated. |
| [in] | addr | An array of pointers for holding the handles. The entries can be NULL. |
| [in] | size | An array of sizes corresponding to handles. The entries will be looked at if the corresponding handle is not NULL. |
| [in] | num_entries | Number of valid entries in addr[]. This should match the number of handles expected to be maintained internally by 'ref' (ex:- for an image object with multiple planes, num_extries > 1). |
vx_status_e enumeration. | VX_SUCCESS | if the import operation is successful. The 'ref' object will have the internal handles updated. |
| VX_FAILURE | if the operation is unsuccessful. The state of the reference object is not changed. A failure can occur for the following reasons:
|
| VX_API_ENTRY vx_status VX_API_CALL tivxReferenceExportHandle | ( | const vx_reference | ref, |
| void * | addr[], | ||
| uint32_t | size[], | ||
| uint32_t | max_num_entries, | ||
| uint32_t * | num_entries | ||
| ) |
Exports the handles from a reference object.
It is the responsibility of the caller to make sure that the addr array is dimensioned to hold all the handles expected from the reference object.
Only the following reference object types are supported:
The memory exported from an OpenVX reference adheres to the semantics of how the framework allocates memory. This is of particular note for a few OpenVX objects listed below.
Please note the important details below on semantics about the usage of the reference import and export. Errors will occur if the below requirements are not adhered to.
Finally, please refer to the usage section of the TIOVX documentation for further information and diagrams showcasing the proper usage of these API's.
| [in] | ref | The reference object to export the handles from. |
| [out] | addr | An array of pointers for holding the handles. |
| [out] | size | An array of sizes corresponding to handles. The entries will be looked |
| [in] | max_num_entries | Maximum number of entries to export. |
| [out] | num_entries | Number of valid entries in addr[]. This should match the number of handles expected to be maintained internally by 'ref' (ex:- for an image object with multiple planes, num_extries > 1). |
vx_status_e enumeration. | VX_SUCCESS | if the export operation is successful. The 'addr' object will be populated with 'num_entries' handles. size[i] will correspond to the handle addr[i]. |
| VX_FAILURE | if the operation is unsuccessful. The state of the reference object is not changed. A failure can occur for the following reasons:
|
| VX_API_ENTRY vx_reference VX_API_CALL tivxCreateReferenceFromExemplar | ( | vx_context | context, |
| vx_reference | exemplar | ||
| ) |
Create reference from a exemplar object.
This API is used to create a new reference using the same meta information as an already created reference object.
| [in] | context | The reference to the implementation context. |
| [in] | exemplar | The exemplar object. |
vx_reference. Any possible errors preventing a successful creation should be checked using vxGetStatus.