|
| PTK_Alg_StereoOG_BoxProp * | PTK_Alg_StereOG_get3DBB (PTK_Alg_StereoOG_obs3DBox *obsBB) |
| | Get bounding box pointer. More...
|
| |
| void | PTK_Alg_StereoOG_CreateOGSetParams (PTK_Alg_StereoOG_CreateOGAllParams *params, PTK_Alg_StereoOG_CreateOGObj *cntxt) |
| | Initialize OG Map creation parameters. More...
|
| |
| int32_t | PTK_Alg_StereoOG_CreateOGConfig (PTK_Alg_StereoOG_CreateOGAllParams *params, PTK_Api_MemoryReq *memReq) |
| | Computes the memory requirements based on the given algorithm configuration parameters. More...
|
| |
| PTK_AlgHandle | PTK_Alg_StereoOG_CreateOGInit (PTK_Alg_StereoOG_CreateOGAllParams *params, const PTK_Api_MemoryRsp *memRsp) |
| | Initializes the library based on the given algorithm configuration parameters and allocated memory blocks. More...
|
| |
| void | PTK_Alg_StereoOG_createOG (PTK_Alg_StereoOG_CreateOGObj *cntxt, PTK_PointCloud *pc, PTK_Alg_StereoOG_obs3DBox *obsBB) |
| | Root function to create OG map from point clouds. More...
|
| |
| int32_t | PTK_Alg_StereoOG_CreateOGGetMem (PTK_Alg_StereoOG_CreateOGObj *cntxt, uint8_t *memPtr) |
| | Get memory size. More...
|
| |
| int32_t | PTK_Alg_StereoOG_getGridPropMem (PTK_Alg_StereoOG_CreateOGObj *cntxt, uint8_t *memPtr) |
| | Get memory size for GridProp mem. More...
|
| |
| int32_t | PTK_Alg_StereoOG_getOGMem (PTK_Alg_StereoOG_CreateOGObj *cntxt, uint8_t *memPtr) |
| | Get memory size for OG map. More...
|
| |
| int32_t | PTK_Alg_StereoOG_getObjMem (PTK_Alg_StereoOG_CreateOGObj *cntxt, PTK_Alg_StereoOG_Object *obj, uint8_t *memPtr) |
| | Get memory size for OG objects. More...
|
| |
| int32_t | PTK_Alg_StereoOG_getOGConnMem (PTK_Alg_StereoOG_CreateOGObj *cntxt, uint8_t *memPtr) |
| | Get memory size for connected component analysis. More...
|
| |
| uint32_t | PTK_Alg_StereoOG_getObsBBSize (const PTK_Alg_StereoOG_CreateOGParams *ogParams) |
| | Get memory size for object 3D bounding box on image without allocating memory. More...
|
| |
| PTK_Alg_StereoOG_obs3DBox * | PTK_Alg_StereoOG_initObsBB (uint8_t *memPtr) |
| | Initialize bouning box structure using the given chunk of memory. More...
|
| |
| void | PTK_Alg_StereoOG_addPoints (PTK_Alg_StereoOG_CreateOGObj *cntxt, PTK_Point *points, int32_t numPoints) |
| | Add point clouds to OG map. More...
|
| |
| void | PTK_Alg_StereoOG_CCA (PTK_Alg_StereoOG_CreateOGObj *cntxt) |
| | Connected component analysis. More...
|
| |
| int16_t | getNeighbor8Idx (PTK_Alg_StereoOG_CreateOGParams *ogParams, PTK_Alg_StereoOG_OGConn *ogConn, int32_t idx, int32_t xIdx, int32_t yIdx) |
| | Find 8 neighboring grids. More...
|
| |
| int16_t | getNeighbor24Idx (PTK_Alg_StereoOG_CreateOGParams *ogParams, PTK_Alg_StereoOG_OGConn *ogConn, int32_t idx, int32_t xIdx, int32_t yIdx) |
| | Find 24 neighboring grids. More...
|
| |
| void | PTK_Alg_StereoOG_mergeObjects (PTK_Alg_StereoOG_CreateOGObj *cntxt) |
| | Merge neighboring objects. More...
|
| |
| bool | PTK_Alg_StereoOG_mergeTwoObjects (PTK_Alg_StereoOG_Object *curObj, PTK_Alg_StereoOG_Object *newObj, int32_t gridSize, int16_t index) |
| | Merge neighboring objects. More...
|
| |
| void | PTK_Alg_StereoOG_applyTemporalFilter (PTK_Alg_StereoOG_CreateOGObj *cntxt) |
| | Apply temporal filtering of objects. More...
|
| |
| void | PTK_Alg_StereoOG_findCorrespondence (PTK_Alg_StereoOG_CreateOGObj *cntxt, PTK_Alg_StereoOG_Object *srcObj, PTK_Alg_StereoOG_Object *refObj, uint8_t direction) |
| | Find corresponding objects in two frames. More...
|
| |
| void | PTK_Alg_StereoOG_associateCorrespondence (PTK_Alg_StereoOG_CreateOGObj *cntxt, PTK_Alg_StereoOG_Object *curObj, PTK_Alg_StereoOG_Object *prevObj) |
| | Associate the objects in the current frame to the previous frame's object. The assocaited objects shuold have the matched forward serach and backward search. More...
|
| |
| void | PTK_Alg_StereoOG_mergeObjectsTemporal (PTK_Alg_StereoOG_CreateOGObj *cntxt, int8_t direction) |
| | Merge the current (or previous) frame's object, which does not have
correspondences in the prvious (or current ) frame, with a close object in the same frame. More...
|
| |
| float | PTK_Alg_StereoOG_computeDistanceObjects (uint8_t mode, PTK_Alg_StereoOG_Object *obj1, PTK_Alg_StereoOG_Object *obj2, int16_t idx1, int16_t idx2) |
| | Merge neighboring objects. More...
|
| |
| void | PTK_Alg_StereoOG_createBB (PTK_Alg_StereoOG_CreateOGObj *cntxt, PTK_Alg_StereoOG_Object *object, PTK_Alg_StereoOG_obs3DBox *obsBB) |
| | Create 3D bounding boxes for detected objects. More...
|
| |
| void | PTK_Alg_StereoOG_copyObjectInfo (PTK_Alg_StereoOG_Object *srcObj, PTK_Alg_StereoOG_Object *dstObj, int16_t srcIdx, int16_t dstIdx) |
| | Merge neighboring objects. More...
|
| |
| void | PTK_Alg_StereoOG_resetOG (PTK_Alg_StereoOG_CreateOGObj *cntxt) |
| | Reset OG. More...
|
| |
| void | PTK_Alg_StereoOG_resetTemporalReference (PTK_Alg_StereoOG_CreateOGObj *cntxt) |
| | Reset temporal object reference. More...
|
| |