MATHLIB User Guide
MATHLIB_tanh.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_tanh (size_t length, T *pSrc, T *pDst)
 Performs the elementwise hyperbolic tangent of an input vector. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise hyperbolic tangent of a vector. More...
 
MATHLIB_STATUS MATHLIB_tanh_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_tanh. Function accepts float pointers. More...