![]() |
MATHLIB User Guide
|
Go to the source code of this file.
Functions | |
| template<typename T > | |
| MATHLIB_STATUS | MATHLIB_sqrt (size_t length, T *pSrc, T *pDst) |
| Performs the elementwise square root of an input vectors. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise square root of an input vector. More... | |
| MATHLIB_STATUS | MATHLIB_sqrt_sp (size_t length, float *pSrc, float *pDst) |
| This function is the C interface for MATHLIB_sqrt. Function accepts float pointers. More... | |
| MATHLIB_STATUS | MATHLIB_sqrt_dp (size_t length, double *pSrc, double *pDst) |
| This function is the C interface for MATHLIB_sqrt. Function accepts double pointers. More... | |