MATHLIB User Guide
MATHLIB_sin.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_sin (size_t length, T *pSrc, T *pDst)
 Performs the elementwise sine of an input vector. Function can be overloaded with float and double pointers, and the appropriate precision is employed to compute elementwise sine of the input vector. More...
 
MATHLIB_STATUS MATHLIB_sin_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_sin. Function accepts float pointers. More...
 
MATHLIB_STATUS MATHLIB_sin_dp (size_t length, double *pSrc, double *pDst)
 This function is the C interface for MATHLIB_sin. Function accepts double pointers. More...