MATHLIB User Guide
MATHLIB_rsqrt.h File Reference

Go to the source code of this file.

Functions

template<typename T >
MATHLIB_STATUS MATHLIB_rsqrt (size_t length, T *pSrc, T *pDst)
 Performs the elementwise reciprocal square root of an input vectors. Function can be overloaded with float pointers, and the appropriate precision is employed to compute elementwise reciprocal square root of an input vector. More...
 
MATHLIB_STATUS MATHLIB_rsqrt_sp (size_t length, float *pSrc, float *pDst)
 This function is the C interface for MATHLIB_rsqrt. Function accepts float pointers. More...